![Logo](ti_logo.svg) |
AM62x MCU+ SDK
08.04.00
|
|
Go to the documentation of this file.
54 #ifndef MESSAGES_CORE_H
55 #define MESSAGES_CORE_H
TISCI_MSG_QUERY_MSMC request response providing currently available MSMC memory if present in the SoC...
Definition: tisci_core.h:287
Empty response for TISCI_MSG_BOARD_CONFIG_PM.
Definition: tisci_core.h:257
TISCI_MSG_VERSION request to provide version info about currently running firmware.
Definition: tisci_core.h:87
uint32_t tisci_boardcfg_rmp_high
Definition: tisci_core.h:135
uint8_t abi_major
Definition: tisci_core.h:91
uint32_t msmc_end_low
Definition: tisci_core.h:291
uint32_t tisci_boardcfg_pmp_low
Definition: tisci_core.h:243
TISCI_MSG_QUERY_MSMC request to provide currently available MSMC memory if present in the SoC.
Definition: tisci_core.h:271
uint32_t msmc_start_low
Definition: tisci_core.h:289
uint32_t tisci_boardcfgp_high
Definition: tisci_core.h:178
struct tisci_header hdr
Definition: tisci_core.h:161
uint32_t extboot_status
Definition: tisci_core.h:105
struct tisci_header hdr
Definition: tisci_core.h:288
Empty response for TISCI_MSG_BOARD_CONFIG_RESASG.
Definition: tisci_core.h:160
uint8_t abi_minor
Definition: tisci_core.h:92
struct tisci_header hdr
Definition: tisci_core.h:272
char str[32]
Definition: tisci_core.h:89
uint8_t patch_version
Definition: tisci_core.h:94
Empty response for TISCI_MSG_BOARD_CONFIG.
Definition: tisci_core.h:191
uint16_t version
Definition: tisci_core.h:90
struct tisci_header hdr
Definition: tisci_core.h:149
uint16_t tisci_boardcfg_security_size
Definition: tisci_core.h:212
TISCI_MSG_BOARD_CONFIG request to provide the location and size of the tisci_boardcfg structure.
Definition: tisci_core.h:175
struct tisci_header hdr
Definition: tisci_core.h:133
Empty response for TISCI_MSG_BOARD_CONFIG_SECURITY.
Definition: tisci_core.h:224
struct tisci_header hdr
Definition: tisci_core.h:192
uint16_t tisci_boardcfg_size
Definition: tisci_core.h:179
struct tisci_header hdr
Definition: tisci_core.h:117
uint32_t tisci_boardcfg_securityp_high
Definition: tisci_core.h:211
struct tisci_header hdr
Definition: tisci_core.h:88
Notification message to indicate the DMSC is available.
Definition: tisci_core.h:103
struct tisci_header hdr
Definition: tisci_core.h:258
uint32_t tisci_boardcfg_rmp_low
Definition: tisci_core.h:134
uint32_t tisci_boardcfg_pmp_high
Definition: tisci_core.h:244
struct tisci_header hdr
Definition: tisci_core.h:242
uint8_t devgrp_t
Defines the sysfw DEVGRP type. This is meant to be used in code or data structures that require disti...
Definition: sciclient.h:336
devgrp_t tisci_boardcfg_rm_devgrp
Definition: tisci_core.h:137
devgrp_t tisci_boardcfg_pm_devgrp
Definition: tisci_core.h:246
struct tisci_header hdr
Definition: tisci_core.h:225
TISCI_MSG_BOARD_CONFIG_RM request to provide the location and size of the tisci_boardcfg Resource Man...
Definition: tisci_core.h:132
Empty response for TISCI_MSG_BOARD_CONFIG_RM.
Definition: tisci_core.h:148
This file contains:
Definition: tisci_core.h:72
uint32_t tisci_boardcfg_securityp_low
Definition: tisci_core.h:210
Response to notification message about firmware availability.
Definition: tisci_core.h:116
uint16_t tisci_boardcfg_rm_size
Definition: tisci_core.h:136
struct tisci_header hdr
Definition: tisci_core.h:209
struct tisci_header hdr
Definition: tisci_core.h:176
uint32_t msmc_end_high
Definition: tisci_core.h:292
uint32_t tisci_boardcfgp_low
Definition: tisci_core.h:177
uint16_t tisci_boardcfg_pm_size
Definition: tisci_core.h:245
TISCI_MSG_BOARD_CONFIG_PM request to provide the location and size of the tisci_boardcfg Power Manage...
Definition: tisci_core.h:241
devgrp_t tisci_boardcfg_devgrp
Definition: tisci_core.h:180
struct tisci_msg_version_req __attribute__((__packed__))
struct tisci_header hdr
Definition: tisci_core.h:73
TISCI_MSG_BOARD_CONFIG_SECURITY request to provide the location and size of the tisci_boardcfg securi...
Definition: tisci_core.h:208
uint8_t sub_version
Definition: tisci_core.h:93
devgrp_t tisci_boardcfg_security_devgrp
Definition: tisci_core.h:213
struct tisci_header hdr
Definition: tisci_core.h:104
uint32_t msmc_start_high
Definition: tisci_core.h:290