AM62x MCU+ SDK  08.04.00

Detailed Description

Releases interrupt peripheral resources according to the valid configuration provided. The following tisci_msg_rm_irq_release_req::valid_params valid bit combinations are allowed: Interrupt Router Mux Release - Release an IR input to output mux connection where the IR input is the src_index and the IR output is the dst_host_irq. Both the src_id and the dst_id must be the device ID of the IR being configured. tisci_msg_rm_irq_release_req::dst_id valid bit == STRUE tisci_msg_rm_irq_release_req::dst_host_irq valid bit == STRUE tisci_msg_rm_irq_release_req::ia_id valid bit == SFALSE tisci_msg_rm_irq_release_req::vint valid bit == SFALSE tisci_msg_rm_irq_release_req::global_event valid bit == SFALSE tisci_msg_rm_irq_release_req::vint_status_bit_index valid bit == SFALSE Event to VINT Unmap Only - Clear only peripheral OES register and event to VINT status bit mapping tisci_msg_rm_irq_release_req::dst_id valid bit == SFALSE tisci_msg_rm_irq_release_req::dst_host_irq valid bit == SFALSE tisci_msg_rm_irq_release_req::ia_id valid bit == STRUE tisci_msg_rm_irq_release_req::vint valid bit == STRUE tisci_msg_rm_irq_release_req::global_event valid bit == STRUE tisci_msg_rm_irq_release_req::vint_status_bit_index valid bit == STRUE OES Register Programming Only - Only clears the OES register of the source. Useful for clearing UDMAP trigger events and any other events that are not translated to the interrupt domain: tisci_msg_rm_irq_release_req::dst_id valid bit == SFALSE tisci_msg_rm_irq_release_req::dst_host_irq valid bit == SFALSE tisci_msg_rm_irq_release_req::ia_id valid bit == SFALSE tisci_msg_rm_irq_release_req::vint valid bit == SFALSE tisci_msg_rm_irq_release_req::global_event valid bit == STRUE tisci_msg_rm_irq_release_req::vint_status_bit_index valid bit == SFALSE.

Parameters
hdrStandard TISCI header
valid_paramsBitfield defining validity of interrupt route release parameters. The interrupt route release fields are not valid, and will not be used for route release, if their corresponding valid bit is zero. Valid bit usage: 0 - Valid bit for tisci_msg_rm_irq_release_req::dst_id 1 - Valid bit for tisci_msg_rm_irq_release_req::dst_host_irq 2 - Valid bit for tisci_msg_rm_irq_release_req::ia_id 3 - Valid bit for tisci_msg_rm_irq_release_req::vint 4 - Valid bit for tisci_msg_rm_irq_release_req::global_event 5 - Valid bit for tisci_msg_rm_irq_release_req::vint_status_bit_index 31 - Valid bit for tisci_msg_rm_irq_release_req::secondary_host
src_idID of interrupt source peripheral
src_indexInterrupt source index within source peripheral
dst_idSoC IR device ID when the valid_params bits are set to release an IR mux connection. This field is only valid if TISCI_MSG_VALUE_RM_DST_ID_VALID is set in tisci_msg_rm_irq_release_req::valid_params.
dst_host_irqSoC IR output index when the valid_params are set to release an IR mux connection. This field is only valid if TISCI_MSG_VALUE_RM_DST_HOST_IRQ_VALID is set in tisci_msg_rm_irq_release_req::valid_params.
ia_idDevice ID of interrupt aggregator in which the virtual interrupt resides. This field is only valid if TISCI_MSG_VALUE_RM_IA_ID_VALID is set in tisci_msg_rm_irq_release_req::valid_params.
vintVirtual interrupt number if the interrupt route is through an interrupt aggregator. This field is only valid if TISCI_MSG_VALUE_RM_VINT_VALID is set in tisci_msg_rm_irq_release_req::valid_params.
global_eventGlobal event mapped to interrupt aggregator virtual interrupt status bit. The event is cleared from the OES register of the interrupt source. This field is only applicable for interrupt source's capable of generating global events. This field is only valid if TISCI_MSG_VALUE_RM_GLOBAL_EVENT_VALID is set in tisci_msg_rm_irq_release_req::valid_params.
vint_status_bit_indexVirtual interrupt status bit to release if the interrupt route utilizes an interrupt aggregator virtual interrupt. This field is only valid if TISCI_MSG_VALUE_RM_VINT_STATUS_BIT_INDEX_VALID is set in tisci_msg_rm_irq_release_req::valid_params.
secondary_hostThe interrupt route destination is the specified secondary host if the secondary_host's corresponding valid bit is set in tisci_msg_rm_irq_release_req::valid_params. Otherwise, the host within the TISCI message header is the route destination.

Data Fields

struct tisci_header hdr
 
uint32_t valid_params
 
uint16_t src_id
 
uint16_t src_index
 
uint16_t dst_id
 
uint16_t dst_host_irq
 
uint16_t ia_id
 
uint16_t vint
 
uint16_t global_event
 
uint8_t vint_status_bit_index
 
uint8_t secondary_host
 

Field Documentation

◆ hdr

struct tisci_header tisci_msg_rm_irq_release_req::hdr

◆ valid_params

uint32_t tisci_msg_rm_irq_release_req::valid_params

◆ src_id

uint16_t tisci_msg_rm_irq_release_req::src_id

◆ src_index

uint16_t tisci_msg_rm_irq_release_req::src_index

◆ dst_id

uint16_t tisci_msg_rm_irq_release_req::dst_id

◆ dst_host_irq

uint16_t tisci_msg_rm_irq_release_req::dst_host_irq

◆ ia_id

uint16_t tisci_msg_rm_irq_release_req::ia_id

◆ vint

uint16_t tisci_msg_rm_irq_release_req::vint

◆ global_event

uint16_t tisci_msg_rm_irq_release_req::global_event

◆ vint_status_bit_index

uint8_t tisci_msg_rm_irq_release_req::vint_status_bit_index

◆ secondary_host

uint8_t tisci_msg_rm_irq_release_req::secondary_host