AM62x MCU+ SDK  08.03.00

Detailed Description

I2C Parameters.

I2C parameters are used to with the I2C_open() call. Default values for these parameters are set using I2C_Params_init().

If I2C_TransferMode is set to I2C_MODE_BLOCKING then I2C_transfer function calls will block thread execution until the transaction has completed.

If I2C_TransferMode is set to I2C_MODE_CALLBACK then I2C_transfer will not block thread execution and it will call the function specified by transferCallbackFxn. Sequential calls to I2C_transfer in I2C_MODE_CALLBACK mode will put the designated transaction onto an internal queue that automatically starts queued transactions after the previous transaction has completed. (regardless of error state).

I2C_BitRate specifies the I2C bus rate used for I2C communications.

Data Fields

uint8_t transferMode
 
void(* transferCallbackFxn )(I2C_Handle i2cHnd, I2C_Transaction *msg, int32_t transferStatus)
 
uint8_t bitRate
 

Field Documentation

◆ transferMode

uint8_t I2C_Params::transferMode

Blocking or Callback mode

◆ transferCallbackFxn

void(* I2C_Params::transferCallbackFxn) (I2C_Handle i2cHnd, I2C_Transaction *msg, int32_t transferStatus)

I2C_CallbackFxn transferCallbackFxn; Callback function pointer

◆ bitRate

uint8_t I2C_Params::bitRate

I2C bus bit rate