AM62Px MCU+ SDK  12.00.00
tisci_rm_irq.h File Reference

Go to the source code of this file.

Data Structures

struct  tisci_msg_rm_irq_set_req
 Configures peripherals within the interrupt subsystem according to the valid configuration provided. The following tisci_msg_rm_irq_set_req::valid_params valid bit combinations are allowed: Interrupt Router Mux Configuration - Configures an IR input to output mux connection where the IR input is the src_index and the IR output is the dst_host_irq. Both the src_id and the dst_id must be the device ID of the IR being configured. tisci_msg_rm_irq_set_req::dst_id valid bit == STRUE tisci_msg_rm_irq_set_req::dst_host_irq valid bit == STRUE tisci_msg_rm_irq_set_req::ia_id valid bit == SFALSE tisci_msg_rm_irq_set_req::vint valid bit == SFALSE tisci_msg_rm_irq_set_req::global_event valid bit == SFALSE tisci_msg_rm_irq_set_req::vint_status_bit_index valid bit == SFALSE Event to VINT Mapping Only - Configure peripheral OES register and add an event mapping to an IA VINT tisci_msg_rm_irq_set_req::dst_id valid bit == SFALSE tisci_msg_rm_irq_set_req::dst_host_irq valid bit == SFALSE tisci_msg_rm_irq_set_req::ia_id valid bit == STRUE tisci_msg_rm_irq_set_req::vint valid bit == STRUE tisci_msg_rm_irq_set_req::global_event valid bit == STRUE tisci_msg_rm_irq_set_req::vint_status_bit_index valid bit == STRUE OES Register Programming Only - Only programs the OES register of the source. Useful for setting UDMAP trigger events and any other events that are not translated to the interrupt domain: tisci_msg_rm_irq_set_req::dst_id valid bit == SFALSE tisci_msg_rm_irq_set_req::dst_host_irq valid bit == SFALSE tisci_msg_rm_irq_set_req::ia_id valid bit == SFALSE tisci_msg_rm_irq_set_req::vint valid bit == SFALSE tisci_msg_rm_irq_set_req::global_event valid bit == STRUE tisci_msg_rm_irq_set_req::vint_status_bit_index valid bit == SFALSE. More...
 
struct  tisci_msg_rm_irq_set_resp
 Response to setting a peripheral to processor interrupt. More...
 
struct  tisci_msg_rm_irq_release_req
 Releases interrupt peripheral resources according to the valid configuration provided. The following tisci_msg_rm_irq_release_req::valid_params valid bit combinations are allowed: Interrupt Router Mux Release - Release an IR input to output mux connection where the IR input is the src_index and the IR output is the dst_host_irq. Both the src_id and the dst_id must be the device ID of the IR being configured. tisci_msg_rm_irq_release_req::dst_id valid bit == STRUE tisci_msg_rm_irq_release_req::dst_host_irq valid bit == STRUE tisci_msg_rm_irq_release_req::ia_id valid bit == SFALSE tisci_msg_rm_irq_release_req::vint valid bit == SFALSE tisci_msg_rm_irq_release_req::global_event valid bit == SFALSE tisci_msg_rm_irq_release_req::vint_status_bit_index valid bit == SFALSE Event to VINT Unmap Only - Clear only peripheral OES register and event to VINT status bit mapping tisci_msg_rm_irq_release_req::dst_id valid bit == SFALSE tisci_msg_rm_irq_release_req::dst_host_irq valid bit == SFALSE tisci_msg_rm_irq_release_req::ia_id valid bit == STRUE tisci_msg_rm_irq_release_req::vint valid bit == STRUE tisci_msg_rm_irq_release_req::global_event valid bit == STRUE tisci_msg_rm_irq_release_req::vint_status_bit_index valid bit == STRUE OES Register Programming Only - Only clears the OES register of the source. Useful for clearing UDMAP trigger events and any other events that are not translated to the interrupt domain: tisci_msg_rm_irq_release_req::dst_id valid bit == SFALSE tisci_msg_rm_irq_release_req::dst_host_irq valid bit == SFALSE tisci_msg_rm_irq_release_req::ia_id valid bit == SFALSE tisci_msg_rm_irq_release_req::vint valid bit == SFALSE tisci_msg_rm_irq_release_req::global_event valid bit == STRUE tisci_msg_rm_irq_release_req::vint_status_bit_index valid bit == SFALSE. More...
 
struct  tisci_msg_rm_irq_release_resp
 Response to releasing a peripheral to processor interrupt. More...
 

Macros

#define TISCI_MSG_VALUE_RM_DST_ID_VALID   (1u << 0u)
 This file contains: More...
 
#define TISCI_MSG_VALUE_RM_DST_HOST_IRQ_VALID   (1u << 1u)
 
#define TISCI_MSG_VALUE_RM_IA_ID_VALID   (1u << 2u)
 
#define TISCI_MSG_VALUE_RM_VINT_VALID   (1u << 3u)
 
#define TISCI_MSG_VALUE_RM_GLOBAL_EVENT_VALID   (1u << 4u)
 
#define TISCI_MSG_VALUE_RM_VINT_STATUS_BIT_INDEX_VALID   (1u << 5u)
 

Functions

struct tisci_msg_rm_irq_set_req __attribute__ ((__packed__))
 

Variables

struct tisci_header hdr
 
uint32_t valid_params
 
uint16_t src_id
 
uint16_t src_index
 
uint16_t dst_id
 
uint16_t dst_host_irq
 
uint16_t ia_id
 
uint16_t vint
 
uint16_t global_event
 
uint8_t vint_status_bit_index
 
uint8_t secondary_host
 

Variable Documentation

◆ hdr

struct tisci_header hdr

◆ valid_params

uint32_t valid_params

◆ src_id

uint16_t src_id

◆ src_index

uint16_t src_index

◆ dst_id

uint16_t dst_id

◆ dst_host_irq

uint16_t dst_host_irq

◆ ia_id

uint16_t ia_id

◆ vint

uint16_t vint

◆ global_event

uint16_t global_event

◆ vint_status_bit_index

uint8_t vint_status_bit_index

◆ secondary_host

uint8_t secondary_host