AM62Px MCU+ SDK  12.00.00
tisci_boot_mode.h File Reference

Go to the source code of this file.

Data Structures

struct  tisci_msg_set_otp_boot_mode_req
 This file contains: More...
 
struct  tisci_msg_set_otp_boot_mode_resp
 Response to set boot mode request. More...
 

Functions

struct tisci_msg_set_otp_boot_mode_req __attribute__ ((__packed__))
 

Variables

struct tisci_header hdr
 
uint8_t boot_mode_efuse_idx
 
uint8_t resv [3]
 
uint32_t write_val
 

Variable Documentation

◆ hdr

struct tisci_header hdr

◆ boot_mode_efuse_idx

uint8_t boot_mode_efuse_idx

◆ resv

uint8_t resv[3]

◆ write_val

uint32_t write_val