AM62Px MCU+ SDK  12.00.00
I2CLLD_targetTransaction Struct Reference

Detailed Description

I2C Target Transaction.

This structure defines the complete I2C transfer.

This structure specifies the buffer and buffer's size that is to be read from or written to the I2C controller. In restart condition, readBuf/writeBuf and readCount/writeCount are used repeatedly for every start in one transfer. When each restart happens, driver will call back to application with the restart transfer status, and application should save the data transferred in the previous start, and provide the new data to the current start. When all the starts complete (stop condition), driver will call back to application with transfer success status, and readBuf/writeBuf and readCount/writeCount will only record the data transferred in the last start condition.

Data Fields

uint8_t * writeBuf
 
uint32_t writeCount
 
uint8_t * readBuf
 
uint32_t readCount
 
uint32_t timeout
 
bool expandSA
 

Field Documentation

◆ writeBuf

uint8_t* I2CLLD_targetTransaction::writeBuf

Buffer containing data to be written to controller

◆ writeCount

uint32_t I2CLLD_targetTransaction::writeCount

Number of bytes to be written to the controller

◆ readBuf

uint8_t* I2CLLD_targetTransaction::readBuf

Buffer to which data from controller is to be read into

◆ readCount

uint32_t I2CLLD_targetTransaction::readCount

Number of bytes to be read to the controller

◆ timeout

uint32_t I2CLLD_targetTransaction::timeout

Timeout value for i2c transaction in Micro Seconds

◆ expandSA

bool I2CLLD_targetTransaction::expandSA

Expand target address: true: 10-bit address mode, false: 7-bit address mode