AM62Px MCU+ SDK  12.00.00

Detailed Description

Structure used to pass information about the heap out of HeapP_getHeapStats().

Data Fields

size_t availableHeapSpaceInBytes
 
size_t sizeOfLargestFreeBlockInBytes
 
size_t sizeOfSmallestFreeBlockInBytes
 
size_t numberOfFreeBlocks
 
size_t minimumEverFreeBytesRemaining
 
size_t numberOfSuccessfulAllocations
 
size_t numberOfSuccessfulFrees
 

Field Documentation

◆ availableHeapSpaceInBytes

size_t HeapP_MemStats::availableHeapSpaceInBytes

The total heap size, in bytes, currently available - this is the sum of all the free blocks, not the largest block that can be allocated.

◆ sizeOfLargestFreeBlockInBytes

size_t HeapP_MemStats::sizeOfLargestFreeBlockInBytes

The maximum size, in bytes, of all the free blocks within the heap at the time vPortGetHeapStats() is called.

◆ sizeOfSmallestFreeBlockInBytes

size_t HeapP_MemStats::sizeOfSmallestFreeBlockInBytes

The minimum size, in bytes, of all the free blocks within the heap at the time vPortGetHeapStats() is called.

◆ numberOfFreeBlocks

size_t HeapP_MemStats::numberOfFreeBlocks

The number of free memory blocks within the heap at the time vPortGetHeapStats() is called.

◆ minimumEverFreeBytesRemaining

size_t HeapP_MemStats::minimumEverFreeBytesRemaining

The minimum amount of total free memory, in bytes, (sum of all free blocks) there has been in the heap since the system booted.

◆ numberOfSuccessfulAllocations

size_t HeapP_MemStats::numberOfSuccessfulAllocations

The number of calls to HeapP_alloc() that have returned a valid memory block.

◆ numberOfSuccessfulFrees

size_t HeapP_MemStats::numberOfSuccessfulFrees

The number of calls to HeapP_free() that has successfully freed a block of memory.