AM62Px MCU+ SDK  12.00.00
EnetPhy_FsmTimeoutCfg Struct Reference

Detailed Description

PHY State-Machine time-out values.

Data Fields

uint32_t findingStateTicks
 FINDING state timeout (in ticks). More...
 
uint32_t resetWaitStateTicks
 RESET_WAIT state timeout (in ticks). More...
 
uint32_t resetWaitStateResidenceTicks
 RESET_WAIT state residence time (in ticks). More...
 
uint32_t nwayStartStateTicks
 NWAY_START state timeout (in ticks). More...
 
uint32_t nwayWaitStateTicks
 NWAY_WAIT state timeout (in ticks). More...
 
uint32_t linkWaitStateTicks
 LINK_WAIT state timeout (in ticks). More...
 
uint32_t mdixTicks
 Timeout if MDIX is enabled (in ticks). More...
 

Field Documentation

◆ findingStateTicks

uint32_t EnetPhy_FsmTimeoutCfg::findingStateTicks

FINDING state timeout (in ticks).

Set to ENETPHY_TIMEOUT_WAIT_FOREVER, to disable timeout.
Set to ENETPHY_TIMEOUT_NO_WAIT, to expire immediately

◆ resetWaitStateTicks

uint32_t EnetPhy_FsmTimeoutCfg::resetWaitStateTicks

RESET_WAIT state timeout (in ticks).

Set to ENETPHY_TIMEOUT_WAIT_FOREVER, to disable timeout.
Set to ENETPHY_TIMEOUT_NO_WAIT, to expire immediately

◆ resetWaitStateResidenceTicks

uint32_t EnetPhy_FsmTimeoutCfg::resetWaitStateResidenceTicks

RESET_WAIT state residence time (in ticks).

◆ nwayStartStateTicks

uint32_t EnetPhy_FsmTimeoutCfg::nwayStartStateTicks

NWAY_START state timeout (in ticks).

Set to ENETPHY_TIMEOUT_WAIT_FOREVER, to disable timeout.
Set to ENETPHY_TIMEOUT_NO_WAIT, to expire immediately

◆ nwayWaitStateTicks

uint32_t EnetPhy_FsmTimeoutCfg::nwayWaitStateTicks

NWAY_WAIT state timeout (in ticks).

Set to ENETPHY_TIMEOUT_WAIT_FOREVER, to disable timeout.
Set to ENETPHY_TIMEOUT_NO_WAIT, to expire immediately

◆ linkWaitStateTicks

uint32_t EnetPhy_FsmTimeoutCfg::linkWaitStateTicks

LINK_WAIT state timeout (in ticks).

Set to ENETPHY_TIMEOUT_WAIT_FOREVER, to disable timeout.
Set to ENETPHY_TIMEOUT_NO_WAIT, to expire immediately

◆ mdixTicks

uint32_t EnetPhy_FsmTimeoutCfg::mdixTicks

Timeout if MDIX is enabled (in ticks).