AM62Px MCU+ SDK  12.00.00

Detailed Description

CPTS EST timestamp.

Data Fields

uint64_t tsVal
 
uint8_t priority
 
uint32_t seqNum
 
uint32_t ingressPort
 
uint32_t egressPort
 
uint32_t domain
 

Field Documentation

◆ tsVal

uint64_t CpswCpts_EstEvent::tsVal

Time stamp value when the event occurred

◆ priority

uint8_t CpswCpts_EstEvent::priority

Hardware switch priority

◆ seqNum

uint32_t CpswCpts_EstEvent::seqNum

Sequence number of the event

◆ ingressPort

uint32_t CpswCpts_EstEvent::ingressPort

Packet receive port number

◆ egressPort

uint32_t CpswCpts_EstEvent::egressPort

Transmit port number

◆ domain

uint32_t CpswCpts_EstEvent::domain

Domain number of the event