AM62Px MCU+ SDK  12.00.00

Detailed Description

Port specific VLAN security configuration.

Data Fields

bool vidIngressCheck
 
bool dropUntagged
 
bool dropDualVlan
 
bool dropDoubleVlan
 

Field Documentation

◆ vidIngressCheck

bool CpswAle_PortVlanSecurityCfg::vidIngressCheck

VLAN ID Ingress Check

◆ dropUntagged

bool CpswAle_PortVlanSecurityCfg::dropUntagged

Drop untagged packets

◆ dropDualVlan

bool CpswAle_PortVlanSecurityCfg::dropDualVlan

Drop Dual VLAN - When set will cause any received packet with dual VLAN stag followed by ctag to be dropped

◆ dropDoubleVlan

bool CpswAle_PortVlanSecurityCfg::dropDoubleVlan

Drop Double VLAN - When set cause any received packet with double VLANs to be dropped. That is if there are two ctag or two stag fields in the packet it will be dropped