AM62Px MCU+ SDK  09.02.01

Introduction

The DMSC firmware Resource Management (RM) (sub) system manages SoC shared resources. RM manages access and configuration of shared resources amongst SoC processing entities. RM provides a set of interfaces over which SoC processing entities can allocate, configure, and free shared resources.

Files

file  sciclient_rm.h
 This file contains the definition of all the message IDs, message formats to be able to interact with the System Controller firmware for resource management.
 

Functions

int32_t Sciclient_rmGetResourceRange (const struct tisci_msg_rm_get_resource_range_req *req, struct tisci_msg_rm_get_resource_range_resp *resp, uint32_t timeout)
 Retrieves a host's assigned range for a resource. More...
 
int32_t Sciclient_rmIrqSet (const struct tisci_msg_rm_irq_set_req *req, const struct tisci_msg_rm_irq_set_resp *resp, uint32_t timeout)
 Configures a peripheral to processor IRQ. More...
 
int32_t Sciclient_rmIrqRelease (const struct tisci_msg_rm_irq_release_req *req, uint32_t timeout)
 Releases a peripheral to processor IRQ. More...
 
int32_t Sciclient_rmIrqTranslateIrOutput (uint16_t ir_dev_id, uint16_t ir_output, uint16_t dst_dev_id, uint16_t *dst_input)
 Translates an interrupt router output to the peripheral input it's connected to. The primary use of the function is to retrieve the processor input IRQ an interrupt router output is connected to. More...
 
int32_t Sciclient_rmIrqTranslateIaOutput (uint16_t ia_dev_id, uint16_t ia_output, uint16_t dst_dev_id, uint16_t *dst_input)
 Translates an interrupt aggregator output to the peripheral input it's connected to. The primary use of the function is to retrieve the processor input IRQ or IR input an interrupt aggregator output is connected to. More...
 
int32_t Sciclient_rmIrqTranslateIrqInput (uint16_t dst_dev_id, uint16_t dst_input, uint16_t src_dev_id, uint16_t *src_output)
 Translates a peripheral input to the connected interrupt router or aggregator output. The primary use of the function is to retrieve the interrupt router or aggregator output connected to a processor input IRQ. More...
 
int32_t Sciclient_rmIrqSetRaw (const struct tisci_msg_rm_irq_set_req *req, const struct tisci_msg_rm_irq_set_resp *resp, uint32_t timeout)
 Configures individual peripherals within the interrupt subsystem (interrupt routers, interrupt aggregators, etc.) according to the configuration provided. Each call of the API only configures a single peripheral within the interrupt route. Multiple calls of the API are required to setup a complete interrupt connection between source and destination which contains multiple hops. More...
 
int32_t Sciclient_rmIrqReleaseRaw (const struct tisci_msg_rm_irq_release_req *req, uint32_t timeout)
 Releases configurations within individual peripherals within the interrupt subsystem (interrupt routers, interrupt aggregators, etc.) according to the configuration provided. Each call of the API only releases a configuration within a single peripheral within the interrupt route. Multiple calls of the API are required to teardown a complete interrupt connection between source and destination which contains multiple hops. More...
 
int32_t Sciclient_rmRingCfg (const struct tisci_msg_rm_ring_cfg_req *req, const struct tisci_msg_rm_ring_cfg_resp *resp, uint32_t timeout)
 Configures a Navigator Subsystem ring. More...
 
int32_t Sciclient_rmUdmapGcfgCfg (const struct tisci_msg_rm_udmap_gcfg_cfg_req *req, const struct tisci_msg_rm_udmap_gcfg_cfg_resp *resp, uint32_t timeout)
 Configures Navigator Subsystem UDMAP GCFG region. More...
 
int32_t Sciclient_rmUdmapTxChCfg (const struct tisci_msg_rm_udmap_tx_ch_cfg_req *req, const struct tisci_msg_rm_udmap_tx_ch_cfg_resp *resp, uint32_t timeout)
 Configures a Navigator Subsystem UDMAP transmit channel. More...
 
int32_t Sciclient_rmUdmapRxChCfg (const struct tisci_msg_rm_udmap_rx_ch_cfg_req *req, const struct tisci_msg_rm_udmap_rx_ch_cfg_resp *resp, uint32_t timeout)
 Configures a Navigator Subsystem UDMAP receive channel. More...
 
int32_t Sciclient_rmUdmapFlowCfg (const struct tisci_msg_rm_udmap_flow_cfg_req *req, const struct tisci_msg_rm_udmap_flow_cfg_resp *resp, uint32_t timeout)
 Configures a Navigator Subsystem UDMAP receive flow. More...
 
int32_t Sciclient_rmUdmapFlowSizeThreshCfg (const struct tisci_msg_rm_udmap_flow_size_thresh_cfg_req *req, const struct tisci_msg_rm_udmap_flow_size_thresh_cfg_resp *resp, uint32_t timeout)
 Configures a Navigator Subsystem UDMAP receive flow's size threshold fields. More...
 
int32_t Sciclient_rmPsilPair (const struct tisci_msg_rm_psil_pair_req *req, uint32_t timeout)
 Pairs a PSI-L source thread and destination threads. More...
 
int32_t Sciclient_rmPsilUnpair (const struct tisci_msg_rm_psil_unpair_req *req, uint32_t timeout)
 Unpairs a PSI-L source thread and destination thread. More...
 
int32_t Sciclient_rmPsilRead (const struct tisci_msg_rm_psil_read_req *req, struct tisci_msg_rm_psil_read_resp *resp, uint32_t timeout)
 Reads a PSI-L thread real-time register. More...
 
int32_t Sciclient_rmPsilWrite (const struct tisci_msg_rm_psil_write_req *req, uint32_t timeout)
 Writes a PSI-L thread real-time register. More...
 
int32_t Sciclient_rmIrOutpIsFree (uint16_t id, uint16_t outp)
 Checks the output's control register to see if the output line has an input line mapped to it. More...
 

Function Documentation

◆ Sciclient_rmGetResourceRange()

int32_t Sciclient_rmGetResourceRange ( const struct tisci_msg_rm_get_resource_range_req req,
struct tisci_msg_rm_get_resource_range_resp resp,
uint32_t  timeout 
)

Retrieves a host's assigned range for a resource.

Returns the range for a unique resource type assigned to the specified host, or secondary host. The unique resource type is formed by combining the 10 LSB of type and the 6 LSB of subtype.

Unique types which do not map to an SoC resource will not be NACK'd. Instead the tisci_msg_rm_get_resource_range_resp range_start and range_num values are zeroed. This provides a known response mechanism across varied SoCs.


Message: TISCI_MSG_RM_GET_RESOURCE_RANGE
Request: tisci_msg_rm_get_resource_range_req
Response: tisci_msg_rm_get_resource_range_resp

Parameters
reqPointer to resource range get payload
respPointer to resource range response payload
timeoutGives a sense of how long to wait for the operation. Refer SystemP_Timeout.
Returns
SystemP_SUCCESS on success, else failure

◆ Sciclient_rmIrqSet()

int32_t Sciclient_rmIrqSet ( const struct tisci_msg_rm_irq_set_req req,
const struct tisci_msg_rm_irq_set_resp resp,
uint32_t  timeout 
)

Configures a peripheral to processor IRQ.

Configures an interrupt route between the peripheral and host processor specified within the tisci_msg_rm_irq_set_req payload. The interrupt destination is either the processor sending the request, or the secondary host if it's defined as a valid host. The following message valid_params bit combinations are allowed:

Non-Event Sourced Direct Interrupt - Non-event peripheral interrupt direct to destination processor. One thing to note is an IA unmapped VINT route can be configured via this combination by passing the IA ID and VINT values as the src_id and src_index parameters. An IA unmapped VINT route is considered a non-event sourced direct interrupt route until a global event is mapped to the IA VINT: dst_id valid bit == true dst_host_irq valid bit == true ia_id valid bit == false vint valid bit == false global_event valid bit == false vint_status_bit_index valid bit == false

Event Sourced Direct Interrupt - Event-based peripheral interrupt direct to destination processor: dst_id valid bit == true dst_host_irq valid bit == true ia_id valid bit == true vint valid bit == true global_event valid bit == true vint_status_bit_index valid bit == true

Unmapped VINT Direct Interrupt - Event-based peripheral interrupt direct to processor with no global event to VINT status bit mapping configured on allocation of the VINT. Allows all event to VINT status bit mappings to take place at a later time: dst_id valid bit == true dst_host_irq valid bit == true ia_id valid bit == true vint valid bit == true global_event valid bit == false vint_status_bit_index valid bit == false

Event to VINT Mapping Only - Configure, or add a mapping to, an event-based peripheral interrupt polled from IA VINT real-time registers. Can also be used to add an event to VINT status bit mapping to an event-based direct interrupt route: dst_id valid bit == false dst_host_irq valid bit == false ia_id valid bit == true vint valid bit == true global_event valid bit == true vint_status_bit_index valid bit == true

OES Register Programming Only - Only programs the OES register of the source. Useful for setting UDMAP trigger events and any other events that are not translated to the interrupt domain: dst_id valid bit == false dst_host_irq valid bit == false ia_id valid bit == false vint valid bit == false global_event valid bit == true vint_status_bit_index valid bit == false The shortest route between the peripheral and the host processor is programmed. Interrupts are not configured on the host processor.


Message: TISCI_MSG_RM_IRQ_SET
Request: tisci_msg_rm_irq_set_req
Response: tisci_msg_rm_irq_set_resp

Parameters
reqPointer to interrupt route set payload
respPointer to interrupt route set response payload
timeoutGives a sense of how long to wait for the operation. Refer SystemP_Timeout.
Returns
SystemP_SUCCESS on success, else failure

◆ Sciclient_rmIrqRelease()

int32_t Sciclient_rmIrqRelease ( const struct tisci_msg_rm_irq_release_req req,
uint32_t  timeout 
)

Releases a peripheral to processor IRQ.

Releases a previously configured interrupt route between a peripheral and host processor. The interrupt destination is either the processor sending the request, or the secondary host if it's defined as a valid host. The following valid_params valid bit combinations are allowed:

Non-Event Sourced Direct Interrupt - Non-event peripheral interrupt direct to destination processor. One thing to note is an IA unmapped VINT route can be released via this combination by passing the IA ID and VINT values as the src_id and src_index parameters. An IA unmapped VINT route is considered a non-event sourced direct interrupt route until a global event is mapped to the IA VINT: dst_id valid bit == true dst_host_irq valid bit == true ia_id valid bit == false vint valid bit == false global_event valid bit == false vint_status_bit_index valid bit == false

Event Sourced Direct Interrupt - Event-based peripheral interrupt direct to destination processor: dst_id valid bit == true dst_host_irq valid bit == true ia_id valid bit == true vint valid bit == true global_event valid bit == true vint_status_bit_index valid bit == true

Unmapped VINT Direct Interrupt - Clear event-based interrupt direct to destination processor which does not have any existing event to VINT status bit mappings: dst_id valid bit == true dst_host_irq valid bit == true ia_id valid bit == true vint valid bit == true global_event valid bit == false vint_status_bit_index valid bit == false

Event to VINT Mapping Only - Clear only peripheral OES register and event to VINT status bit mapping from direct to processor and polled routes. Event-based peripheral interrupt polled routes are polled from the IA VINT real-time registers. For direct to processor routes the entire route is NOT released when the last event to VINT status bit is unmapped using this valid bit combination. This differs from using the Event Source Direct Interrupt valid bit combination where the entire route is released when the last event to VINT status bit mapping is cleared. The Unmapped VINT Direct Interrupt valid bit combination is used to clear an event sourced direct interrupt with no existing event to VINT status bit mappings: dst_id valid bit == false dst_host_irq valid bit == false ia_id valid bit == true vint valid bit == true global_event valid bit == true vint_status_bit_index valid bit == true

OES Register Programming Only - Only clears the OES register of the source. Useful for clearing UDMAP trigger events and any other events that are not translated to the interrupt domain: dst_id valid bit == false dst_host_irq valid bit == false ia_id valid bit == false vint valid bit == false global_event valid bit == true vint_status_bit_index valid bit == false


Message: TISCI_MSG_RM_IRQ_RELEASE
Request: tisci_msg_rm_irq_release_req

Parameters
reqPointer to interrupt route release payload
timeoutGives a sense of how long to wait for the operation. Refer SystemP_Timeout.
Returns
SystemP_SUCCESS on success, else failure

◆ Sciclient_rmIrqTranslateIrOutput()

int32_t Sciclient_rmIrqTranslateIrOutput ( uint16_t  ir_dev_id,
uint16_t  ir_output,
uint16_t  dst_dev_id,
uint16_t *  dst_input 
)

Translates an interrupt router output to the peripheral input it's connected to. The primary use of the function is to retrieve the processor input IRQ an interrupt router output is connected to.

Parameters
ir_dev_idInterrupt router device ID
ir_outputInterrupt router output index
dst_dev_idDevice ID of entity connected to interrupt router output
dst_inputPointer to returned input index of entity connected to interrupt router output
Returns
SystemP_SUCCESS on successful translation, else failure

◆ Sciclient_rmIrqTranslateIaOutput()

int32_t Sciclient_rmIrqTranslateIaOutput ( uint16_t  ia_dev_id,
uint16_t  ia_output,
uint16_t  dst_dev_id,
uint16_t *  dst_input 
)

Translates an interrupt aggregator output to the peripheral input it's connected to. The primary use of the function is to retrieve the processor input IRQ or IR input an interrupt aggregator output is connected to.

Parameters
ia_dev_idInterrupt aggregator device ID
ia_outputInterrupt aggregator output index
dst_dev_idDevice ID of entity connected to interrupt router output
dst_inputPointer to returned input index of entity connected to interrupt router output
Returns
SystemP_SUCCESS on successful translation, else failure

◆ Sciclient_rmIrqTranslateIrqInput()

int32_t Sciclient_rmIrqTranslateIrqInput ( uint16_t  dst_dev_id,
uint16_t  dst_input,
uint16_t  src_dev_id,
uint16_t *  src_output 
)

Translates a peripheral input to the connected interrupt router or aggregator output. The primary use of the function is to retrieve the interrupt router or aggregator output connected to a processor input IRQ.

Parameters
dst_dev_idDevice ID of entity connected to interrupt router or aggregator output
dst_inputInput index of entity connected to interrupt router or aggregator output
src_dev_idInterrupt router or aggregator device ID
src_outputPointer to returned Interrupt router or aggregator output index
Returns
SystemP_SUCCESS on successful translation, else failure

◆ Sciclient_rmIrqSetRaw()

int32_t Sciclient_rmIrqSetRaw ( const struct tisci_msg_rm_irq_set_req req,
const struct tisci_msg_rm_irq_set_resp resp,
uint32_t  timeout 
)

Configures individual peripherals within the interrupt subsystem (interrupt routers, interrupt aggregators, etc.) according to the configuration provided. Each call of the API only configures a single peripheral within the interrupt route. Multiple calls of the API are required to setup a complete interrupt connection between source and destination which contains multiple hops.


Message: TISCI_MSG_RM_IRQ_SET
Request: tisci_msg_rm_irq_set_req
Response: tisci_msg_rm_irq_set_resp

Parameters
reqPointer to interrupt peripheral set payload
respPointer to interrupt peripheral set response payload
timeoutGives a sense of how long to wait for the operation. Refer SystemP_Timeout.
Returns
SystemP_SUCCESS on success, else failure

◆ Sciclient_rmIrqReleaseRaw()

int32_t Sciclient_rmIrqReleaseRaw ( const struct tisci_msg_rm_irq_release_req req,
uint32_t  timeout 
)

Releases configurations within individual peripherals within the interrupt subsystem (interrupt routers, interrupt aggregators, etc.) according to the configuration provided. Each call of the API only releases a configuration within a single peripheral within the interrupt route. Multiple calls of the API are required to teardown a complete interrupt connection between source and destination which contains multiple hops.


Message: TISCI_MSG_RM_IRQ_RELEASE
Request: tisci_msg_rm_irq_release_req

Parameters
reqPointer to interrupt peripheral release payload
timeoutGives a sense of how long to wait for the operation. Refer SystemP_Timeout.
Returns
SystemP_SUCCESS on success, else failure

◆ Sciclient_rmRingCfg()

int32_t Sciclient_rmRingCfg ( const struct tisci_msg_rm_ring_cfg_req req,
const struct tisci_msg_rm_ring_cfg_resp resp,
uint32_t  timeout 
)

Configures a Navigator Subsystem ring.

Configures the non-real-time registers of a Navigator Subsystem ring. The ring index must be assigned to the host defined in the TISCI header via the RM board configuration resource assignment range list.


Message: TISCI_MSG_RM_RING_CFG
Request: tisci_msg_rm_ring_cfg_req
Response: tisci_msg_rm_ring_cfg_resp

Parameters
reqPointer to Ring Accelerator configure payload
respPointer to Ring Accelerator configure response payload
timeoutGives a sense of how long to wait for the operation. Refer SystemP_Timeout.
Returns
SystemP_SUCCESS on success, else failure

◆ Sciclient_rmUdmapGcfgCfg()

int32_t Sciclient_rmUdmapGcfgCfg ( const struct tisci_msg_rm_udmap_gcfg_cfg_req req,
const struct tisci_msg_rm_udmap_gcfg_cfg_resp resp,
uint32_t  timeout 
)

Configures Navigator Subsystem UDMAP GCFG region.

Configures a Navigator Subsystem UDMAP global configuration region. Configures the non-real-time registers of a Navigator Subsystem UDMAP global configuration region. The register fields specified as valid for programming must be assigned to the host defined in the TISCI header via the RM board configuration resource assignment array.


Message: TISCI_MSG_RM_UDMAP_GCFG_CFG
Request: tisci_msg_rm_udmap_gcfg_cfg_req
Response: tisci_msg_rm_udmap_gcfg_cfg_resp

Parameters
reqPointer to UDMAP GCFG configure payload
respPointer to UDMAP GCFG configure response payload
timeoutGives a sense of how long to wait for the operation. Refer SystemP_Timeout.
Returns
SystemP_SUCCESS on success, else failure

◆ Sciclient_rmUdmapTxChCfg()

int32_t Sciclient_rmUdmapTxChCfg ( const struct tisci_msg_rm_udmap_tx_ch_cfg_req req,
const struct tisci_msg_rm_udmap_tx_ch_cfg_resp resp,
uint32_t  timeout 
)

Configures a Navigator Subsystem UDMAP transmit channel.

Configures the non-real-time registers of a Navigator Subsystem UDMAP transmit channel. The channel index must be assigned to the host defined in the TISCI header via the RM board configuration resource assignment range list.


Message: TISCI_MSG_RM_UDMAP_TX_CH_CFG
Request: tisci_msg_rm_udmap_tx_ch_cfg_req
Response: tisci_msg_rm_udmap_tx_ch_cfg_resp

Parameters
reqPointer to UDMAP Tx channel configure payload
respPointer to UDMAP Tx channel configure response payload
timeoutGives a sense of how long to wait for the operation. Refer SystemP_Timeout.
Returns
SystemP_SUCCESS on success, else failure

◆ Sciclient_rmUdmapRxChCfg()

int32_t Sciclient_rmUdmapRxChCfg ( const struct tisci_msg_rm_udmap_rx_ch_cfg_req req,
const struct tisci_msg_rm_udmap_rx_ch_cfg_resp resp,
uint32_t  timeout 
)

Configures a Navigator Subsystem UDMAP receive channel.

Configures the non-real-time registers of a Navigator Subsystem UDMAP receive channel. The channel index must be assigned to the host defined in the TISCI header via the RM board configuration resource assignment range list.


Message: TISCI_MSG_RM_UDMAP_RX_CH_CFG
Request: tisci_msg_rm_udmap_rx_ch_cfg_req
Response: tisci_msg_rm_udmap_rx_ch_cfg_resp

Parameters
reqPointer to UDMAP Rx channel configure payload
respPointer to UDMAP Rx channel configure response payload
timeoutGives a sense of how long to wait for the operation. Refer SystemP_Timeout.
Returns
SystemP_SUCCESS on success, else failure

◆ Sciclient_rmUdmapFlowCfg()

int32_t Sciclient_rmUdmapFlowCfg ( const struct tisci_msg_rm_udmap_flow_cfg_req req,
const struct tisci_msg_rm_udmap_flow_cfg_resp resp,
uint32_t  timeout 
)

Configures a Navigator Subsystem UDMAP receive flow.

Configures a Navigator Subsystem UDMAP receive flow's registers. Configuration does not include the flow registers which handle size-based free descriptor queue routing. The tisci_msg_rm_udmap_flow_size_thresh_cfg_req message is used to configure register fields related to size based free descriptor queues.

The flow index must be assigned to the host defined in the TISCI header via the RM board configuration resource assignment range list.

It's the user's responsibility to make sure any receive channels using the flow are disabled when changing the receive flow configuration. Otherwise, unknown operation may occur.


Message: TISCI_MSG_RM_UDMAP_FLOW_CFG
Request: tisci_msg_rm_udmap_flow_cfg_req
Response: tisci_msg_rm_udmap_flow_cfg_resp

Parameters
reqPointer to UDMAP Rx flow configure payload
respPointer to UDMAP Rx flow configure response payload
timeoutGives a sense of how long to wait for the operation. Refer SystemP_Timeout.
Returns
SystemP_SUCCESS on success, else failure

◆ Sciclient_rmUdmapFlowSizeThreshCfg()

int32_t Sciclient_rmUdmapFlowSizeThreshCfg ( const struct tisci_msg_rm_udmap_flow_size_thresh_cfg_req req,
const struct tisci_msg_rm_udmap_flow_size_thresh_cfg_resp resp,
uint32_t  timeout 
)

Configures a Navigator Subsystem UDMAP receive flow's size threshold fields.

Configures a Navigator Subsystem UDMAP receive flow's size threshold fields

The flow index must be assigned to the host defined in the TISCI header via the RM board configuration resource assignment range list.

It's the user's responsibility to make sure any receive channels using the flow are disabled when changing the receive flow configuration. Otherwise, unknown operation may occur.


Message: TISCI_MSG_RM_UDMAP_FLOW_SIZE_THRESH_CFG
Request: tisci_msg_rm_udmap_flow_size_thresh_cfg_req
Response: tisci_msg_rm_udmap_flow_size_thresh_cfg_resp

Parameters
reqPointer to UDMAP Rx flow size threshold based free queue routing configure payload
respPointer to UDMAP Rx flow size threshold based free queue routing configure response payload
timeoutGives a sense of how long to wait for the operation. Refer SystemP_Timeout.
Returns
SystemP_SUCCESS on success, else failure

◆ Sciclient_rmPsilPair()

int32_t Sciclient_rmPsilPair ( const struct tisci_msg_rm_psil_pair_req req,
uint32_t  timeout 
)

Pairs a PSI-L source thread and destination threads.

Pairs a PSI-L source thread to a PSI-L destination thread. The pairing occurs only if both threads are unpaired at the time of the pairing request. The source thread's width and credit count parameters are set to the destination thread's capabilities. Both the source and destination threads are non-real-time enabled on successful pairing.

The PSI-L configuration proxy used to pair the source and destination threads is based on the Navigator Subsystem specified by tisci_msg_rm_psil_pair_req::nav_id


Message: TISCI_MSG_RM_PSIL_PAIR
Request: tisci_msg_rm_psil_pair_req

Parameters
reqPointer to PSI-L thread pair payload
timeoutGives a sense of how long to wait for the operation. Refer SystemP_Timeout.
Returns
SystemP_SUCCESS on success, else failure

◆ Sciclient_rmPsilUnpair()

int32_t Sciclient_rmPsilUnpair ( const struct tisci_msg_rm_psil_unpair_req req,
uint32_t  timeout 
)

Unpairs a PSI-L source thread and destination thread.

Unpairs a PSI-L source thread from a PSI-L destination thread. The source thread's width and credit count parameters are cleared. Both the source and destination threads are non-real-time disabled on successful unpairing.


Message: TISCI_MSG_RM_PSIL_UNPAIR
Request: tisci_msg_rm_psil_unpair_req

Parameters
reqPointer to PSI-L thread unpair payload
timeoutGives a sense of how long to wait for the operation. Refer SystemP_Timeout.
Returns
SystemP_SUCCESS on success, else failure

◆ Sciclient_rmPsilRead()

int32_t Sciclient_rmPsilRead ( const struct tisci_msg_rm_psil_read_req req,
struct tisci_msg_rm_psil_read_resp resp,
uint32_t  timeout 
)

Reads a PSI-L thread real-time register.

Reads the specified thread real-time configuration register from a specified PSI-L thread using the PSI-L configuration proxy.


Message: TISCI_MSG_RM_PSIL_READ
Request: tisci_msg_rm_psil_read_req

Parameters
reqPointer to PSI-L thread read payload
respPointer to PSI-L thread read response payload
timeoutGives a sense of how long to wait for the operation. Refer SystemP_Timeout.
Returns
SystemP_SUCCESS on success, else failure

◆ Sciclient_rmPsilWrite()

int32_t Sciclient_rmPsilWrite ( const struct tisci_msg_rm_psil_write_req req,
uint32_t  timeout 
)

Writes a PSI-L thread real-time register.

Writes the specified thread real-time configuration register to a specified PSI-L thread using the PSI-L configuration proxy.


Message: TISCI_MSG_RM_PSIL_WRITE
Request: tisci_msg_rm_psil_write_req

Parameters
reqPointer to PSI-L thread write payload
timeoutGives a sense of how long to wait for the operation. Refer SystemP_Timeout.
Returns
SystemP_SUCCESS on success, else failure

◆ Sciclient_rmIrOutpIsFree()

int32_t Sciclient_rmIrOutpIsFree ( uint16_t  id,
uint16_t  outp 
)

Checks the output's control register to see if the output line has an input line mapped to it.

Parameters
idTISCI Device ID of the interrupt router. Some possible values are :
                   TISCI_DEV_CMP_EVENT_INTROUTER0
                   TISCI_DEV_MAIN_GPIOMUX_INTROUTER0
                   TISCI_DEV_WKUP_MCU_GPIOMUX_INTROUTER0
                   TISCI_DEV_TIMESYNC_EVENT_ROUTER0
outpOutput line of the interrupt router. Check TRM for number of output pins of the interrupt router
Returns
SystemP_SUCCESS on success, else failure