AM62Px MCU+ SDK  09.02.01
APIs for MPU for ARMv7 (ARM R5, ARM M4)

Introduction

For more details and example usage, see MPU for ARMv7 (ARM R5, ARM M4)

Data Structures

struct  MpuP_RegionAttrs
 Attribute's to apply for a MPU region. More...
 
struct  MpuP_RegionConfig
 Region config structure, this used by SysConfig and not to be used by end-users directly. More...
 
struct  MpuP_Config
 MPU config structure, this used by SysConfig and not to be used by end-users directly. More...
 

Functions

void MpuP_RegionAttrs_init (MpuP_RegionAttrs *region)
 Set default values to MpuP_RegionAttrs. More...
 
void MpuP_setRegion (uint32_t regionNum, void *addr, uint32_t size, MpuP_RegionAttrs *attrs)
 Setup a region in the MPU. More...
 
void MpuP_resetRegion (uint32_t regionNum)
 Reset a region in the MPU. More...
 
void MpuP_enable (void)
 Enable MPU sub-system using the region that are setup using MpuP_setRegion. More...
 
void MpuP_disable (void)
 Disable MPU sub-system. More...
 
uint32_t MpuP_isEnable (void)
 Check if MPU sub-system is enabled. More...
 
void MpuP_init (void)
 Initialize MPU sub-system, called by SysConfig, not to be called by end users. More...
 

Enumerations

enum  MpuP_AccessPerm {
  MpuP_AP_ALL_BLOCK = (0x0u), MpuP_AP_S_RW = (0x1u), MpuP_AP_S_RW_U_R = (0x2u), MpuP_AP_ALL_RW = (0x3u),
  MpuP_AP_S_R = (0x5u), MpuP_AP_ALL_R = (0x6u)
}
 Enum's to represent different types of access permissions that are possible for a given MPU region. More...
 
enum  MpuP_RegionSize {
  MpuP_RegionSize_32 = 0x4, MpuP_RegionSize_64, MpuP_RegionSize_128, MpuP_RegionSize_256,
  MpuP_RegionSize_512, MpuP_RegionSize_1K, MpuP_RegionSize_2K, MpuP_RegionSize_4K,
  MpuP_RegionSize_8K, MpuP_RegionSize_16K, MpuP_RegionSize_32K, MpuP_RegionSize_64K,
  MpuP_RegionSize_128K, MpuP_RegionSize_256K, MpuP_RegionSize_512K, MpuP_RegionSize_1M,
  MpuP_RegionSize_2M, MpuP_RegionSize_4M, MpuP_RegionSize_8M, MpuP_RegionSize_16M,
  MpuP_RegionSize_32M, MpuP_RegionSize_64M, MpuP_RegionSize_128M, MpuP_RegionSize_256M,
  MpuP_RegionSize_512M, MpuP_RegionSize_1G, MpuP_RegionSize_2G, MpuP_RegionSize_4G
}
 Enum's to represent different possible MPU region size. More...
 

Enumeration Type Documentation

◆ MpuP_AccessPerm

Enum's to represent different types of access permissions that are possible for a given MPU region.

Enumerator
MpuP_AP_ALL_BLOCK 

All accesses are blocked

MpuP_AP_S_RW 

Only RD+WR supervisor mode accesses are allowed

MpuP_AP_S_RW_U_R 

RD+WR supervisor and RD only user mode accesses are allowed

MpuP_AP_ALL_RW 

All RD+WR accesses are allowed

MpuP_AP_S_R 

Only RD supervisor mode accesses are allowed

MpuP_AP_ALL_R 

All RD accesses are allowed

◆ MpuP_RegionSize

Enum's to represent different possible MPU region size.

Enumerator
MpuP_RegionSize_32 
MpuP_RegionSize_64 
MpuP_RegionSize_128 
MpuP_RegionSize_256 
MpuP_RegionSize_512 
MpuP_RegionSize_1K 
MpuP_RegionSize_2K 
MpuP_RegionSize_4K 
MpuP_RegionSize_8K 
MpuP_RegionSize_16K 
MpuP_RegionSize_32K 
MpuP_RegionSize_64K 
MpuP_RegionSize_128K 
MpuP_RegionSize_256K 
MpuP_RegionSize_512K 
MpuP_RegionSize_1M 
MpuP_RegionSize_2M 
MpuP_RegionSize_4M 
MpuP_RegionSize_8M 
MpuP_RegionSize_16M 
MpuP_RegionSize_32M 
MpuP_RegionSize_64M 
MpuP_RegionSize_128M 
MpuP_RegionSize_256M 
MpuP_RegionSize_512M 
MpuP_RegionSize_1G 
MpuP_RegionSize_2G 
MpuP_RegionSize_4G 

Function Documentation

◆ MpuP_RegionAttrs_init()

void MpuP_RegionAttrs_init ( MpuP_RegionAttrs region)

Set default values to MpuP_RegionAttrs.

Strongly recommended to be called before seting values in MpuP_RegionAttrs

Parameters
region[out] parameter structure to set to default

◆ MpuP_setRegion()

void MpuP_setRegion ( uint32_t  regionNum,
void *  addr,
uint32_t  size,
MpuP_RegionAttrs attrs 
)

Setup a region in the MPU.

Note
Refer to ARMv7-R or ARMv7-M architecture manual for more details
Recommended to disable MPU and disable cache before setting up MPU regions
Parameters
regionNum[in] region to setup
addr[in] region start address, MUST aligned to region size
size[in] region size, see MpuP_RegionSize
attrs[in] region attrs, see MpuP_RegionAttrs

◆ MpuP_resetRegion()

void MpuP_resetRegion ( uint32_t  regionNum)

Reset a region in the MPU.

Note
Refer to ARMv7-R or ARMv7-M architecture manual for more details
Parameters
regionNum[in] region to reset

◆ MpuP_enable()

void MpuP_enable ( void  )

Enable MPU sub-system using the region that are setup using MpuP_setRegion.

◆ MpuP_disable()

void MpuP_disable ( void  )

Disable MPU sub-system.

◆ MpuP_isEnable()

uint32_t MpuP_isEnable ( void  )

Check if MPU sub-system is enabled.

Returns
0: MPU sub-system is disabled, 1: MPU sub-system is enabled

◆ MpuP_init()

void MpuP_init ( void  )

Initialize MPU sub-system, called by SysConfig, not to be called by end users.