AM62Px MCU+ SDK  12.00.00

Introduction

This module contains APIs to program and use the PMU module. The APIs can be used by other drivers to get access to PMU and also by application to initiate data transfer operation.

Files

file  pmu.h
 PMU Driver API/interface file.
 

Data Structures

struct  PMU_EventCfg
 Data structure used in PMU_Config. More...
 
struct  PMU_Config
 Data structure to be used with PMU_init. More...
 

Functions

int32_t PMU_init (PMU_Config *cfg)
 Function to initialize the PMU for profiling. More...
 
int32_t PMU_profileStart (const char *name)
 Function to start profiling with the current configuration. More...
 
int32_t PMU_profileEnd (const char *name)
 Function to end profiling with the current configuration. More...
 
void PMU_profilePrintEntry (const char *name)
 Function to print the profiling stats for a particular profiling point. More...
 
void PMU_profilePrint (void)
 Function to print the profiling stats for all the points done till now. More...
 

Function Documentation

◆ PMU_init()

int32_t PMU_init ( PMU_Config cfg)

Function to initialize the PMU for profiling.

Parameters
cfgPMU_Config
Returns
SystemP_SUCCESS if command read was successful; else error on failure

◆ PMU_profileStart()

int32_t PMU_profileStart ( const char *  name)

Function to start profiling with the current configuration.

Parameters
nameName of the profile point. Should be a const char *
Returns
SystemP_SUCCESS if command read was successful; else error on failure

◆ PMU_profileEnd()

int32_t PMU_profileEnd ( const char *  name)

Function to end profiling with the current configuration.

Make sure that a PMU_profileStart is called with the same name before this is invoked.

Parameters
nameName of the profile point. Should be a const char *
Returns
SystemP_SUCCESS if command read was successful; else error on failure

◆ PMU_profilePrintEntry()

void PMU_profilePrintEntry ( const char *  name)

Function to print the profiling stats for a particular profiling point.

This has to be called after PMU_profileEnd is called for the point

Parameters
nameName of the profile point. Should be a const char *

◆ PMU_profilePrint()

void PMU_profilePrint ( void  )

Function to print the profiling stats for all the points done till now.

This has to be called after PMU_profileEnd is called for at least one point.