These are FVID2 IOCTLs that can be called by the application.
◆ FVID2_SET_FORMAT
Control command used by Fvid2_setFormat()
- Parameters
-
- Returns
- FVID2_SOK on success, else failure.
◆ FVID2_GET_FORMAT
Control command used by Fvid2_getFormat()
- Parameters
-
- Returns
- FVID2_SOK on success, else failure.
◆ FVID2_START
Control command used by Fvid2_start()
- Parameters
-
cmdArgs | [IN] Driver specific |
cmdStatusArgs | [OUT] NULL |
- Returns
- FVID2_SOK on success, else failure.
◆ FVID2_STOP
Control command used by Fvid2_stop()
- Parameters
-
cmdArgs | [IN] Driver specific |
cmdStatusArgs | [OUT] NULL |
- Returns
- FVID2_SOK on success, else failure.
◆ FVID2_REGISTER_TIMESTAMP_FXN
Register an application function (pointer) for getting the time stamp value used at the frame completion time.
The same IOCTL could be used to un-register the existing time stamp function by passing NULL to the function pointer.
- Parameters
-
- Returns
- FVID2_SOK on success, else failure.