AM62Px MCU+ SDK  12.00.00

Introduction

This module contains APIs to program and use the Panel module on the board like HDMI Panel connected over a bridge. See PANEL for more details.

Data Structures

struct  Panel_BridgeParams
 Bridge configuration parameters. More...
 
struct  Panel_vidOutputParams
 Configuration paramters for bridge encoder. More...
 
struct  Panel_PinConfig
 Panel pin control data. More...
 
struct  Panel_PinCtrl
 Configuration paramters for panel pin control. More...
 
struct  Panel_Params
 Parameters passed during Panel_open() More...
 
struct  Panel_Fxns
 Driver implementation callbacks. More...
 
struct  Panel_Config
 Panel driver configuration, these are filled by SysCfg based on the panel device that is selected. More...
 

Functions

Panel_Handle Panel_open (uint32_t instanceId, Panel_Params *params)
 Open panel driver. More...
 
void Panel_close (Panel_Handle handle)
 Close panel driver. More...
 
Panel_Handle Panel_getHandle (uint32_t instanceId)
 Get handle to panel driver. More...
 
int32_t Panel_control (Panel_Handle handle, uint32_t cmd, void *cmdArgs)
 Control Panel operation using panel specific commands. More...
 
int32_t Panel_reset (Panel_Handle handle)
 Do a reset of the panel. More...
 
uint32_t Panel_getPanelInterfaceIndex (uint32_t panelType)
 Return panel index based on type of panel. More...
 
void Panel_init (void)
 This function initializes the Panel module. More...
 
void Panel_deinit (void)
 This function de-initializes the Panel module. More...
 

Typedefs

typedef void * Panel_Handle
 Handle to the FLash driver returned by Panel_open() More...
 
typedef struct Panel_Config_s Panel_Config
 Forward declaration of Panel_Config. More...
 
typedef struct Panel_Params_s Panel_Params
 Forward declaration of Panel_Params. More...
 

Macros

#define PANEL_INVALID_VALUE   (0xFFFFFFFFU)
 
#define PANEL_MAX_NUM_PINS_CTRL   (0xAU)
 Max number pins configured for panel pin control. More...
 
#define CONFIG_PANEL_TYPE_I2C   (0x00U)
 Panel type supported. More...
 
#define CONFIG_PANEL_TYPE_DSI   (0x01U)
 
#define CONFIG_PANEL_TYPE_INVALID   (0xFFU)
 

Panel driver implementation callbacks

typedef int32_t(* Panel_OpenFxn) (Panel_Config *config, Panel_Params *params)
 Driver implementation to open a specific panel driver. More...
 
typedef void(* Panel_CloseFxn) (Panel_Config *config, Panel_Params *params)
 Driver implementation to close a specific panel driver. More...
 
typedef int32_t(* Panel_ControlFxn) (Panel_Config *config, Panel_Params *params, uint32_t cmd, void *cmdArgs)
 Driver implementation to control panel using a specific panel driver. More...
 
typedef int32_t(* Panel_ResetFxn) (Panel_Config *config, Panel_Params *params)
 Driver implementation to soft reset the panel. More...
 

Macro Definition Documentation

◆ PANEL_INVALID_VALUE

#define PANEL_INVALID_VALUE   (0xFFFFFFFFU)

◆ CONFIG_PANEL_TYPE_I2C

#define CONFIG_PANEL_TYPE_I2C   (0x00U)

Panel type supported.

◆ CONFIG_PANEL_TYPE_DSI

#define CONFIG_PANEL_TYPE_DSI   (0x01U)

◆ CONFIG_PANEL_TYPE_INVALID

#define CONFIG_PANEL_TYPE_INVALID   (0xFFU)

◆ PANEL_MAX_NUM_PINS_CTRL

#define PANEL_MAX_NUM_PINS_CTRL   (0xAU)

Max number pins configured for panel pin control.

Typedef Documentation

◆ Panel_Handle

typedef void* Panel_Handle

Handle to the FLash driver returned by Panel_open()

◆ Panel_Config

typedef struct Panel_Config_s Panel_Config

Forward declaration of Panel_Config.

◆ Panel_Params

typedef struct Panel_Params_s Panel_Params

Forward declaration of Panel_Params.

◆ Panel_OpenFxn

typedef int32_t(* Panel_OpenFxn) (Panel_Config *config, Panel_Params *params)

Driver implementation to open a specific panel driver.

Typically this callback is hidden from the end application and is implemented when a new type of panel device needs to be implemented.

Parameters
config[in] Panel configuration for the specific panel device
params[in] User controllable parameters when opening the panel device
Returns
SystemP_SUCCESS on success, else failure

◆ Panel_CloseFxn

typedef void(* Panel_CloseFxn) (Panel_Config *config, Panel_Params *params)

Driver implementation to close a specific panel driver.

Typically this callback is hidden from the end application and is implemented when a new type of panel device needs to be implemented.

Parameters
config[in] Panel configuration for the specific panel device.
params[in] User controllable parameters when opening the panel device.
Returns
SystemP_SUCCESS on success, else failure.

◆ Panel_ControlFxn

typedef int32_t(* Panel_ControlFxn) (Panel_Config *config, Panel_Params *params, uint32_t cmd, void *cmdArgs)

Driver implementation to control panel using a specific panel driver.

Typically this callback is hidden from the end application and is implemented when a new type of panel device needs to be implemented.

Parameters
config[in] Panel configuration for the specific panel device.
params[in] User controllable parameters.
cmd[in] Specific command to panel control.
cmdArgs[in] Pointer to arguments associated with command.
Returns
SystemP_SUCCESS on success, else failure

◆ Panel_ResetFxn

typedef int32_t(* Panel_ResetFxn) (Panel_Config *config, Panel_Params *params)

Driver implementation to soft reset the panel.

Typically this callback is hidden from the end application and is implemented when a new type of panel device needs to be implemented.

Parameters
config[in] Panel configuration for the specific panel device.
params[in] User controllable parameters when opening the panel device.
Returns
SystemP_SUCCESS on success, else failure.

Function Documentation

◆ Panel_open()

Panel_Handle Panel_open ( uint32_t  instanceId,
Panel_Params params 
)

Open panel driver.

Global variables Panel_Config gPanelConfig[] and uint32_t gPanelConfigNum is instantiated by SysCfg to describe the panel configuration based on user selection in SysCfg.

Parameters
instanceId[in] Index within Panel_Config gPanelConfig[] denoting the panel driver to open.
params[in] Open parameters.
Returns
Handle to panel driver which should be used in subsequent API call.
NULL in case of failure.

◆ Panel_close()

void Panel_close ( Panel_Handle  handle)

Close panel driver.

Parameters
handle[in] Panel driver handle from Panel_open.

◆ Panel_getHandle()

Panel_Handle Panel_getHandle ( uint32_t  instanceId)

Get handle to panel driver.

Parameters
instanceId[in] Index within Panel_Config gPanelConfig[].
Returns
Handle to panel driver.
NULL in case of failure.

◆ Panel_control()

int32_t Panel_control ( Panel_Handle  handle,
uint32_t  cmd,
void *  cmdArgs 
)

Control Panel operation using panel specific commands.

Commands can be refered from specific panel interface layer.

Parameters
handle[in] Panel driver handle from Panel_open.
cmd[in] Input command to control panel.
cmdArgs[in] Pointer to command arguments.
Returns
SystemP_SUCCESS on success, else failure.

◆ Panel_reset()

int32_t Panel_reset ( Panel_Handle  handle)

Do a reset of the panel.

Parameters
handle[in] Panel driver handle from Panel_open.
Returns
SystemP_SUCCESS on success, else failure.

◆ Panel_getPanelInterfaceIndex()

uint32_t Panel_getPanelInterfaceIndex ( uint32_t  panelType)

Return panel index based on type of panel.

Parameters
panelType[in] Panel type.
Returns
Panel driver instance index corresponding to the panel type.

◆ Panel_init()

void Panel_init ( void  )

This function initializes the Panel module.

◆ Panel_deinit()

void Panel_deinit ( void  )

This function de-initializes the Panel module.