AM62Px MCU+ SDK  12.00.00
Release Notes 12.00.00

Attention
Also refer to individual module pages for more details on each feature, unsupported features, important usage guidelines.
Note
The examples will show usage of SW modules and APIs on a specific CPU instance and OS combination.
Unless explicitly noted otherwise, the SW modules would work in both FreeRTOS and no-RTOS environment.

Device and Validation Information

SOC Supported CPUs EVM Host PC
AM62P MCU R5F, WKUP R5F SK-AM62P-LP EVM (referred to as am62px-sk in code) Windows 10 64b or Ubuntu 22.04 64b

Features Added in This Release

Note
Update of OSPI tuning algorithm on this SDK causes increase in tuning time. Refer OSPI NOR Flash Performance
Feature Module
PADCFG drive strength adjustment through SYSCFG Pinmux
LBIST/PBIST initiated in SBL EMMC SBL
Enable WKUP-R5F ATCM SBL
Watchdog support for DM R5/WKUP-R5F WDT
Save/Restore of FPU registers on context switch enabled by default on A53 FreeRTOS
MMCSD drive strength as a configurable option MMCSD
Add 8S-8S-8S protocol support OSPI
Route SecProxy event for MCU cores DM
Interrupt mode in SCIClient SCI Client
Move task stack allocation to application layer SCI Server
Add WFI in MCU only mode to save power LPM

Experimental Features

Attention
Features listed below are early versions and should be considered as "experimental".
Users can evaluate the feature, however the feature is not fully tested at TI side.
TI would not support these feature on public e2e.
Experimental features will be enabled with limited examples and SW modules.
Feature Module
Ethernet traffic sharing accross multiple cores, called Ethernet Firmware Networking
C++ SUpport NA

Dependent Tools and Compiler Information

Attention
It is recommended to use the TIFS version provided with the release for ensuring compatibility between TIFS and device manager. Using the TIFS from different MCU+SDK release is not recommended and may cause TIFS/ DM functionality to break.
Tools/Components Supported CPUs Version
Code Composer Studio MCU-R5F, WKUP-R5F 20.3.1
SysConfig MCU-R5F, WKUP-R5F 1.24.2, build 4234
TI ARM CLANG MCU-R5F, WKUP-R5F 4.0.1.LTS
GCC AARCH64 A53 9.2-2019.12
FreeRTOS Kernel MCU-R5F, WKUP-R5F 11.1.0

SDK Components

SYSFW / TIFS

Version 12.00.02
Release Notes LINK
User Guide LINK

Key Features

OS Kernel

OS Supported CPUs SysConfig Support
FreeRTOS Kernel MCU-R5F, WKUP-R5F NA
FreeRTOS POSIX MCU-R5F NA
No RTOS MCU-R5F, WKUP-R5F NA

Driver Porting Layer (DPL)

Module Supported CPUs SysConfig Support OS support
Address Translate MCU-R5F, WKUP-R5F Yes FreeRTOS, NORTOS
Cache MCU-R5F, WKUP-R5F Yes FreeRTOS, NORTOS
Clock MCU-R5F, WKUP-R5F Yes FreeRTOS, NORTOS
CycleCounter MCU-R5F, WKUP-R5F NA FreeRTOS, NORTOS
Debug MCU-R5F, WKUP-R5F Yes FreeRTOS, NORTOS
Heap MCU-R5F, WKUP-R5F NA FreeRTOS, NORTOS
Hwi MCU-R5F, WKUP-R5F Yes FreeRTOS, NORTOS
MPU MCU-R5F, WKUP-R5F Yes FreeRTOS, NORTOS
Semaphore MCU-R5F, WKUP-R5F NA FreeRTOS, NORTOS
Task MCU-R5F, WKUP-R5F NA FreeRTOS
Timer MCU-R5F, WKUP-R5F Yes FreeRTOS, NORTOS

Secondary Bootloader (SBL)

SBL Mode Supported CPUs SysConfig Support PHY Support DMA Support OS support
OSPI NOR WKUP-R5F Yes Yes Yes NORTOS
EMMC WKUP-R5F Yes NA NA NORTOS
UART WKUP-R5F Yes NA No NORTOS

SDL

SDL Module Supported CPUs SysConfig Support
MCRC MCU-R5F No
ESM MCU-R5F No
VTM MCU-R5F No
DCC MCU-R5F No
ECC MCU-R5F No
RTI MCU-R5F No
POK MCU-R5F No
STOG MCU-R5F No
MTOG MCU-R5F No
PBIST MCU-R5F No
LBIST MCU-R5F No
ROM_CHECKSUM MCU-R5F No

Networking

Module Supported CPUs SysConfig Support OS Support Key features tested Key features not tested
TSN WKUP-R5F NO FreeRTOS gPTP IEEE 802.1 AS-2020 compliant gPTP stack, End Nodes and Bridge mode support, YANG data model configuration Multi-Clock Domain
LwIP WKUP-R5F YES FreeRTOS TCP/UDP IP networking stack with and without checksum offload enabled, TCP/UDP IP networking stack with server and client functionality, basic Socket APIs, netconn APIs and raw APIs, DHCP, ping, TCP iperf, scatter-gather, DSCP priority mapping, LwIP bridge, shared memory driver Other LwIP features
Ethernet driver (ENET) WKUP-R5F YES FreeRTOS Ethernet as port using CPSW, MAC loopback and PHY loopback, Layer 2 MAC, Packet Timestamping, CPSW Switch, Policer and Classifier, MDIO Manual Mode, CBS (IEEE 802.1Qav) on CPSW, IET (IEEE 802.1Qbu) on CPSW, Strapped PHY (Early Ethernet), cut through switch on CPSW RMII mode

SOC Device Drivers

Note
See the updated MCASP usage guidelines in MCASP for changes in MCASP driver
Peripheral Domain Supported CPUs SysConfig Support
DDR Main WKUP-R5F Yes
ECAP Main MCU-R5F Yes
EPWM Main MCU-R5F, WKUP-R5F Yes
DSS Main WKUP-R5F Yes
GPIO MCU MCU-R5F, WKUP-R5F Yes
Main MCU-R5F, WKUP-R5F Yes
I2C Main MCU-R5F, WKUP-R5F Yes
MCU MCU-R5F, WKUP-R5F Yes
Wakeup MCU-R5F, WKUP-R5F Yes
IPC Main MCU-R5F, WKUP-R5F Yes
MCAN MCU MCU-R5F Yes
Wakeup WKUP-R5F Yes
MCASP Main WKUP-R5F Yes
MCSPI Main MCU-R5F, WKUP-R5F Yes
MCU MCU-R5F, WKUP-R5F Yes
MMCSD Main WKUP-R5F, MCU-R5F Yes
OSPI Main WKUP-R5F Yes
Pinmux Main MCU-R5F, WKUP-R5F Yes
MCU MCU-R5F, WKUP-R5F Yes
Wakeup MCU-R5F, WKUP-R5F Yes
PMU Wakeup WKUP-R5F Yes
SOC NA MCU-R5F, WKUP-R5F Yes
SCIClient NA MCU-R5F, WKUP-R5F Yes
RTC MCU MCU-R5F Yes
Wakeup WKUP-R5F Yes
UART Main MCU-R5F, WKUP-R5F Yes
MCU MCU-R5F, WKUP-R5F Yes
Wakeup WKUP-R5F Yes
UDMA MCU MCU-R5F Yes
Wakeup WKUP-R5F Yes
WDT Wakeup WKUP-R5F Yes

Board Device Drivers

Peripheral Supported CPUs SysConfig Support
EEPROM MCU-R5F, WKUP-R5F Yes
Ethernet PHY WKUP-R5F Yes
Flash WKUP-R5F Yes
LED MCU-R5F, WKUP-R5F Yes
PMIC MCU-R5F Yes

Fixed Issues

ID Head Line Module
EXT_SITMPUSW-245 MCU+ SDK LPDDR4 Driver starts DDR Training/Leveling Sequence twice DDR
EXT_SITMPUSW-293 Sciclient driver uses incorrect context for the TISCI_MSG_KEYRING_IMPORT DM
EXT_SITMPUSW-309 LPM: Spurious wake up on MCU only mode DM
EXT_SITMPUSW-312 Incorrect context description of SCICLIENT_CONTEXT_DM2TIFS DM
EXT_SITMPUSW-288 LPM: Unable to enter LPM in Interrupt Mode DM
EXT_SITMPUSW-302 Compilation Errors when disabling DebugP logs. DPL
EXT_SITMPUSW-251 MCU+ SDK Example Projects using incorrect ARMv7 MPU Attributes for Peripheral Register Region Examples
EXT_SITMPUSW-301 OSPI_norFlashInit1s1s1s has an implementation of wait for 500 milliseconds instead of microseconds Flash
EXT_SITMPUSW-282 Sysconfig not generating code for GPIO Trigger GPIO
EXT_SITMPUSW-279 I2C close is not working properly during error conditions I2C
EXT_SITMPUSW-310 Incorrect handling of the timeout for the CMD6 command MMCSD
EXT_SITMPUSW-114 MMCSD_enableBootPartition implements two mutually exclusive concepts as one function MMCSD
EXT_SITMPUSW-295 Flash Close Logic Requires OSPI Handle to be reset to 1S-1S-1S OSPI
EXT_SITMPUSW-280 OSPI Indac Mode Should Check for odd bytes OSPI
EXT_SITMPUSW-256 Incorrect calculation of rowColEnd in the ext_otp_writeMmr OTP
EXT_SITMPUSW-292 Bootloader_socOpenFirewalls is called before System_init in the SBLs SBL
EXT_SITMPUSW-214 WDT: Hang due to no valid argument check in APIs Watchdog
EXT_EP-13267 SDL ESM: Wrong instance argument in SDL_ESM_loInterruptHandler causing misidentification of ESM0 interrupts SDL-ESM

Known Issues

ID Head Line Module
EXT_SITMPUSW-153 MCU+ SDK CCS Project Build Generates Invalid/Redundant Boot Image Files Build
EXT_SITMPUSW-28 Outstanding mailbox messages prevent suspend IPC
EXT_SITMPUSW-259 eMMC retuning may be attempted during the initialization sequence MMCSD
EXT_SITMPUSW-222 MMCSD field Card Type is not ordered logically in the Sysconfig MMCSD
EXT_SITMPUSW-135 RTC Test application failing intermittently. RTC
EXT_SITMPUSW-220 SBL_SD bootloaders report incorrect boot image size SBL
EXT_SITMPUSW-324 UART_udmaIsrTx does not handles continuous Callbacks properly UART
EXT_SITMPUSW-258 WKUP UART0 is not working in CallBack mode UART
EXT_EP-12276 ECC: Firewall related aggregators failures SDL-ECC
EXT_EP-12277 AM62Px: ECC: SDL_MCAN1_MCANSS_MSGMEM_WRAP_ECC_AGGR aggregator is failing SDL-ECC
EXT_EP-12279 CSI RX ECC aggregators are failing on AM62P/AM62X SDL-ECC
EXT_EP-13265 MCU R5 ECC Aggr init fails when MCU LBIST is enabled in bootloader SDL-LBIST
EXT_EP-12280 Running MCU LBIST on SBL causes JTAG connection issues to MCU R5F SDL-LBIST

Limitations

S.No Head Line Module
1 The ROM startup model for runtime initializations in TI ARM CLANG is not supported/tested in the SDK NA
2 LPM is not supported with SBL boot flow. It is supported only with SPL boot flow. Bootloader
3 The EVM is limited to only one MAC address in the EEPROM, applications requiring multiple MAC addresses should enable and configure manual MAC address entry in Sysconfig. Networking

Upgrade and Compatibility Information

This section lists changes which could affect user applications developed using older SDK versions. Read this carefully to see if you need to do any changes in your existing application when migrating to this SDK version relative to previous SDK version. Also refer to older SDK version release notes to see changes in earlier SDKs.

The below table captures the list of migration document sections when migrating from one version to another. The migration for a partcluar module will be applicable, if you are migrating from older version listed to newer version listed on the table below.

Module Migration guide Older version Newer version
Bootloader Bootloader Migration Guidelines<= 10.01.00 >= 11.00.00
NETWORKING Version Updates from earlier SDKs to Latest<= 11.01.00 >= 11.02.00
OSPI OSPI Migration Guide<= 11.01.00 >= 11.02.00
SCI Server Migration Guide 11.02 to 12.00<= 11.02.00 >= 12.00.00
SBL Linker Migration Guide 11.02 to 12.00<= 11.02.00 >= 12.00.00

Networking

Module Affected API Change
TSN notify_linkchange notify_linkchange function is renamed to cb_lld_notify_linkchange, include path <tsn_combase/tilld/cb_lld_ethernet.h> in the file that uses cb_lld_notify_linkchange.