AM62Px MCU+ SDK  09.02.01

Detailed Description

Configuration for doing safety checks.

Data Fields

uint32_t safetyChkEnable
 
uint32_t safetyChkMode
 
uint32_t seedSelectEnable
 
uint32_t thresholdValue
 
uint32_t frameSkip
 
Fvid2_PosConfig regionPos
 
Fvid2_SizeConfig regionSize
 

Field Documentation

◆ safetyChkEnable

uint32_t CSL_DssSafetyChkCfg::safetyChkEnable

Safety check Enable for the region FALSE: Disable Safety Check TRUE: Enable Safety Check

◆ safetyChkMode

uint32_t CSL_DssSafetyChkCfg::safetyChkMode

Mode of operation of the safety check module For valid values see CSL_DssSafetyChkMode

◆ seedSelectEnable

uint32_t CSL_DssSafetyChkCfg::seedSelectEnable

Initial seed selection control FALSE: Initial seed is always 0xFFFFFFFF TRUE: Initial seed is defined by SAFETY_LFSR_SEED

◆ thresholdValue

uint32_t CSL_DssSafetyChkCfg::thresholdValue

Allowed maximum number of frames with the same frame signature. When the freeze frame counter reaches thresholdValue+1, a freeze frame detection will occur

◆ frameSkip

uint32_t CSL_DssSafetyChkCfg::frameSkip

Indicates which frames to be skipped while doing safety checks For valid values see CSL_DssSafetyChkFrameSkip

◆ regionPos

Fvid2_PosConfig CSL_DssSafetyChkCfg::regionPos

Position of the safety region described using Fvid2_PosConfig

startX:
X position of the layer The first pixel on the left of the screen has the X-position 0

startY:
Y position of the layer The first pixel at the top has the Y-position 0

◆ regionSize

Fvid2_SizeConfig CSL_DssSafetyChkCfg::regionSize

Size of the safety region described using Fvid2_SizeConfig

width:
Width of the safety region One pixel wide region has value of 0

height:
Height of the safety region One pixel height region has value of 0