For more details and example usage, see MPU for ARMv7 (ARM R5, ARM M4)
Data Structures | |
struct | MpuP_RegionAttrs |
Attribute's to apply for a MPU region. More... | |
struct | MpuP_RegionConfig |
Region config structure, this used by SysConfig and not to be used by end-users directly. More... | |
struct | MpuP_Config |
MPU config structure, this used by SysConfig and not to be used by end-users directly. More... | |
Functions | |
void | MpuP_RegionAttrs_init (MpuP_RegionAttrs *region) |
Set default values to MpuP_RegionAttrs. More... | |
void | MpuP_setRegion (uint32_t regionNum, void *addr, uint32_t size, MpuP_RegionAttrs *attrs) |
Setup a region in the MPU. More... | |
void | MpuP_resetRegion (uint32_t regionNum) |
Reset a region in the MPU. More... | |
void | MpuP_enable (void) |
Enable MPU sub-system using the region that are setup using MpuP_setRegion. More... | |
void | MpuP_disable (void) |
Disable MPU sub-system. More... | |
uint32_t | MpuP_isEnable (void) |
Check if MPU sub-system is enabled. More... | |
void | MpuP_init (void) |
Initialize MPU sub-system, called by SysConfig, not to be called by end users. More... | |
Enumerations | |
enum | MpuP_AccessPerm { MpuP_AP_ALL_BLOCK = (0x0u), MpuP_AP_S_RW = (0x1u), MpuP_AP_S_RW_U_R = (0x2u), MpuP_AP_ALL_RW = (0x3u), MpuP_AP_S_R = (0x5u), MpuP_AP_ALL_R = (0x6u) } |
Enum's to represent different types of access permissions that are possible for a given MPU region. More... | |
enum | MpuP_RegionSize { MpuP_RegionSize_32 = 0x4, MpuP_RegionSize_64, MpuP_RegionSize_128, MpuP_RegionSize_256, MpuP_RegionSize_512, MpuP_RegionSize_1K, MpuP_RegionSize_2K, MpuP_RegionSize_4K, MpuP_RegionSize_8K, MpuP_RegionSize_16K, MpuP_RegionSize_32K, MpuP_RegionSize_64K, MpuP_RegionSize_128K, MpuP_RegionSize_256K, MpuP_RegionSize_512K, MpuP_RegionSize_1M, MpuP_RegionSize_2M, MpuP_RegionSize_4M, MpuP_RegionSize_8M, MpuP_RegionSize_16M, MpuP_RegionSize_32M, MpuP_RegionSize_64M, MpuP_RegionSize_128M, MpuP_RegionSize_256M, MpuP_RegionSize_512M, MpuP_RegionSize_1G, MpuP_RegionSize_2G, MpuP_RegionSize_4G } |
Enum's to represent different possible MPU region size. More... | |
enum MpuP_AccessPerm |
Enum's to represent different types of access permissions that are possible for a given MPU region.
enum MpuP_RegionSize |
Enum's to represent different possible MPU region size.
void MpuP_RegionAttrs_init | ( | MpuP_RegionAttrs * | region | ) |
Set default values to MpuP_RegionAttrs.
Strongly recommended to be called before seting values in MpuP_RegionAttrs
region | [out] parameter structure to set to default |
void MpuP_setRegion | ( | uint32_t | regionNum, |
void * | addr, | ||
uint32_t | size, | ||
MpuP_RegionAttrs * | attrs | ||
) |
Setup a region in the MPU.
regionNum | [in] region to setup |
addr | [in] region start address, MUST aligned to region size |
size | [in] region size, see MpuP_RegionSize |
attrs | [in] region attrs, see MpuP_RegionAttrs |
void MpuP_resetRegion | ( | uint32_t | regionNum | ) |
Reset a region in the MPU.
regionNum | [in] region to reset |
void MpuP_enable | ( | void | ) |
Enable MPU sub-system using the region that are setup using MpuP_setRegion.
void MpuP_disable | ( | void | ) |
Disable MPU sub-system.
uint32_t MpuP_isEnable | ( | void | ) |
Check if MPU sub-system is enabled.
void MpuP_init | ( | void | ) |
Initialize MPU sub-system, called by SysConfig, not to be called by end users.