AM62Px MCU+ SDK  09.02.00
Generic NOR Flash API for single pin mode

Introduction

These APIs try to communicate with whichever flash is connected the OSPI peripheral in 1-1-1 mode. This can be used in bringing up new flashes and mostly used for debug and diagnostic purposes

Functions

int32_t OSPI_norFlashInit1s1s1s (OSPI_Handle handle)
 This function initializes the NOR flash to work in 1-1-1 mode. More...
 
void OSPI_norFlashSetCmds (uint8_t rdCmd, uint8_t wrCmd, uint8_t eraseCmd)
 This function sets up internal bookkeeping variables for read, write and erase commands. This API has to be called immediately before OSPI_norFlashInit1s1s1s. More...
 
int32_t OSPI_norFlashReadId (OSPI_Handle handle, uint32_t *manufacturerId, uint32_t *deviceId)
 This function tries to read the JEDEC ID from the NOR flash connected to the OSPI peripheral. More...
 
int32_t OSPI_norFlashWrite (OSPI_Handle handle, uint32_t offset, uint8_t *buf, uint32_t len)
 This function writes data to the flash at a specified offset. More...
 
int32_t OSPI_norFlashRead (OSPI_Handle handle, uint32_t offset, uint8_t *buf, uint32_t len)
 This function reads data from the flash from a specified offset. More...
 
int32_t OSPI_norFlashReadSfdp (OSPI_Handle handle, uint32_t offset, uint8_t *buf, uint32_t len)
 This function reads SFDP table from the flash from a specified offset. More...
 
int32_t OSPI_norFlashErase (OSPI_Handle handle, uint32_t address)
 This function erases 1 block of data starting from a provided address. More...
 

Function Documentation

◆ OSPI_norFlashInit1s1s1s()

int32_t OSPI_norFlashInit1s1s1s ( OSPI_Handle  handle)

This function initializes the NOR flash to work in 1-1-1 mode.

Precondition
OSPI controller has been opened using OSPI_open()
Parameters
handleAn OSPI_Handle returned from an OSPI_open()
Returns
SystemP_SUCCESS on success, SystemP_FAILURE otherwise

◆ OSPI_norFlashSetCmds()

void OSPI_norFlashSetCmds ( uint8_t  rdCmd,
uint8_t  wrCmd,
uint8_t  eraseCmd 
)

This function sets up internal bookkeeping variables for read, write and erase commands. This API has to be called immediately before OSPI_norFlashInit1s1s1s.

Precondition
OSPI controller has been opened using OSPI_open()
Parameters
rdCmdCommand to be used in single mode read
wrCmdCommand to be used in single mode write/page program
eraseCmdCommand to be used to erase (block or sector)

◆ OSPI_norFlashReadId()

int32_t OSPI_norFlashReadId ( OSPI_Handle  handle,
uint32_t *  manufacturerId,
uint32_t *  deviceId 
)

This function tries to read the JEDEC ID from the NOR flash connected to the OSPI peripheral.

Precondition
OSPI controller has been opened using OSPI_open()
Parameters
handleAn OSPI_Handle returned from an OSPI_open()
manufacturerIdPointer to a uint32_t variable. This will be filled with the manufacturer ID on success
deviceIdPointer to a uint32_t variable. This will be filled with the device ID on success
Returns
SystemP_SUCCESS on success, SystemP_FAILURE otherwise

◆ OSPI_norFlashWrite()

int32_t OSPI_norFlashWrite ( OSPI_Handle  handle,
uint32_t  offset,
uint8_t *  buf,
uint32_t  len 
)

This function writes data to the flash at a specified offset.

Precondition
OSPI controller has been opened using OSPI_open()
Parameters
handleAn OSPI_Handle returned from an OSPI_open()
offsetOffset at which the data is to be written
bufBuffer which has the data to be written to the flash
lenNumber of bytes to be written to the flash
Returns
SystemP_SUCCESS on success, SystemP_FAILURE otherwise

◆ OSPI_norFlashRead()

int32_t OSPI_norFlashRead ( OSPI_Handle  handle,
uint32_t  offset,
uint8_t *  buf,
uint32_t  len 
)

This function reads data from the flash from a specified offset.

Precondition
OSPI controller has been opened using OSPI_open()
Parameters
handleAn OSPI_Handle returned from an OSPI_open()
offsetOffset at which the data is to be read from
bufBuffer to which data will be written into
lenNumber of bytes to be read from the flash
Returns
SystemP_SUCCESS on success, SystemP_FAILURE otherwise

◆ OSPI_norFlashReadSfdp()

int32_t OSPI_norFlashReadSfdp ( OSPI_Handle  handle,
uint32_t  offset,
uint8_t *  buf,
uint32_t  len 
)

This function reads SFDP table from the flash from a specified offset.

Precondition
OSPI controller has been opened using OSPI_open()
Parameters
handleAn OSPI_Handle returned from an OSPI_open()
offsetOffset at which the data is to be read from
bufBuffer to which data will be written into
lenNumber of bytes to be read from the flash
Returns
SystemP_SUCCESS on success, SystemP_FAILURE otherwise

◆ OSPI_norFlashErase()

int32_t OSPI_norFlashErase ( OSPI_Handle  handle,
uint32_t  address 
)

This function erases 1 block of data starting from a provided address.

Precondition
OSPI controller has been opened using OSPI_open()
Parameters
handleAn OSPI_Handle returned from an OSPI_open()
addressAddress of the data block to be erased. This address should be block aligned.
Returns
SystemP_SUCCESS on success, SystemP_FAILURE otherwise