AM62Px MCU+ SDK  09.02.00

Introduction

DSS Video Pipe layer interface file.

Go to the source code of this file.

Data Structures

struct  CSL_DssVidPipeCfg
 Configuration for DSS Video Pipe. More...
 
struct  CSL_DssVidPipeDmaCfg
 DSS Video Pipe DMA related Config parameters. More...
 
struct  CSL_DssVidPipeLumaCfg
 DSS Video Pipe Luma Key Config parameters. More...
 
struct  CSL_DssVidPipeAlphaCfg
 DSS Video Pipe Alpha Config parameters. More...
 
struct  CSL_DssVidPipeVC1Cfg
 DSS Video Pipe VC1 configuration. More...
 
struct  CSL_DssVidPipeMFlagCfg
 DSS Video Pipe MFLAG Config parameters. More...
 

Macros

DSS Video Pipe YUV Alignment

DSS Video Pipe alignment for unpacked YUV data

#define CSL_DSS_VID_PIPE_YUV_ALIGN_LSB    ((uint32_t) CSL_DSS_VID_ATTRIBUTES2_YUV_ALIGN_VAL_LSB)
 Data is LSB aligned (MSB unused) More...
 
#define CSL_DSS_VID_PIPE_YUV_ALIGN_MSB    ((uint32_t) CSL_DSS_VID_ATTRIBUTES2_YUV_ALIGN_VAL_MSB)
 Data is MSB aligned (LSB unused) More...
 
DSS Video Pipe Scaler Value

#define CSL_DSS_VID_PIPE_SC_DISABLED    ((uint32_t) CSL_DSS_VID_ATTRIBUTES_RESIZEENABLE_VAL_RESIZEPROC)
 Scaler is disabled. More...
 
#define CSL_DSS_VID_PIPE_SC_ENABLED_H    ((uint32_t) CSL_DSS_VID_ATTRIBUTES_RESIZEENABLE_VAL_HRESIZE)
 Horizontal scaling is enabled. More...
 
#define CSL_DSS_VID_PIPE_SC_ENABLED_V    ((uint32_t) CSL_DSS_VID_ATTRIBUTES_RESIZEENABLE_VAL_VRESIZE)
 Vertical scaling is enabled. More...
 
#define CSL_DSS_VID_PIPE_SC_ENABLED_HV    ((uint32_t) CSL_DSS_VID_ATTRIBUTES_RESIZEENABLE_VAL_HVRESIZE)
 Both horizontal and vertical scaling is enabled. More...
 
DSS Video Pipe Preload Control Value

DSS Video Pipe Preload Value can be fixed HW value or SW determined

#define CSL_DSS_VID_PIPE_PRELOAD_CONTROL_SW    ((uint32_t) CSL_DSS_VID_ATTRIBUTES_BUFPRELOAD_VAL_DEFVAL)
 Value is defined by preload register. More...
 
#define CSL_DSS_VID_PIPE_PRELOAD_CONTROL_HW    ((uint32_t) CSL_DSS_VID_ATTRIBUTES_BUFPRELOAD_VAL_HIGHTHRES)
 HW pre-fetches pixels up to high threshold value. More...
 
DSS Video Pipe Priority Value

#define CSL_DSS_VID_PIPE_PRIORITY_NORMAL    ((uint32_t) CSL_DSS_VID_ATTRIBUTES_ARBITRATION_VAL_NORMALPRIO)
 Priority of video pipeline is normal. More...
 
#define CSL_DSS_VID_PIPE_PRIORITY_HIGH    ((uint32_t) CSL_DSS_VID_ATTRIBUTES_ARBITRATION_VAL_HIGHPRIO)
 Priority of video pipeline is high. More...
 
DSS Video Pipe Self Refresh Mode Control

#define CSL_DSS_VID_PIPE_REFRESH_CONTROL_SW    ((uint32_t) CSL_DSS_VID_ATTRIBUTES_SELFREFRESHAUTO_VAL_SELFREFRESHAUTODIS)
 Transition is controlled by SW. More...
 
#define CSL_DSS_VID_PIPE_REFRESH_CONTROL_HW    ((uint32_t) CSL_DSS_VID_ATTRIBUTES_SELFREFRESHAUTO_VAL_SELFREFRESHAUTOEN)
 Transition is controlled by HW. More...
 

Typedefs

typedef CSL_dss_vidRegs CSL_dss_pipeRegs
 DSS Video Pipe Registers. More...
 

Functions

int32_t CSL_dssVidPipeSetConfig (CSL_dss_pipeRegs *pipeRegs, const CSL_DssVidPipeCfg *pipeCfg, const CSL_DssVidPipeVC1Cfg *vc1Cfg)
 Configure the Video Pipe. More...
 
void CSL_dssVidPipeSetDmaConfig (CSL_dss_pipeRegs *pipeRegs, const CSL_DssVidPipeDmaCfg *dmaCfg)
 Configure the Video Pipe DMA parameters. More...
 
void CSL_dssVidPipeEnableTransparency (CSL_dss_pipeRegs *pipeRegs, const CSL_DssVidPipeLumaCfg *lumaCfg)
 Enable the Luma Key transparency matching and set luma params. More...
 
void CSL_dssVidPipeSetAlphaConfig (CSL_dss_pipeRegs *pipeRegs, const CSL_DssVidPipeAlphaCfg *alphaCfg)
 Set DSS Video Pipe Alpha parameters. More...
 
void CSL_dssVidPipeSetCSCCoeff (CSL_dss_pipeRegs *pipeRegs, const CSL_DssCscCoeff *coeff)
 Configure the coefficients for Color Space Conversion. More...
 
void CSL_dssVidPipeSetBuffAddr (CSL_dss_pipeRegs *pipeRegs, uint32_t field, uint64_t baseAddrRGBY, uint64_t baseAddrUV)
 Set the video buffer address. More...
 
void CSL_dssVidPipeEnable (CSL_dss_pipeRegs *pipeRegs, uint32_t enable)
 Enable the DSS Video Pipe. More...
 
void CSL_dssVidPipeSetSafetySignSeedVal (CSL_dss_pipeRegs *pipeRegs, uint32_t signSeedVal)
 Set the seed value for the signature calculation. More...
 
void CSL_dssVidPipeSetSafetyReferenceSign (CSL_dss_pipeRegs *pipeRegs, uint32_t referenceSign)
 Set the reference safety signature for data correctness check. More...
 
void CSL_dssVidPipeSetSafetyChkConfig (CSL_dss_pipeRegs *pipeRegs, const CSL_DssSafetyChkCfg *safetyCfg)
 Configure the Safety Check Params. More...
 
uint32_t CSL_dssVidPipeGetSafetySign (const CSL_dss_pipeRegs *pipeRegs)
 Get the Safety Signature. More...
 
void CSL_dssVidPipeSetMflagConfig (CSL_dss_pipeRegs *pipeRegs, const CSL_DssVidPipeMFlagCfg *mflagCfg)
 Set the MFLAG configuration. More...
 
static void CSL_dssVidPipeCfgInit (CSL_DssVidPipeCfg *pipeCfg)
 CSL_DssVidPipeCfg structure init function. More...
 
static void CSL_dssVidPipeDmaCfgInit (CSL_DssVidPipeDmaCfg *dmaCfg)
 CSL_DssVidPipeDmaCfg structure init function. More...
 
static void CSL_dssVidPipeLumaCfgInit (CSL_DssVidPipeLumaCfg *lumaCfg)
 CSL_DssVidPipeLumaCfg structure init function. More...
 
static void CSL_dssVidPipeAlphaCfgInit (CSL_DssVidPipeAlphaCfg *alphaCfg)
 CSL_DssVidPipeAlphaCfg structure init function. More...
 
static void CSL_dssVidPipeVC1CfgInit (CSL_DssVidPipeVC1Cfg *vc1Cfg)
 CSL_DssVidPipeVC1Cfg structure init function. More...
 
static void CSL_dssVidPipeMFlagCfgInit (CSL_DssVidPipeMFlagCfg *mflagCfg)
 CSL_DssVidPipeMFlagCfg structure init function. More...