AM62Px MCU+ SDK  09.01.00
Fvid2_EdgeCropConfig Struct Reference

Detailed Description

Structure containing edge crop configuration - used in DSS.

struct Fvid2_EdgeCropConfig

A frame has four edges: top, bottom, left and right. User can decide to crop in any direction. cropTop will be used to remove the particular number of lines from the top of the frame. Similarly other fields will be used.

Data Fields

uint32_t cropTop
 
uint32_t cropBottom
 
uint32_t cropLeft
 
uint32_t cropRight
 

Field Documentation

◆ cropTop

uint32_t Fvid2_EdgeCropConfig::cropTop

Crop Top Edge in Lines

◆ cropBottom

uint32_t Fvid2_EdgeCropConfig::cropBottom

Crop Bottom Edge in Lines

◆ cropLeft

uint32_t Fvid2_EdgeCropConfig::cropLeft

Crop Left Edge in Pixels

◆ cropRight

uint32_t Fvid2_EdgeCropConfig::cropRight

Crop Right Edge in Pixels