AM62Px MCU+ SDK  09.01.00
Dss_DctrlLcdBlankTimingParams Struct Reference

Detailed Description

Structure containing LCD Blank Timing Configuration. This structure is used as an argument to IOCTL_DSS_DCTRL_SET_LCD_BLANK_TIMING_PARAMS.

Data Fields

uint32_t vpId
 
uint32_t dvoFormat
 
CSL_DssVpLcdBlankTimingCfg lcdBlankTimingCfg
 

Field Documentation

◆ vpId

uint32_t Dss_DctrlLcdBlankTimingParams::vpId

Video Port Id. See CSL_DssVpId for values

◆ dvoFormat

uint32_t Dss_DctrlLcdBlankTimingParams::dvoFormat

Digital output format. For valid values see Fvid2_DVFormat

◆ lcdBlankTimingCfg

CSL_DssVpLcdBlankTimingCfg Dss_DctrlLcdBlankTimingParams::lcdBlankTimingCfg

Timing configuration for the LCD. See CSL_DssVpLcdBlankTimingCfg for details