AM62Px MCU+ SDK  09.01.00

Introduction

DMSC controls the power management, security and resource management of the device.

Data Structures

struct  tisci_msg_rm_irq_set_req
 Configures peripherals within the interrupt subsystem according to the valid configuration provided. The following tisci_msg_rm_irq_set_req::valid_params valid bit combinations are allowed: Interrupt Router Mux Configuration - Configures an IR input to output mux connection where the IR input is the src_index and the IR output is the dst_host_irq. Both the src_id and the dst_id must be the device ID of the IR being configured. tisci_msg_rm_irq_set_req::dst_id valid bit == STRUE tisci_msg_rm_irq_set_req::dst_host_irq valid bit == STRUE tisci_msg_rm_irq_set_req::ia_id valid bit == SFALSE tisci_msg_rm_irq_set_req::vint valid bit == SFALSE tisci_msg_rm_irq_set_req::global_event valid bit == SFALSE tisci_msg_rm_irq_set_req::vint_status_bit_index valid bit == SFALSE Event to VINT Mapping Only - Configure peripheral OES register and add an event mapping to an IA VINT tisci_msg_rm_irq_set_req::dst_id valid bit == SFALSE tisci_msg_rm_irq_set_req::dst_host_irq valid bit == SFALSE tisci_msg_rm_irq_set_req::ia_id valid bit == STRUE tisci_msg_rm_irq_set_req::vint valid bit == STRUE tisci_msg_rm_irq_set_req::global_event valid bit == STRUE tisci_msg_rm_irq_set_req::vint_status_bit_index valid bit == STRUE OES Register Programming Only - Only programs the OES register of the source. Useful for setting UDMAP trigger events and any other events that are not translated to the interrupt domain: tisci_msg_rm_irq_set_req::dst_id valid bit == SFALSE tisci_msg_rm_irq_set_req::dst_host_irq valid bit == SFALSE tisci_msg_rm_irq_set_req::ia_id valid bit == SFALSE tisci_msg_rm_irq_set_req::vint valid bit == SFALSE tisci_msg_rm_irq_set_req::global_event valid bit == STRUE tisci_msg_rm_irq_set_req::vint_status_bit_index valid bit == SFALSE. More...
 
struct  tisci_msg_rm_irq_set_resp
 Response to setting a peripheral to processor interrupt. More...
 
struct  tisci_msg_rm_irq_release_req
 Releases interrupt peripheral resources according to the valid configuration provided. The following tisci_msg_rm_irq_release_req::valid_params valid bit combinations are allowed: Interrupt Router Mux Release - Release an IR input to output mux connection where the IR input is the src_index and the IR output is the dst_host_irq. Both the src_id and the dst_id must be the device ID of the IR being configured. tisci_msg_rm_irq_release_req::dst_id valid bit == STRUE tisci_msg_rm_irq_release_req::dst_host_irq valid bit == STRUE tisci_msg_rm_irq_release_req::ia_id valid bit == SFALSE tisci_msg_rm_irq_release_req::vint valid bit == SFALSE tisci_msg_rm_irq_release_req::global_event valid bit == SFALSE tisci_msg_rm_irq_release_req::vint_status_bit_index valid bit == SFALSE Event to VINT Unmap Only - Clear only peripheral OES register and event to VINT status bit mapping tisci_msg_rm_irq_release_req::dst_id valid bit == SFALSE tisci_msg_rm_irq_release_req::dst_host_irq valid bit == SFALSE tisci_msg_rm_irq_release_req::ia_id valid bit == STRUE tisci_msg_rm_irq_release_req::vint valid bit == STRUE tisci_msg_rm_irq_release_req::global_event valid bit == STRUE tisci_msg_rm_irq_release_req::vint_status_bit_index valid bit == STRUE OES Register Programming Only - Only clears the OES register of the source. Useful for clearing UDMAP trigger events and any other events that are not translated to the interrupt domain: tisci_msg_rm_irq_release_req::dst_id valid bit == SFALSE tisci_msg_rm_irq_release_req::dst_host_irq valid bit == SFALSE tisci_msg_rm_irq_release_req::ia_id valid bit == SFALSE tisci_msg_rm_irq_release_req::vint valid bit == SFALSE tisci_msg_rm_irq_release_req::global_event valid bit == STRUE tisci_msg_rm_irq_release_req::vint_status_bit_index valid bit == SFALSE. More...
 
struct  tisci_msg_rm_irq_release_resp
 Response to releasing a peripheral to processor interrupt. More...
 

Functions

struct tisci_msg_rm_irq_set_req __attribute__ ((__packed__))
 

Macros

#define TISCI_MSG_VALUE_RM_DST_ID_VALID   (1u << 0u)
 This file contains: More...
 
#define TISCI_MSG_VALUE_RM_DST_HOST_IRQ_VALID   (1u << 1u)
 
#define TISCI_MSG_VALUE_RM_IA_ID_VALID   (1u << 2u)
 
#define TISCI_MSG_VALUE_RM_VINT_VALID   (1u << 3u)
 
#define TISCI_MSG_VALUE_RM_GLOBAL_EVENT_VALID   (1u << 4u)
 
#define TISCI_MSG_VALUE_RM_VINT_STATUS_BIT_INDEX_VALID   (1u << 5u)
 

Macro Definition Documentation

◆ TISCI_MSG_VALUE_RM_DST_ID_VALID

#define TISCI_MSG_VALUE_RM_DST_ID_VALID   (1u << 0u)

This file contains:

    WARNING!!: Autogenerated file from SYSFW. DO NOT MODIFY!!

System Firmware TISCI RM IRQ Messaging

TISCI Protocol Definitions for RM IRQ messages The dst_id parameter is valid for any RM IRQ TISCI message modifying interrupt routers.

◆ TISCI_MSG_VALUE_RM_DST_HOST_IRQ_VALID

#define TISCI_MSG_VALUE_RM_DST_HOST_IRQ_VALID   (1u << 1u)

The dst_host_irq parameter is valid for any RM IRQ TISCI message modifying interrupt routers.

◆ TISCI_MSG_VALUE_RM_IA_ID_VALID

#define TISCI_MSG_VALUE_RM_IA_ID_VALID   (1u << 2u)

The ia_id parameter is valid for any RM IRQ TISCI message modifying routes through an interrupt aggregator virtual interrupt.

◆ TISCI_MSG_VALUE_RM_VINT_VALID

#define TISCI_MSG_VALUE_RM_VINT_VALID   (1u << 3u)

The vint parameter is valid for any RM IRQ TISCI message modifying routes through an interrupt aggregator virtual interrupt.

◆ TISCI_MSG_VALUE_RM_GLOBAL_EVENT_VALID

#define TISCI_MSG_VALUE_RM_GLOBAL_EVENT_VALID   (1u << 4u)

The global_event parameter is valid for any RM IRQ TISCI message modifying routes through an interrupt aggregator virtual interrupt.

◆ TISCI_MSG_VALUE_RM_VINT_STATUS_BIT_INDEX_VALID

#define TISCI_MSG_VALUE_RM_VINT_STATUS_BIT_INDEX_VALID   (1u << 5u)

The vint_status_bit_index parameter is valid for any RM IRQ TISCI message modifying routes through an interrupt aggregator virtual interrupt.

Function Documentation

◆ __attribute__()

struct tisci_msg_rm_irq_set_req __attribute__ ( (__packed__)  )