This is DSS documentation specific to AM62px SoC
|
struct | Dss_IrqParams |
| Structure containing DSS interrupt information. Events should be enabled only for available Video Ports and Video Pipes. More...
|
|
struct | Dss_RmInfo |
| Structure containing resources manager information. This enables display sharing between two different softwares. More...
|
|
struct | Dss_SocParams |
| DSS SOC parameters. More...
|
|
struct | Dss_DctrlOldiParams |
| Structure containing OLDI configuration. This structure is used as an argument to IOCTL_DSS_DCTRL_SET_OLDI_PARAMS. More...
|
|
|
#define | DSS_DCTRL_MAX_NODES ((uint32_t) 9U) |
| Defines maximum number of nodes for allocation including invalid node. More...
|
|
#define | DSS_DCTRL_MAX_EDGES ((uint32_t) 8U) |
| Defines maximum number of edges for allocation. This is derived by looking at all possible DSS connections in the SoC. More...
|
|
#define | DSS_FUNC_IRQ_DEFAULT_NUM (CSLR_WKUP_R5FSS0_CORE0_INTR_DSS0_DISPC_INTR_REQ_0_0) |
|
◆ DSS_DCTRL_INST_0
#define DSS_DCTRL_INST_0 (0U) |
Display controller instance 0.
◆ DSS_DCTRL_INST_MAX
#define DSS_DCTRL_INST_MAX (1U) |
Maximum number of display driver instances.
◆ DSS_DISP_INST_VID1
Video 1 Pipeline display driver instance number.
◆ DSS_DISP_INST_VIDL1
Video Lite 1 Pipeline display driver instance number.
◆ DSS_DISP_INST_MAX
Maximum number of display driver instances.
◆ DSS_DISP_INST_INVALIUD
Maximum number of display driver instances.
◆ DSS_DCTRL_NODE_TYPE_INVALID
#define DSS_DCTRL_NODE_TYPE_INVALID ((uint32_t) 0x0U) |
◆ DSS_DCTRL_NODE_TYPE_PIPE
#define DSS_DCTRL_NODE_TYPE_PIPE ((uint32_t) 0x1U) |
◆ DSS_DCTRL_NODE_TYPE_OVERLAY
#define DSS_DCTRL_NODE_TYPE_OVERLAY ((uint32_t) 0x2U) |
◆ DSS_DCTRL_NODE_TYPE_VP
#define DSS_DCTRL_NODE_TYPE_VP ((uint32_t) 0x3U) |
◆ DSS_DCTRL_NODE_TYPE_OUTPUT
#define DSS_DCTRL_NODE_TYPE_OUTPUT ((uint32_t) 0x4U) |
◆ DSS_DCTRL_NODE_INVALID
#define DSS_DCTRL_NODE_INVALID ((uint32_t) 0x0U) |
◆ DSS_DCTRL_NODE_VID1
#define DSS_DCTRL_NODE_VID1 ((uint32_t) 0x1U) |
◆ DSS_DCTRL_NODE_VIDL1
#define DSS_DCTRL_NODE_VIDL1 ((uint32_t) 0x2U) |
◆ DSS_DCTRL_NODE_OVR1
#define DSS_DCTRL_NODE_OVR1 ((uint32_t) 0x3U) |
◆ DSS_DCTRL_NODE_OVR2
#define DSS_DCTRL_NODE_OVR2 ((uint32_t) 0x4U) |
◆ DSS_DCTRL_NODE_VP1
#define DSS_DCTRL_NODE_VP1 ((uint32_t) 0x5U) |
◆ DSS_DCTRL_NODE_VP2
#define DSS_DCTRL_NODE_VP2 ((uint32_t) 0x6U) |
◆ DSS_DCTRL_NODE_OLDI
#define DSS_DCTRL_NODE_OLDI ((uint32_t) 0x7U) |
◆ DSS_DCTRL_NODE_DPI1
#define DSS_DCTRL_NODE_DPI1 ((uint32_t) 0x8U) |
◆ DSS_DCTRL_MAX_NODES
#define DSS_DCTRL_MAX_NODES ((uint32_t) 9U) |
Defines maximum number of nodes for allocation including invalid node.
◆ DSS_DCTRL_MAX_EDGES
#define DSS_DCTRL_MAX_EDGES ((uint32_t) 8U) |
Defines maximum number of edges for allocation. This is derived by looking at all possible DSS connections in the SoC.
DSS Functional Interrupt Number for R5
◆ DSS_FUNC_IRQ_DEFAULT_NUM
#define DSS_FUNC_IRQ_DEFAULT_NUM (CSLR_WKUP_R5FSS0_CORE0_INTR_DSS0_DISPC_INTR_REQ_0_0) |
◆ DSS_EVT_MGR_INST_ID_FUNC
#define DSS_EVT_MGR_INST_ID_FUNC ((uint32_t) 0x00U) |
Instance Id for functional interrupts.
<
Max Instance Id
◆ DSS_EVT_MGR_INST_ID_MAX
#define DSS_EVT_MGR_INST_ID_MAX ((uint32_t) 0x01U) |
◆ DSS_EVT_MGR_INST_ID_INVALID
#define DSS_EVT_MGR_INST_ID_INVALID ((uint32_t) 0xFFU) |
◆ Dss_dispIsVidInst()
static uint32_t Dss_dispIsVidInst |
( |
uint32_t |
instId | ) |
|
|
inlinestatic |
Check if the display driver instance is of type Video pipeline.
- Parameters
-
instId | [IN]Driver Instance Id. |
- Returns
- TRUE if instance is Video pipeline else returns FALSE.
◆ Dss_dispIsVidLInst()
static uint32_t Dss_dispIsVidLInst |
( |
uint32_t |
instId | ) |
|
|
inlinestatic |
Check if the display driver instance is of type Video lite pipeline.
- Parameters
-
instId | [IN]Driver Instance Id. |
- Returns
- TRUE if instance is Video lite pipeline else returns FALSE.
◆ Dss_irqParamsInit()
◆ Dss_rmInfoInit()
◆ Dss_socParamsInit()
◆ Dss_dctrlOldiParamsInit()
◆ Dss_setDssSoftReset()
void Dss_setDssSoftReset |
( |
| ) |
|
◆ Dss_setOLDITxPowerDown()
void Dss_setOLDITxPowerDown |
( |
uint32_t |
oldiLinkMode, |
|
|
uint32_t |
powerState |
|
) |
| |
Set OLDI Power Domain Control to power on and off OLDI TX.
- Parameters
-
oldiLinkMode | Oldi Map type. See CSL_DssVpOldiMapType for valid values |
powerState | True to switch ON, false to switch OFF |