AM62L FreeRTOS SDK  11.02.00

Introduction

UDMA Driver API/interface file.

Requirement: DOX_REQ_TAG(PDK-2494)

Go to the source code of this file.

Data Structures

struct  Udma_InitPrms
 UDMA initialization parameters. More...
 
struct  Udma_DrvObject
 Opaque UDMA driver object. More...
 

Typedefs

typedef uint64_t(* Udma_VirtToPhyFxn) (const void *virtAddr, uint32_t chNum, void *appData)
 UDMA Virtual to Physical address translation callback function. More...
 
typedef void *(* Udma_PhyToVirtFxn) (uint64_t phyAddr, uint32_t chNum, void *appData)
 UDMA Physical to Virtual address translation callback function. More...
 

Functions

int32_t Udma_init (Udma_DrvHandle drvHandle, const Udma_InitPrms *initPrms)
 UDMA init function. More...
 
int32_t Udma_deinit (Udma_DrvHandle drvHandle)
 UDMA deinit function. More...
 
int32_t UdmaInitPrms_init (uint32_t instId, Udma_InitPrms *initPrms)
 Udma_InitPrms structure init function. More...
 
uint64_t Udma_defaultVirtToPhyFxn (const void *virtAddr, uint32_t chNum, void *appData)
 Default virtual to physical translation function. More...
 
void * Udma_defaultPhyToVirtFxn (uint64_t phyAddr, uint32_t chNum, void *appData)
 Default physical to virtual translation function. More...