AM62L FreeRTOS SDK  11.02.00

Detailed Description

UDMA RX channel flow parameters.

Data Fields

Udma_ChHandle ChHandle
 
uint8_t einfoPresent
 
uint8_t psInfoPresent
 
uint8_t errorHandling
 
uint8_t descType
 
uint8_t psLocation
 
uint16_t sopOffset
 
uint16_t defaultRxCQ
 

Field Documentation

◆ ChHandle

Udma_ChHandle Udma_FlowPrms::ChHandle

[IN] TX/RX chHandle.

◆ einfoPresent

uint8_t Udma_FlowPrms::einfoPresent

[IN] Set to 1 if extended packet info is present in the descriptor

◆ psInfoPresent

uint8_t Udma_FlowPrms::psInfoPresent

[IN] Set to 1 if protocol-specific info is present in the descriptor

◆ errorHandling

uint8_t Udma_FlowPrms::errorHandling

[IN] Determines how starvation errors are handled. 0=drop packet, 1=retry

◆ descType

uint8_t Udma_FlowPrms::descType

[IN] Descriptor type

◆ psLocation

uint8_t Udma_FlowPrms::psLocation

[IN] Protocol-specific info location.

◆ sopOffset

uint16_t Udma_FlowPrms::sopOffset

[IN] Start of rx packet data (byte offset from the start of the SOP buffer)

◆ defaultRxCQ

uint16_t Udma_FlowPrms::defaultRxCQ

[IN] Rx destination queue