AM62L FreeRTOS SDK  11.02.00
SCMI_PdProtocolAttrs Struct Reference

Data Fields

int32_t status
 
uint32_t attributes
 
uint32_t statsAddrLow
 
uint32_t statsAddrHigh
 
uint32_t statsLen
 

Field Documentation

◆ status

int32_t SCMI_PdProtocolAttrs::status

SCMI command status

◆ attributes

uint32_t SCMI_PdProtocolAttrs::attributes

Protocol attributes

◆ statsAddrLow

uint32_t SCMI_PdProtocolAttrs::statsAddrLow

Lower 32 bits of address of statistics memory region

◆ statsAddrHigh

uint32_t SCMI_PdProtocolAttrs::statsAddrHigh

Higher 32 bits of address of statistics memory region

◆ statsLen

uint32_t SCMI_PdProtocolAttrs::statsLen

Length of statistics memory region