AM62L FreeRTOS SDK  11.02.00
SCMI_ClockRateGetOut Struct Reference

Data Fields

int32_t status
 
uint32_t clockRateLSB
 
uint32_t clockRateMSB
 

Field Documentation

◆ status

int32_t SCMI_ClockRateGetOut::status

SCMI command status

◆ clockRateLSB

uint32_t SCMI_ClockRateGetOut::clockRateLSB

32bit LSB of the clock rate in Hertz

◆ clockRateMSB

uint32_t SCMI_ClockRateGetOut::clockRateMSB