AM62L FreeRTOS SDK  11.02.00

Detailed Description

ICSSG statistics counters.

The statistics counters reported by PRU-ICSSG. This structure type must be used by application to retrieve ICSSG statistics via ENET_STATS_IOCTL_GET_MACPORT_STATS.

Data Fields

uint32_t rxGoodFrames
 
uint32_t rxBCastFrames
 
uint32_t rxMCastFrames
 
uint32_t rxCRCErrors
 
uint32_t rxMIIErrors
 
uint32_t rxOddNibbleFrame
 
uint32_t rxMaxSizeFrame
 
uint32_t rxMaxSizeErrFrame
 
uint32_t rxMinSizeFrame
 
uint32_t rxMinSizeErrFrame
 
uint32_t rxOverrunFrame
 
uint32_t rxClass0
 
uint32_t rxClass1
 
uint32_t rxClass2
 
uint32_t rxClass3
 
uint32_t rxClass4
 
uint32_t rxClass5
 
uint32_t rxClass6
 
uint32_t rxClass7
 
uint32_t rxClass8
 
uint32_t rxClass9
 
uint32_t rxClass10
 
uint32_t rxClass11
 
uint32_t rxClass12
 
uint32_t rxClass13
 
uint32_t rxClass14
 
uint32_t rxClass15
 
uint32_t rxSMDFragErr
 
uint32_t rxBucket1SizeConfig
 
uint32_t rxBucket2SizeConfig
 
uint32_t rxBucket3SizeConfig
 
uint32_t rxBucket4SizeConfig
 
uint32_t rx64BSizedFrame
 
uint32_t rxBucket1SizedFrame
 
uint32_t rxBucket2SizedFrame
 
uint32_t rxBucket3SizedFrame
 
uint32_t rxBucket4SizedFrame
 
uint32_t rxBucket5SizedFrame
 
uint32_t rxTotalByte
 
uint32_t rxTxTotalByte
 
uint32_t txGoodFrame
 
uint32_t txBcastFrame
 
uint32_t txMcastFrame
 
uint32_t txOddNibbleFrame
 
uint32_t txUnderFlowErr
 
uint32_t txMaxSizeFrame
 
uint32_t txMaxSizeErrFrame
 
uint32_t txMinSizeFrame
 
uint32_t txMinSizeErrFrame
 
uint32_t txBucket1SizeConfig
 
uint32_t txBucket2SizeConfig
 
uint32_t txBucket3SizeConfig
 
uint32_t txBucket4SizeConfig
 
uint32_t tx64BSizedFrame
 
uint32_t txBucket1SizedFrame
 
uint32_t txBucket2SizedFrame
 
uint32_t txBucket3SizedFrame
 
uint32_t txBucket4SizedFrame
 
uint32_t txBucket5SizedFrame
 
uint32_t txTotalByte
 

Field Documentation

◆ rxGoodFrames

uint32_t IcssgStats_MacPort::rxGoodFrames

RX Good Frame Count Inc on none min err max err crc err odd err, Wrt subtracts

◆ rxBCastFrames

uint32_t IcssgStats_MacPort::rxBCastFrames

RX BC Frame Count Inc on BC type, Wrt subtracts

◆ rxMCastFrames

uint32_t IcssgStats_MacPort::rxMCastFrames

RX MC Frame Count Inc on MC type, Wrt subtracts

◆ rxCRCErrors

uint32_t IcssgStats_MacPort::rxCRCErrors

RX CRC Err Frame Count Inc on crc err, Wrt subtracts

◆ rxMIIErrors

uint32_t IcssgStats_MacPort::rxMIIErrors

RX MII Err Frame Count Inc on mii sgmii rgmii err, Wrt subtracts

◆ rxOddNibbleFrame

uint32_t IcssgStats_MacPort::rxOddNibbleFrame

RX Odd Nibble Frame Count Inc on odd nibble mii, Wrt subtracts

◆ rxMaxSizeFrame

uint32_t IcssgStats_MacPort::rxMaxSizeFrame

RX Max Size Frame Count Limit

◆ rxMaxSizeErrFrame

uint32_t IcssgStats_MacPort::rxMaxSizeErrFrame

RX MAX Size Err Frame Count Inc if > than Limit, Wrt subtracts

◆ rxMinSizeFrame

uint32_t IcssgStats_MacPort::rxMinSizeFrame

RX Min Size Frame Limit

◆ rxMinSizeErrFrame

uint32_t IcssgStats_MacPort::rxMinSizeErrFrame

RX MIN Size Frame Count incremented if < than limit

◆ rxOverrunFrame

uint32_t IcssgStats_MacPort::rxOverrunFrame

RX L1 FIFO overflow frame count

◆ rxClass0

uint32_t IcssgStats_MacPort::rxClass0

RX Class0 Hit Count

◆ rxClass1

uint32_t IcssgStats_MacPort::rxClass1

RX Class1 Hit Count

◆ rxClass2

uint32_t IcssgStats_MacPort::rxClass2

RX Class2 Hit Count

◆ rxClass3

uint32_t IcssgStats_MacPort::rxClass3

RX Class3 Hit Count

◆ rxClass4

uint32_t IcssgStats_MacPort::rxClass4

RX Class4 Hit Count

◆ rxClass5

uint32_t IcssgStats_MacPort::rxClass5

RX Class5 Hit Count

◆ rxClass6

uint32_t IcssgStats_MacPort::rxClass6

RX Class6 Hit Count

◆ rxClass7

uint32_t IcssgStats_MacPort::rxClass7

RX Class7 Hit Count

◆ rxClass8

uint32_t IcssgStats_MacPort::rxClass8

RX Class8 Hit Count

◆ rxClass9

uint32_t IcssgStats_MacPort::rxClass9

RX Class9 Hit Count

◆ rxClass10

uint32_t IcssgStats_MacPort::rxClass10

RX Class10 Hit Count

◆ rxClass11

uint32_t IcssgStats_MacPort::rxClass11

RX Class11 Hit Count

◆ rxClass12

uint32_t IcssgStats_MacPort::rxClass12

RX Class12 Hit Count

◆ rxClass13

uint32_t IcssgStats_MacPort::rxClass13

RX Class13 Hit Count

◆ rxClass14

uint32_t IcssgStats_MacPort::rxClass14

RX Class14 Hit Count

◆ rxClass15

uint32_t IcssgStats_MacPort::rxClass15

RX Class15 Hit Count

◆ rxSMDFragErr

uint32_t IcssgStats_MacPort::rxSMDFragErr

SMD FRAG Frames Received with Errors

◆ rxBucket1SizeConfig

uint32_t IcssgStats_MacPort::rxBucket1SizeConfig

RX Bucket1 Byte Size

◆ rxBucket2SizeConfig

uint32_t IcssgStats_MacPort::rxBucket2SizeConfig

RX Bucket2 Byte Size

◆ rxBucket3SizeConfig

uint32_t IcssgStats_MacPort::rxBucket3SizeConfig

RX Bucket3 Byte Size

◆ rxBucket4SizeConfig

uint32_t IcssgStats_MacPort::rxBucket4SizeConfig

RX Bucket4 Byte Size

◆ rx64BSizedFrame

uint32_t IcssgStats_MacPort::rx64BSizedFrame

RX 64Byte Frame Count

◆ rxBucket1SizedFrame

uint32_t IcssgStats_MacPort::rxBucket1SizedFrame

RX Bucket1 Frame Count Inc if <= than Bucket1 Byte Size

◆ rxBucket2SizedFrame

uint32_t IcssgStats_MacPort::rxBucket2SizedFrame

RX Bucket2 Frame Count Inc if <= than Bucket2 Byte Size and if > than Bucket1 Byte Size

◆ rxBucket3SizedFrame

uint32_t IcssgStats_MacPort::rxBucket3SizedFrame

RX Bucket3 Frame Count Inc if <= than Bucket3 Byte Size and if > than Bucket2 Byte Size

◆ rxBucket4SizedFrame

uint32_t IcssgStats_MacPort::rxBucket4SizedFrame

RX Bucket4 Frame Count Inc if <= than Bucket4 Byte Size and if > than Bucket3 Byte Size

◆ rxBucket5SizedFrame

uint32_t IcssgStats_MacPort::rxBucket5SizedFrame

RX Bucket5 Frame Count Inc if > than Bucket4 Byte Size

◆ rxTotalByte

uint32_t IcssgStats_MacPort::rxTotalByte

RX Total Byte Count

◆ rxTxTotalByte

uint32_t IcssgStats_MacPort::rxTxTotalByte

RX and TX Total Byte Count

◆ txGoodFrame

uint32_t IcssgStats_MacPort::txGoodFrame

TX Good Frame Count Inc if no min size err max size err or mii odd nibble

◆ txBcastFrame

uint32_t IcssgStats_MacPort::txBcastFrame

TX Broadcast Frame Count Inc if BC

◆ txMcastFrame

uint32_t IcssgStats_MacPort::txMcastFrame

TX Multicast Frame Count Inc if MC

◆ txOddNibbleFrame

uint32_t IcssgStats_MacPort::txOddNibbleFrame

TX Odd Nibble Frame Count Inc if mii odd nibble

◆ txUnderFlowErr

uint32_t IcssgStats_MacPort::txUnderFlowErr

TX Max Underflow Error Count

◆ txMaxSizeFrame

uint32_t IcssgStats_MacPort::txMaxSizeFrame

TX Max Size Frame Count Limit

◆ txMaxSizeErrFrame

uint32_t IcssgStats_MacPort::txMaxSizeErrFrame

TX Max Size Err Frame Count Inc if > max Limit

◆ txMinSizeFrame

uint32_t IcssgStats_MacPort::txMinSizeFrame

TX Min Size Frame Count Limit

◆ txMinSizeErrFrame

uint32_t IcssgStats_MacPort::txMinSizeErrFrame

TX Min Size Err Frame Count Inc if < min Limit

◆ txBucket1SizeConfig

uint32_t IcssgStats_MacPort::txBucket1SizeConfig

TX Bucket1 Byte Size

◆ txBucket2SizeConfig

uint32_t IcssgStats_MacPort::txBucket2SizeConfig

TX Bucket2 Byte Size

◆ txBucket3SizeConfig

uint32_t IcssgStats_MacPort::txBucket3SizeConfig

TX Bucket3 Byte Size

◆ txBucket4SizeConfig

uint32_t IcssgStats_MacPort::txBucket4SizeConfig

TX Bucket4 Byte Size

◆ tx64BSizedFrame

uint32_t IcssgStats_MacPort::tx64BSizedFrame

TX 64Byte Frame Count Inc if 64B

◆ txBucket1SizedFrame

uint32_t IcssgStats_MacPort::txBucket1SizedFrame

TX Bucket1 Frame Count if <= than Bucket1

◆ txBucket2SizedFrame

uint32_t IcssgStats_MacPort::txBucket2SizedFrame

TX Bucket2 Frame Count if <= than Bucket2 Size and > Bucket 1 Size

◆ txBucket3SizedFrame

uint32_t IcssgStats_MacPort::txBucket3SizedFrame

TX Bucket3 Frame Count if <= than Bucket3 Size and > Bucket 2 Size

◆ txBucket4SizedFrame

uint32_t IcssgStats_MacPort::txBucket4SizedFrame

TX Bucket4 Frame Count if <= than Bucket4 Size and > Bucket 3 Size

◆ txBucket5SizedFrame

uint32_t IcssgStats_MacPort::txBucket5SizedFrame

TX Bucket5 Frame Count if > Bucket 4 Size

◆ txTotalByte

uint32_t IcssgStats_MacPort::txTotalByte

Total Bytes Sent