AM62L FreeRTOS SDK  11.02.00

Detailed Description

Holds status information regarding the source of the last data abort.

Note
Refer to ARMv7-R architecture manual for more details

Data Fields

volatile uint32_t status
 
volatile uint32_t sd
 
volatile uint32_t rw
 

Field Documentation

◆ status

volatile uint32_t DFSR::status

◆ sd

volatile uint32_t DFSR::sd

◆ rw

volatile uint32_t DFSR::rw