AM62L FreeRTOS SDK  11.02.00

Detailed Description

Input args for CPSW_ALE_IOCTL_SET_POLICER_THREADCFG command.

Configuration to set the thread/flow id associated with a classifier.

Data Fields

CpswAle_PolicerMatchParams policerMatch
 
bool threadIdEn
 
uint32_t threadId
 

Field Documentation

◆ policerMatch

CpswAle_PolicerMatchParams CpswAle_SetPolicerThreadCfgInArgs::policerMatch

Policer match config

◆ threadIdEn

bool CpswAle_SetPolicerThreadCfgInArgs::threadIdEn

Enable/disable thread id setting for this policer entry

◆ threadId

uint32_t CpswAle_SetPolicerThreadCfgInArgs::threadId

Thread Id which will be enabled for this policer match