This is UDMA driver resource manager related configuration parameters and API
|
| file | udma_rm.h |
| | UDMA RM related parameters and API.
|
| |
◆ UDMA_RM_RES_ID_INVALID
| #define UDMA_RM_RES_ID_INVALID ((uint32_t) 0xFFFF0005U) |
Macro used to specify that Resource ID is invalid.
◆ UDMA_RM_SHARED_RES_CNT_MIN
| #define UDMA_RM_SHARED_RES_CNT_MIN ((uint32_t) 0xFFFF0006U) |
Macro used to specify - reserve minimum required number of resources for an instance.
◆ UDMA_RM_SHARED_RES_CNT_REST
| #define UDMA_RM_SHARED_RES_CNT_REST ((uint32_t) 0xFFFF0007U) |
Macro used to specify - reserve all the remaining unreserved resources for an instance.