This example configures a GPIO pin connected to an LED on the EVM in output mode. The application toggles the LED on/off for 10 seconds and exits.
| Parameter | Value |
|---|---|
| CPU + OS | a53ss0-0 freertos |
| a53ss0-0 nortos | |
| Toolchain | arm.gnu.aarch64-none |
| Board | am62lx-evm |
| Example folder | examples/drivers/gpio/gpio_led_blink/ |
Shown below is a sample output when the application is run,