AM62L FreeRTOS SDK  11.02.00
GPIO

The General-Purpose Input/Output (GPIO) driver provides API to configure general-purpose pins as either inputs or outputs. It also provided API to configure GPIO to produce host CPU interrupts and DMA synchronization events in different interrupt/event generation modes.

Features Supported

  • Supports up to 16 GPIO signals per bank
  • Supports up to 9 banks of interrupt and DMA trigger capable GPIOs
  • Set/clear functionality

SysConfig Features

Note
It is strongly recommend to use SysConfig where it is available instead of using direct SW API calls. This will help simplify the SW application and also catch common mistakes early in the development cycle.
  • Set pin direction: input or output
  • Set interrupt trigger type
  • Configuring pinmux based on selected pin

Features NOT Supported

NA

Important Usage Guidelines

  • Note: Not all GPIO pins, banks are present in a particular device. Refer device TRM for actual GPIO instances and pins supported

Example Usage

Include the below file to access the APIs

#include <drivers/gpio.h>

GPIO configuration as output

uint32_t pinNum = gGpioPinNum, pinValue;
GPIO_setDirMode(gGpioBaseAddr, pinNum, GPIO_DIRECTION_OUTPUT);
GPIO_pinWriteHigh(gGpioBaseAddr, pinNum);
GPIO_pinWriteLow(gGpioBaseAddr, pinNum);
/* Check output value */
pinValue = GPIO_pinOutValueRead(gGpioBaseAddr, pinNum);
if(pinValue != GPIO_PIN_LOW)
{
}

GPIO configuration as input

uint32_t pinNum = gGpioPinNum, pinValue;
GPIO_setDirMode(gGpioBaseAddr, pinNum, GPIO_DIRECTION_INPUT);
pinValue = GPIO_pinRead(gGpioBaseAddr, pinNum);
if(pinValue == GPIO_PIN_HIGH)
{
DebugP_log("Pin value is HIGH\r\n");
}
else
{
DebugP_log("Pin value is LOW\r\n");
}

GPIO configuration for bank interrupt

static void GPIO_bankIsrFxn(void *args)
{
uint32_t pinNum = (uint32_t) args, bankNum;
uint32_t intrStatus, pinMask = GPIO_GET_BANK_BIT_MASK(pinNum);
bankNum = GPIO_GET_BANK_INDEX(pinNum);
intrStatus = GPIO_getBankIntrStatus(gGpioBaseAddr, bankNum);
GPIO_clearBankIntrStatus(gGpioBaseAddr, bankNum, intrStatus);
if(intrStatus & pinMask)
{
/*
* Handle all the expected pin interrupts within a bank using intrStatus flag
*/
}
}
void gpio_bank_interrupt_init(void)
{
int32_t retVal;
uint32_t pinNum = gGpioPinNum, bankNum;
HwiP_Params hwiPrms;
bankNum = GPIO_GET_BANK_INDEX(pinNum);
/* Interrupt setup */
GPIO_setDirMode(gGpioBaseAddr, pinNum, GPIO_DIRECTION_INPUT);
GPIO_setTrigType(gGpioBaseAddr, pinNum, GPIO_TRIG_TYPE_RISE_EDGE);
GPIO_bankIntrEnable(gGpioBaseAddr, bankNum);
/* Register bank interrupt */
HwiP_Params_init(&hwiPrms);
hwiPrms.intNum = gGpioBankIntrNum;
hwiPrms.callback = &GPIO_bankIsrFxn;
hwiPrms.args = (void *) pinNum;
retVal = HwiP_construct(&gGpioHwiObject, &hwiPrms);
if(SystemP_SUCCESS != retVal)
{
}
}
void gpio_bank_interrupt_deinit(void)
{
uint32_t pinNum = gGpioPinNum, bankNum, intrStatus;
bankNum = GPIO_GET_BANK_INDEX(pinNum);
/* Interrupt disable and clear any pending interrupts */
GPIO_bankIntrDisable(gGpioBaseAddr, bankNum);
GPIO_setTrigType(gGpioBaseAddr, pinNum, GPIO_TRIG_TYPE_NONE);
intrStatus = GPIO_getBankIntrStatus(gGpioBaseAddr, bankNum);
GPIO_clearBankIntrStatus(gGpioBaseAddr, bankNum, intrStatus);
/* Unregister interrupt */
HwiP_destruct(&gGpioHwiObject);
}

GPIO configuration for per pin interrupt

static void GPIO_pinIsrFxn(void *args)
{
/*
* Handle pin interrupt - This is pulse interrupt. No need to clear status
*/
}
void gpio_pin_interrupt_init(void)
{
int32_t retVal;
uint32_t pinNum = gGpioPinNum, bankNum;
HwiP_Params hwiPrms;
bankNum = GPIO_GET_BANK_INDEX(pinNum);
/* Interrupt setup */
GPIO_setDirMode(gGpioBaseAddr, pinNum, GPIO_DIRECTION_INPUT);
GPIO_setTrigType(gGpioBaseAddr, pinNum, GPIO_TRIG_TYPE_RISE_EDGE);
GPIO_bankIntrEnable(gGpioBaseAddr, bankNum);
/* Register pin interrupt */
HwiP_Params_init(&hwiPrms);
hwiPrms.intNum = gGpioPinIntrNum;
hwiPrms.callback = &GPIO_pinIsrFxn;
hwiPrms.args = (void *) pinNum;
retVal = HwiP_construct(&gGpioHwiObject, &hwiPrms);
if(SystemP_SUCCESS != retVal)
{
}
}
void gpio_pin_interrupt_deinit(void)
{
uint32_t pinNum = gGpioPinNum, bankNum;
bankNum = GPIO_GET_BANK_INDEX(pinNum);
/* Interrupt disable and clear any pending interrupts */
GPIO_bankIntrDisable(gGpioBaseAddr, bankNum);
GPIO_setTrigType(gGpioBaseAddr, pinNum, GPIO_TRIG_TYPE_NONE);
GPIO_clearIntrStatus(gGpioBaseAddr, pinNum);
/* Unregister interrupt */
HwiP_destruct(&gGpioHwiObject);
}

API

APIs for GPIO

GPIO_GET_BANK_BIT_MASK
#define GPIO_GET_BANK_BIT_MASK(pinNum)
Returns the bit mask within a bank based on pin number.
Definition: gpio/v0/gpio.h:136
HwiP_destruct
void HwiP_destruct(HwiP_Object *obj)
Cleanup, delete, destruct a Hwi object.
HwiP_Params
Parameters passed during HwiP_construct.
Definition: HwiP.h:74
ClockP_sleep
void ClockP_sleep(uint32_t sec)
Sleep for user specified seconds.
GPIO_PIN_LOW
#define GPIO_PIN_LOW
GPIO pin is at logic low.
Definition: gpio/v0/gpio.h:79
HwiP_construct
int32_t HwiP_construct(HwiP_Object *obj, HwiP_Params *params)
Create a Hwi object.
GPIO_pinOutValueRead
uint32_t GPIO_pinOutValueRead(uint32_t baseAddr, uint32_t pinNum)
This API determines the output logic level(value) on a specified GPIO pin.
GPIO_DIRECTION_INPUT
#define GPIO_DIRECTION_INPUT
Definition: gpio/v0/gpio.h:90
GPIO_PIN_HIGH
#define GPIO_PIN_HIGH
GPIO pin is at logic high.
Definition: gpio/v0/gpio.h:81
HwiP_Params_init
void HwiP_Params_init(HwiP_Params *params)
Set default values to HwiP_Params.
DebugP_log
#define DebugP_log(format,...)
Function to log a string to the enabled console.
Definition: DebugP.h:235
GPIO_clearBankIntrStatus
static void GPIO_clearBankIntrStatus(uint32_t baseAddr, uint32_t bankNum, uint32_t intrStatus)
This API clears the interrupt status of the specified bank.
Definition: gpio/v0/gpio.h:374
GPIO_TRIG_TYPE_RISE_EDGE
#define GPIO_TRIG_TYPE_RISE_EDGE
Interrupt request on occurrence of a rising edge on the input pin.
Definition: gpio/v0/gpio.h:101
GPIO_setDirMode
void GPIO_setDirMode(uint32_t baseAddr, uint32_t pinNum, uint32_t pinDir)
This API configures the direction of a specified GPIO pin as being either input or output.
GPIO_clearIntrStatus
static void GPIO_clearIntrStatus(uint32_t baseAddr, uint32_t pinNum)
This API clears the enabled interrupt status of a specified GPIO pin.
Definition: gpio/v0/gpio.h:346
GPIO_pinWriteLow
static void GPIO_pinWriteLow(uint32_t baseAddr, uint32_t pinNum)
This API drives an output GPIO pin to a logic LOW state.
Definition: gpio/v0/gpio.h:321
SystemP_SUCCESS
#define SystemP_SUCCESS
Return status when the API execution was successful.
Definition: SystemP.h:56
GPIO_DIRECTION_OUTPUT
#define GPIO_DIRECTION_OUTPUT
Definition: gpio/v0/gpio.h:89
HwiP_Params::callback
HwiP_FxnCallback callback
Definition: HwiP.h:77
GPIO_pinWriteHigh
static void GPIO_pinWriteHigh(uint32_t baseAddr, uint32_t pinNum)
This API drives an output GPIO pin to a logic HIGH state.
Definition: gpio/v0/gpio.h:309
gpio.h
GPIO_bankIntrDisable
void GPIO_bankIntrDisable(uint32_t baseAddr, uint32_t bankNum)
This API disables the bank interrupt.
GPIO_setTrigType
void GPIO_setTrigType(uint32_t baseAddr, uint32_t pinNum, uint32_t trigType)
This API configures the trigger type for a specified input GPIO pin.
HwiP_Params::args
void * args
Definition: HwiP.h:78
GPIO_GET_BANK_INDEX
#define GPIO_GET_BANK_INDEX(pinNum)
Returns the bank index based on pin number.
Definition: gpio/v0/gpio.h:126
DebugP_assert
#define DebugP_assert(expression)
Function to call for assert check.
Definition: DebugP.h:183
HwiP_Params::intNum
uint32_t intNum
Definition: HwiP.h:76
GPIO_TRIG_TYPE_NONE
#define GPIO_TRIG_TYPE_NONE
No interrupt request on either rising or falling edges on the pin.
Definition: gpio/v0/gpio.h:99
GPIO_getBankIntrStatus
static uint32_t GPIO_getBankIntrStatus(uint32_t baseAddr, uint32_t bankNum)
This API returns the interrupt status of the specified bank.
Definition: gpio/v0/gpio.h:359
FALSE
#define FALSE
Definition: csl_types.h:62
GPIO_pinRead
uint32_t GPIO_pinRead(uint32_t baseAddr, uint32_t pinNum)
This API reads the logic level(value) on a specified GPIO pin.
GPIO_bankIntrEnable
void GPIO_bankIntrEnable(uint32_t baseAddr, uint32_t bankNum)
This API enables the bank interrupt. This has to be called after setting all the GPIO pin triggers of...