- Note
- The steps on this page should be done each time EVM is power cycled or when a new CCS session is started.
Prerequisites
A quick recap of the steps that need to have been done before you proceed
- Make sure you have installed CCS as mentioned in Download, Install and Setup CCS
- Make sure the UART port used for console is identified as mentioned in Setup UART Terminal
- Make sure you have the EVM power cable, JTAG cable, UART cable connected as shown in Cable Connections
- Make sure the UART or CCS console logs on doing EVM POWER-ON indicate that SOC initialization is successful
- Make sure you have built the example of interest as mentioned in Build a Hello World example
Send Application using USB-DFU
- Setup the EVM in USB-DFU bootmode.
- POWER-ON the EVM.
- Send the prebuilt binary "tiboot3.bin" present at
${MCU_PLUS_SDK_PATH}/tools/boot/sbl_prebuilt/am62lx-evm/ as follows: sudo dfu-util -R -a bootloader -D tools/boot/sbl_prebuilt/am62lx-evm/tiboot3.bin
- You will see pre-BL logs on the UART console after this.
- Send the application binary, say,
hello_world.release.appimage.hs_fs after the first binary is sent: sudo dfu-util -R -a bootloader -D examples/hello_world/am62lx-evm/a53ss0-0_freertos/gcc-aarch64/hello_world.release.appimage.hs_fs
- You will see the application being executed after this step.
Application logs
Using CCS for debugging
Follow the below steps to debug an example application using CCS.
Start Project-less Debug
- You will see the AM62LX target configuration in the "Threads" tab of "Debug" window as shown below
Target Configuration After Launch
- Connect the target CPU of interest if not already connected. For the "hello world" example this is
CortexA53_0
Connect CPU
- Load the symbols of the application .out file as desired for debugging.
Load Symbols
- In the "Load Symbols" dialog, select "Browse" and select the program from
examples/{example folder}/{board}/{cpu}_{os}/{compiler} as shown below for the "hello world" program.
Select File for loading symbols
- After this step, you can see the symbols being loaded through the debugger and the entire call stack.
Debugging the application
Re-load and run example binaries
- Here simply repeat the steps shows in Send Application using USB-DFU
- You will need to power-cycle the EVM to reload the application or load a new application example.