AM62D FreeRTOS SDK  12.00.00
yang_db_runtime.h File Reference

Go to the source code of this file.

Macros

#define YANG_DB_LINE_BUF_SIZE   512u
 

Typedefs

typedef struct yang_db_runtime_data yang_db_runtime_dataq_t
 

Functions

yang_db_runtime_dataq_tyang_db_runtime_init (uc_dbald *dbald, uc_hwald *hwald)
 
void yang_db_runtime_close (yang_db_runtime_dataq_t *ydrd)
 
void yang_db_runtime_set_hwadl (yang_db_runtime_dataq_t *ydrd, uc_hwald *hwald)
 hwald is set with yang_db_runtime_init, this function sets/resets later. More...
 
int yang_db_runtime_readfile (yang_db_runtime_dataq_t *ydrd, const char *fname)
 read from a config file, and set data. More...
 
int yang_db_runtime_read_conffile (uc_dbald *dbald, const char *fname)
 internally create ydrd and then call "yang_db_runtime_readfile" More...
 
int yang_db_runtime_get_vtype (uc_dbald *dbald, uint8_t *aps)
 get value type of 'aps' leaf More...
 
int yang_db_runtime_put_oneline (yang_db_runtime_dataq_t *ydrd, char *kstr, char *vstr, uint8_t onhw)
 write one node db data by a string line More...
 
int yang_db_runtime_askaction (yang_db_runtime_dataq_t *ydrd, uc_notice_data_t *ucntd)
 ask to call 'uc_nc_askaction_push' More...
 
uc_range * yang_db_runtime_range_fromline (yang_db_runtime_dataq_t *ydrd, const char *line, void **kvs, uint8_t *kss, bool status)
 get a range from line More...
 
int yang_db_runtime_get_oneline (yang_db_runtime_dataq_t *ydrd, const char *line, void **value, uint32_t *vsize)
 get one node db data by a string line More...
 
int yang_db_runtime_notice_register (yang_db_runtime_dataq_t *ydrd, uc_notice_data_t *ucntd, const char *line, char *semname, UC_NOTICE_SIG_T **sem)
 
uint8_t yang_db_runtime_getvknum (uc_dbald *dbald, uint8_t *aps)
 
int yang_db_runtime_getvkvtype (uc_dbald *dbald, uint8_t *aps, uint8_t vkindex, uint8_t *vkey, uint8_t *vtype)
 
int yang_db_runtime_getvkstr (uc_dbald *dbald, uint8_t *aps, uint8_t vkindex, char **rstr)
 
int yang_db_runtime_waititem (yang_db_runtime_dataq_t *ydrd, const char *witem, void *waitv, uint32_t wvsize, int tout_ms)
 wait witem, if waitv!=NULL wait unitl the value matches. if waitv==NULL wait appearance of witem. More...
 
int yang_db_runtime_apkv2keyvkstr (uc_dbald *dbald, uint8_t *aps, kvs_t *kvs, uint8_t *kss, char **rstr)
 'key node string' and 'value key node string' of (aps,kvs,kss) More...
 
int yang_db_runtime_getkeyvkstr (uc_dbald *dbald, void *key, uint32_t ksize, char **rstr)
 'key node string' and 'value key node string' of key More...
 
int yang_db_runtime_proc_nodestring (yang_db_runtime_dataq_t *ydrd, bool reset, char *kstr, char *vstr)
 
int yang_db_runtime_state_keyvkstr (yang_db_runtime_dataq_t *ydrd, char **rstr)
 call yang_db_runtime_getkeyvkstr with the internal ydrd state More...
 
const char * convxml2conf_getconf (yang_db_runtime_dataq_t *ydrd, const char *ifname, const char *ofname)
 convert xml format config file to Excelfore format config file More...
 
bool yang_db_runtime_needaction (yang_db_runtime_dataq_t *ydrd)
 
int yang_db_runtime_nodestr2apkv (yang_db_runtime_dataq_t *ydrd, const char *line, uint8_t *aps, void **kvs, uint8_t *kss)
 convert yang key string to aps,kvs,kss,,, in ydrd More...
 
void yang_db_runtime_readdb_log (bool consoleprint, uc_dbald *dbald, const char *headmsg, uint8_t aps[], void *kvs[], uint8_t kss[])
 read from the DB, and print into the log file, optionally print on console. More...
 
int yang_db_runtime_iterate_fromline (yang_db_runtime_dataq_t *ydrd, uc_range **range, const char *line, void *kvs[], uint8_t kss[], bool status, void **value, uint32_t *vsize, char **qstr)
 get a range from line, then iterate the contents More...
 
int yang_db_runtime_cache_fromline (yang_db_runtime_dataq_t *ydrd, const char *line, bool status, char **rvalue, int *rvsize)
 call 'yang_db_runtime_iterate_fromline' internally and cache (qstr, vstr) into 'rvalue'. More...
 
void yang_db_runtime_cache_fromline_release (char *rvalue)
 release the reserved memory in 'yang_db_runtime_cache_fromline' More...
 

Macro Definition Documentation

◆ YANG_DB_LINE_BUF_SIZE

#define YANG_DB_LINE_BUF_SIZE   512u

Typedef Documentation

◆ yang_db_runtime_dataq_t

typedef struct yang_db_runtime_data yang_db_runtime_dataq_t

Function Documentation

◆ yang_db_runtime_init()

yang_db_runtime_dataq_t* yang_db_runtime_init ( uc_dbald *  dbald,
uc_hwald *  hwald 
)

◆ yang_db_runtime_close()

void yang_db_runtime_close ( yang_db_runtime_dataq_t ydrd)

◆ yang_db_runtime_set_hwadl()

void yang_db_runtime_set_hwadl ( yang_db_runtime_dataq_t ydrd,
uc_hwald *  hwald 
)

hwald is set with yang_db_runtime_init, this function sets/resets later.

◆ yang_db_runtime_readfile()

int yang_db_runtime_readfile ( yang_db_runtime_dataq_t ydrd,
const char *  fname 
)

read from a config file, and set data.

Parameters
ydrdyang_db_runtime_dataq_t
fnameconfig file name
Returns
-1:error, 0:success

◆ yang_db_runtime_read_conffile()

int yang_db_runtime_read_conffile ( uc_dbald *  dbald,
const char *  fname 
)

internally create ydrd and then call "yang_db_runtime_readfile"

Parameters
dbalduc_dbald
fnameconfig file name
Returns
-1:error, 0:success

◆ yang_db_runtime_get_vtype()

int yang_db_runtime_get_vtype ( uc_dbald *  dbald,
uint8_t *  aps 
)

get value type of 'aps' leaf

Returns
>=0:vtype, -1:error

◆ yang_db_runtime_put_oneline()

int yang_db_runtime_put_oneline ( yang_db_runtime_dataq_t ydrd,
char *  kstr,
char *  vstr,
uint8_t  onhw 
)

write one node db data by a string line

Parameters
ydrdyang_db_runtime_dataq_t
kstrkey string
vstrvalue string
onhwaction on hardware
Returns
-1:error, 0:success

◆ yang_db_runtime_askaction()

int yang_db_runtime_askaction ( yang_db_runtime_dataq_t ydrd,
uc_notice_data_t *  ucntd 
)

ask to call 'uc_nc_askaction_push'

Parameters
ydrdyang_db_runtime_dataq_t
ucntduc_notice_data_t
Returns
-1:error, 0:success
Note
ydrd->aps,kvs,kss must be set already to call this function.

◆ yang_db_runtime_range_fromline()

uc_range* yang_db_runtime_range_fromline ( yang_db_runtime_dataq_t ydrd,
const char *  line,
void **  kvs,
uint8_t *  kss,
bool  status 
)

get a range from line

Parameters
ydrdyang_db_runtime_dataq_t
linekey string
kvsreturn value keys, it must have MAX_KV_DEPTH+1 of void pointer space
kssreturn value key sizes, it must have MAX_KV_DEPTH of uint8_t space
statustrue:get range from status('ro') area, false: get from config('rw') area
Returns
ragne object:success, NULL:error
Note
returned ranage object must be released by calling uc_get_range_release

◆ yang_db_runtime_get_oneline()

int yang_db_runtime_get_oneline ( yang_db_runtime_dataq_t ydrd,
const char *  line,
void **  value,
uint32_t *  vsize 
)

get one node db data by a string line

Parameters
ydrdyang_db_runtime_dataq_t
linekey string
valuevalue pointer to return read value. it is reallocated inside the function. it must be NULL or allocated address.
vsizevalue size
Returns
-1:error, vtype>=0:success

◆ yang_db_runtime_notice_register()

int yang_db_runtime_notice_register ( yang_db_runtime_dataq_t ydrd,
uc_notice_data_t *  ucntd,
const char *  line,
char *  semname,
UC_NOTICE_SIG_T **  sem 
)

◆ yang_db_runtime_getvknum()

uint8_t yang_db_runtime_getvknum ( uc_dbald *  dbald,
uint8_t *  aps 
)
Returns
number of value keys on aps node.

◆ yang_db_runtime_getvkvtype()

int yang_db_runtime_getvkvtype ( uc_dbald *  dbald,
uint8_t *  aps,
uint8_t  vkindex,
uint8_t *  vkey,
uint8_t *  vtype 
)
Returns
vtype of vkindex's key on aps node. return -1: error return 0: vkey, vtype(yang_vtype_enum_t) is set

◆ yang_db_runtime_getvkstr()

int yang_db_runtime_getvkstr ( uc_dbald *  dbald,
uint8_t *  aps,
uint8_t  vkindex,
char **  rstr 
)
Returns
value key node string of vkindex's key on aps node. return -1: error return 0: the result str in '*rst', the caller must call UB_SD_RELMEM to release.

◆ yang_db_runtime_waititem()

int yang_db_runtime_waititem ( yang_db_runtime_dataq_t ydrd,
const char *  witem,
void *  waitv,
uint32_t  wvsize,
int  tout_ms 
)

wait witem, if waitv!=NULL wait unitl the value matches. if waitv==NULL wait appearance of witem.

Parameters
ydrdyang_db_runtime_dataq_t
witemwait item
waitvwait value
wvsizewait value size
tout_mswait timeout (ms)
Returns
return 0:got the waitv, 1:timed out, -1:error

◆ yang_db_runtime_apkv2keyvkstr()

int yang_db_runtime_apkv2keyvkstr ( uc_dbald *  dbald,
uint8_t *  aps,
kvs_t *  kvs,
uint8_t *  kss,
char **  rstr 
)

'key node string' and 'value key node string' of (aps,kvs,kss)

Parameters
dbalduc_dbald
apsnode keys, must be terminated with 255
kvsvalue keys
ksssize of value keys
rstrdata out
Returns
-1: error, 0: the result str in '*rst', the caller must call UB_SD_RELMEM to release.

◆ yang_db_runtime_getkeyvkstr()

int yang_db_runtime_getkeyvkstr ( uc_dbald *  dbald,
void *  key,
uint32_t  ksize,
char **  rstr 
)

'key node string' and 'value key node string' of key

Returns
-1: error, 0: the result str in '*rst', the caller must call UB_SD_RELMEM to release.

◆ yang_db_runtime_proc_nodestring()

int yang_db_runtime_proc_nodestring ( yang_db_runtime_dataq_t ydrd,
bool  reset,
char *  kstr,
char *  vstr 
)
Returns
N>=0:set node and need N value keys, -1:set one value key, -2:pass leaf, -3:error
Parameters
ydrdyang_db_runtime_dataq_t
resetreset ydrd->api to start over
kstrkey stting
vstrvalue string, if this is NULL, kstr should be node

◆ yang_db_runtime_state_keyvkstr()

int yang_db_runtime_state_keyvkstr ( yang_db_runtime_dataq_t ydrd,
char **  rstr 
)

call yang_db_runtime_getkeyvkstr with the internal ydrd state

Returns
0: the result str in '*rst', the caller must call UB_SD_RELMEM to release.

◆ convxml2conf_getconf()

const char* convxml2conf_getconf ( yang_db_runtime_dataq_t ydrd,
const char *  ifname,
const char *  ofname 
)

convert xml format config file to Excelfore format config file

Parameters
ydrdyang_db_runtime_dataq_t
ifnameinput xml format filename
ofnameoutput Excelfore format filename. if NULL, use a default temp file
Returns
'converted filename': success, NULL:fail

◆ yang_db_runtime_needaction()

bool yang_db_runtime_needaction ( yang_db_runtime_dataq_t ydrd)

◆ yang_db_runtime_nodestr2apkv()

int yang_db_runtime_nodestr2apkv ( yang_db_runtime_dataq_t ydrd,
const char *  line,
uint8_t *  aps,
void **  kvs,
uint8_t *  kss 
)

convert yang key string to aps,kvs,kss,,, in ydrd

Parameters
ydrdyang_db_runtime_dataq_t
linekey string
apsreturn node keys, it must have UC_MAX_AP_DEPTH of uint8_t space
kvsreturn value keys, it must have UC_MAX_KV_DEPTH+1 of void pointer space
kssreturn value key sizes, it must have UC_MAX_KV_DEPTH of uint8_t space
Returns
-1:error, vtype>=0:success
Note
returned aps is terminated with 255, kvs with NULL, and kss with 0

◆ yang_db_runtime_readdb_log()

void yang_db_runtime_readdb_log ( bool  consoleprint,
uc_dbald *  dbald,
const char *  headmsg,
uint8_t  aps[],
void *  kvs[],
uint8_t  kss[] 
)

read from the DB, and print into the log file, optionally print on console.

Parameters
consoleprinttrue:priont on console
dbalduc_dbald
headmsgprefix of message log
apsnode keys
kvsvalue keys
kssvalue key sizes

◆ yang_db_runtime_iterate_fromline()

int yang_db_runtime_iterate_fromline ( yang_db_runtime_dataq_t ydrd,
uc_range **  range,
const char *  line,
void *  kvs[],
uint8_t  kss[],
bool  status,
void **  value,
uint32_t *  vsize,
char **  qstr 
)

get a range from line, then iterate the contents

Parameters
ydrdyang_db_runtime_dataq_t
rangewhen the iteration stops at the middle(stop with return 0 status) needs to be released by uc_get_range_release. when it comes to the end it is internally called, and no need to release 'range'
linekey string, value keys can be wildcard without value part
kvsreturn value keys, it must have MAX_KV_DEPTH+1 of void pointer space
kssreturn value key sizes, it must have MAX_KV_DEPTH of uint8_t space
statustrue:get range from status('ro') area, false: get from config('rw') area
valuevalue of the iterated key
vsizevalue size
qstrdata out
Returns
>=0:vtype, -1:error or comes to the end

◆ yang_db_runtime_cache_fromline()

int yang_db_runtime_cache_fromline ( yang_db_runtime_dataq_t ydrd,
const char *  line,
bool  status,
char **  rvalue,
int *  rvsize 
)

call 'yang_db_runtime_iterate_fromline' internally and cache (qstr, vstr) into 'rvalue'.

◆ yang_db_runtime_cache_fromline_release()

void yang_db_runtime_cache_fromline_release ( char *  rvalue)

release the reserved memory in 'yang_db_runtime_cache_fromline'