AM62D FreeRTOS SDK  12.00.00
unibase_macros.h File Reference

Introduction

Utility macros for convenience.

Go to the source code of this file.

Macros

#define UB_SEC_NS   1000000000LL
 one second in unit of nano second More...
 
#define UB_MSEC_NS   1000000
 one mili second in unit of nano second More...
 
#define UB_USEC_NS   1000
 one micro second in unit of nano second More...
 
#define UB_SEC_US   1000000LL
 one second in unit of microsecond More...
 
#define UB_MSEC_US   1000
 one mili second in unit of microsecond More...
 
#define UB_SEC_MS   1000
 one second in unit of milisecond More...
 
#define UB_CHARS_IN_LINE   384
 
#define UB_BIT(x)   (1U<<(x))
 bit x More...
 
#define UB_MAX(x, y)   ((x)>(y)?(x):(y))
 max(x,y) More...
 
#define UB_MIN(x, y)   ((x)<(y)?(x):(y))
 min(x,y) More...
 
#define UB_CONSOLE_PRINT(...)
 
#define UB_DEBUGMEM_PRINT(...)
 
#define UB_CONSOLE_DEBUGMEM_PRINT(...)
 
#define UB_SELECT_PRINT(console, debugmem, ...)
 
#define UB_LOG(level, ...)   UB_LOG_##level(__VA_ARGS__)
 UB_LOG(level, formt, ...), level is compared to the level in the category which is defined by UB_LOGCAT. More...
 
#define UB_TLOG(level, ...)   UB_TLOG_##level(__VA_ARGS__)
 UB_TLOG add timestamp regardless the timestamp option in the category. More...
 
#define UB_VLOG(var, ...)
 UB_VLOG allows for flexible logging with a variable log level specified as an argument in the function call. Example Usage: void func(int level, int abc) { UB_VLOG(level, "hello world\n"); } The func can be called as: func(UBL_DEBUGV, abc); In this case UB_LOG and UB_TLOG can not work. More...
 
#define UB_PRIhexB8   "%02X:%02X:%02X:%02X:%02X:%02X:%02X:%02X"
 use this to print ub_streamid_t More...
 
#define UB_ARRAY_B8(x)   (x)[0],(x)[1],(x)[2],(x)[3],(x)[4],(x)[5],(x)[6],(x)[7]
 
#define UB_PRIhexB6   "%02X:%02X:%02X:%02X:%02X:%02X"
 use this to print ub_macaddr_t More...
 
#define UB_ARRAY_B6(x)   (x)[0],(x)[1],(x)[2],(x)[3],(x)[4],(x)[5]
 used with UB_PRIhexB6 More...
 
#define UB_NON_ZERO_B6(x)   (((x)[0]|(x)[1]|(x)[2]|(x)[3]|(x)[4]|(x)[5])!=0u)
 true if 6-byte binaries are not all zero More...
 
#define UB_NON_ZERO_B8(x)   (((x)[0]|(x)[1]|(x)[2]|(x)[3]|(x)[4]|(x)[5]|(x)[6]|(x)[7])!=0u)
 true if 8-byte binaries are not all zero More...
 
#define UB_ALLFF_B6(x)   (((x)[0]&(x)[1]&(x)[2]&(x)[3]&(x)[4]&(x)[5])==0xffu)
 true if 6-byte binaries are all 0xff More...
 
#define UB_ALLFF_B8(x)   (((x)[0]&(x)[1]&(x)[2]&(x)[3]&(x)[4]&(x)[5]&(x)[6]&(x)[7])==0xffu)
 true if 8-byte binaries are all 0xff More...
 
#define UB_ABIT8_FIELD(name, s, m)
 two of inline functions: name_bit_field, name_set_bit_field are created for bit opperation on a network bit order endian variable. More...
 
#define UB_ABIT16_FIELD(name, s, m)
 the same like UB_BIT8_FILED, works on 16-bit variable More...
 
#define UB_ABIT32_FIELD(name, s, m)
 the same like UB_BIT8_FILED, works on 32-bit variable More...
 
#define UB_ABIT8_TOGGLE_FIELD(name, s, m)
 inline function: name_toggle_bit_field is created for toggling bit opperation on a network bit order variable. More...
 
#define UB_ABIT16_TOGGLE_FIELD(name, s, m)
 the same like UB_BIT8_TOGGLE_FIELD, works on 16-bit variable More...
 
#define UB_ABIT32_TOGGLE_FIELD(name, s, m)
 the same like UB_BIT8_TOGGLE_FIELD, works on 32-bit variable More...
 
#define UB_TS2NSEC(ts)   (((int64_t)(ts).tv_sec*1000000000)+(ts).tv_nsec)
 convert 'struct timespec' vaule to nanosecond integer More...
 
#define UB_TS2USEC(ts)   (((int64_t)(ts).tv_sec*1000000)+(ts).tv_nsec/UB_USEC_NS)
 convert 'struct timespec' vaule to microsecond integer More...
 
#define UB_TS2MSEC(ts)   (((int64_t)(ts).tv_sec*UB_SEC_MS)+(ts).tv_nsec/UB_MSEC_NS)
 convert 'struct timespec' vaule to milisecond integer More...
 
#define UB_TV2NSEC(tv)   (((int64_t)(tv).tv_sec*1000000000)+(int64_t)(tv).tv_usec*UB_USEC_NS)
 convert 'struct timeval' vaule to nanosecond integer More...
 
#define UB_TV2USEC(tv)   (((int64_t)(tv).tv_sec*1000000)+(tv).tv_usec)
 convert 'struct timeval' vaule to nanosecond integer More...
 
#define UB_TV2MSEC(tv)   (((int64_t)(tv).tv_sec*UB_SEC_MS)+(tv).tv_usec/UB_MSEC_US)
 convert 'struct timeval' vaule to milisecond integer More...
 
#define UB_NSEC2TS(ns, ts)   {(ts).tv_sec=(ns)/1000000000;(ts).tv_nsec=(ns)%1000000000;}
 convert nanosec value to 'struct timespec' vaule More...
 
#define UB_USEC2TS(us, ts)   {(ts).tv_sec=(us)/1000000;(ts).tv_nsec=((us)%1000000)*UB_USEC_NS;}
 convert microsec value to 'struct timespec' vaule More...
 
#define UB_MSEC2TS(ms, ts)   {(ts).tv_sec=(ms)/UB_SEC_MS;(ts).tv_nsec=((ms)%UB_SEC_MS)*UB_MSEC_NS;}
 convert milisec value to 'struct timespec' vaule More...
 
#define UB_NSEC2TV(ns, tv)   {(tv).tv_sec=(ns)/1000000000;(tv).tv_usec=((ns)%1000000000)/UB_USEC_NS;}
 convert nanosec value to 'struct timeval' vaule More...
 
#define UB_USEC2TV(us, tv)   {(tv).tv_sec=(us)/1000000;(tv).tv_usec=(us)%1000000;}
 convert microsec value to 'struct timeval' vaule More...
 
#define UB_MSEC2TV(ms, tv)   {(tv).tv_sec=(ms)/UB_SEC_MS;(tv).tv_usec=((ms)%UB_SEC_MS)*UB_MSEC_US;}
 convert milisec value to 'struct timeval' vaule More...
 
#define UB_TV_DIFF64NS(tv1, tv2)   (UB_TV2NSEC(tv1)-UB_TV2NSEC(tv2))
 tv1-tv2 in 64-bit nanosecond unit More...
 
#define UB_TV_ADD64NS(tv1, tv2)   (UB_TV2NSEC(tv1)+UB_TV2NSEC(tv2))
 tv1+tv2 in 64-bit nanosecond unit More...
 
#define UB_TS_DIFF64NS(ts1, ts2)   (UB_TS2NSEC(ts1)-UB_TS2NSEC(ts2))
 ts1-ts2 in 64-bit nanosecond unit More...
 
#define UB_TS_ADD64NS(ts1, ts2)   (UB_TS2NSEC(ts1)+UB_TS2NSEC(ts2))
 ts1+ts2 in 64-bit nanosecond unit More...
 
#define UB_TV_DIFF_TV(rtv, tv1, tv2)
 rtv=tv1-tv2 in 64-bit nanosecond unit More...
 
#define UB_TS_DIFF_TS(rts, ts1, ts2)
 rts=ts1-ts2 in 64-bit nanosecond unit More...
 
#define UB_TV_ADD_TV(rtv, tv1, tv2)
 rtv=tv1+tv2 in 64-bit nanosecond unit More...
 
#define UB_TS_ADD_TS(rts, ts1, ts2)
 rts=ts1+ts2 in 64-bit nanosecond unit More...
 
#define UB_HTONLL(x)
 convert values between host and network byte order. which converts the unsigned integer host long long from host byte order to network byte order. More...
 
#define UB_NTOHLL(x)
 convert values between host and network byte order. converts the unsigned integer netlong from network byte order to host byte order. More...
 
#define UB_STATIC_ASSERT(cond, msg)   typedef char msg[(cond) ? 1 : -1]
 assert during compilation time. When cond is equal to true, no error. Otherwise, compilation error is raised. e.g. UB_STATIC_ASSERT(uint8_t == 1, Uint8InvalidSize) More...
 
#define UB_PROTECTED_FUNC(cbfunc, rval, ...)
 call the cbfunc with an internal mutex protection. The ub_func_private_mutex_lock() and ub_func_private_mutex_unlock() are only used privately in this macro. Please do not use them freely elsewhere. More...
 
#define UB_PROTECTED_FUNC_VOID(cbfunc, ...)
 similar to the UB_PROTECTED_FUNC without return value rval More...