AM62D FreeRTOS SDK  12.00.00
unibase_binding.h File Reference

Introduction

functions to bind unibase to a specific platform

  • This layer support binding to a specific platform.
  • The implementation is platform specific.
  • Using this binding is optional, and for the unibase library, a diferent binding layer can be used.

Go to the source code of this file.

Macros

#define UBB_DEFAULT_DEBUG_LOG_MEMORY   (64*1024)
 ubb_memory_out_init uses this value to allocate internal buffer when 'mem' parameter is NULL. More...
 
#define UBB_MEMOUT_ENDMARK   "---###---"
 ubb_memory_out always add this end mark at the end of printing. More...
 
#define UBB_DEFAULT_LOG_INITSTR   "4,ubase:45"
 ubb_default_initpara uses this string as 'ub_log_initstr' More...
 
#define UBB_GETENV   getenv
 get a string from an environment variable More...
 

Typedefs

typedef uint64_t(* get64ts_t) (void)
 

Functions

int ubb_memory_out_init (char *mem, int size)
 initialize the internal memory_out function More...
 
int ubb_memory_out_close (void)
 de-initialize memory_out function More...
 
char * ubb_memory_out_buffer (void)
 return the memory pointer of memory_out More...
 
int ubb_memory_out_lastline (char **str, int *size)
 return the most recent output line in memory_out More...
 
int ubb_memory_out_alldata (char **rstr, int *size)
 return the all written line data in the buffer More...
 
int ubb_memory_file_out (const char *fname)
 write the data in memory_out buffer into a file More...
 
void ubb_default_initpara (unibase_init_para_t *init_para)
 return the default initialization parameters supported in the binding layer More...
 
void ubb_set_gptp_gettime64 (get64ts_t func)
 set gptptime function for ub_gptp_gettime64 More...
 
void ubb_unibase_easyinit (void)
 initialize unibase with 'ubb_default_initpara' More...