Go to the source code of this file.
Data Structures | |
| struct | tisci_msg_set_device_req |
| Set the desired state of the device. More... | |
| struct | tisci_msg_set_device_resp |
| Empty response for TISCI_MSG_SET_DEVICE. More... | |
| struct | tisci_msg_get_device_req |
| Request to get device based on id. More... | |
| struct | tisci_msg_get_device_resp |
| Response to get device request. More... | |
| struct | tisci_msg_set_device_resets_req |
| Set the desired state of the resets of a device. More... | |
| struct | tisci_msg_set_device_resets_resp |
| Empty response for TISCI_MSG_SET_DEVICE_RESETS. More... | |
| struct | tisci_msg_device_drop_powerup_ref_req |
| Drop any remaining powerup device references. More... | |
| struct | tisci_msg_device_drop_powerup_ref_resp |
| Empty response for TISCI_MSG_DEVICE_DROP_POWERUP_REF. More... | |
| struct | tisci_msg_get_device_multiple_req |
| Request to get current state of multiple devices in the SoC. More... | |
| struct | tisci_msg_get_device_multiple_resp |
| Response containing device states as bitmap. More... | |
Macros | |
| #define | TISCI_MSG_FLAG_DEVICE_WAKE_ENABLED TISCI_BIT(8) |
| This file contains: More... | |
| #define | TISCI_MSG_FLAG_DEVICE_RESET_ISO TISCI_BIT(9) |
| #define | TISCI_MSG_FLAG_DEVICE_EXCLUSIVE TISCI_BIT(10) |
| #define | TISCI_MSG_VALUE_DEVICE_SW_STATE_AUTO_OFF 0U |
| #define | TISCI_MSG_VALUE_DEVICE_SW_STATE_RETENTION 1U |
| #define | TISCI_MSG_VALUE_DEVICE_SW_STATE_ON 2U |
| #define | TISCI_MSG_VALUE_DEVICE_HW_STATE_OFF 0U |
| #define | TISCI_MSG_VALUE_DEVICE_HW_STATE_ON 1U |
| #define | TISCI_MSG_VALUE_DEVICE_HW_STATE_TRANS 2U |
| #define | TISCI_MSG_DEVICE_BITMAP_WORDS 10U |
| #define | TISCI_MSG_MAX_DEVICE_IDS_MULTIPLE 160U |
Functions | |
| struct tisci_msg_set_device_req | __attribute__ ((__packed__)) |
Variables | |
| struct tisci_header | hdr |
| uint32_t | id |
| uint32_t | reserved |
| uint8_t | state |
| uint32_t | context_loss_count |
| uint32_t | resets |
| uint8_t | programmed_state |
| uint8_t | current_state |
| uint16_t | start_device_id |
| uint16_t | count |
| uint16_t | remaining |
| uint32_t | device_state_bitmap [TISCI_MSG_DEVICE_BITMAP_WORDS] |
| struct tisci_header hdr |
| uint32_t id |
| uint32_t reserved |
| uint8_t state |
| uint32_t context_loss_count |
| uint32_t resets |
| uint8_t programmed_state |
| uint8_t current_state |
| uint16_t start_device_id |
| uint16_t count |
| uint16_t remaining |
| uint32_t device_state_bitmap[TISCI_MSG_DEVICE_BITMAP_WORDS] |