OSPI driver object.
Public Member Functions | |
| uint8_t tempBuf[512U] | __attribute__ ((aligned(32))) |
Data Fields | |
| OSPI_Handle | handle |
| uint32_t | transferMode |
| uint32_t | protocol |
| uint32_t | rdDummyCycles |
| uint32_t | cmdDummyCycles |
| uint32_t | rdDataCapDelay |
| uint32_t | phyRdDataCapDelay |
| uint32_t | phyCfgVal |
| uint32_t | phyDummyCycles |
| uint32_t | numAddrBytes |
| uint32_t | cmdExtType |
| uint32_t | isOpen |
| SemaphoreP_Object | lockObj |
| SemaphoreP_Object | transferSemObj |
| HwiP_Object | hwiObj |
| uint32_t | phyEnableSuccess |
| uint32_t | rdDummyValPhyMode |
| OSPI_Transaction * | currTrans |
| void * | ospiDmaHandle |
| uint32_t | deviceSize |
| uint32_t | pageSize |
| uint8_t tempBuf [512U] OSPI_Object::__attribute__ | ( | (aligned(32)) | ) |
| OSPI_Handle OSPI_Object::handle |
Instance handle
| uint32_t OSPI_Object::transferMode |
Polling, Blocking or Callback mode. Refer OSPI_TransferMode
| uint32_t OSPI_Object::protocol |
Protocol for OSPI reading/writing. 32 bit integer with byte0 -> data lines byte1 -> addr lines byte2 -> cmd lines byte3 -> STR/DTR (0 = STR, 1 = DTR)
| uint32_t OSPI_Object::rdDummyCycles |
Number of dummy cycles needed for read
| uint32_t OSPI_Object::cmdDummyCycles |
Number of dummy cycles needed for cmd
| uint32_t OSPI_Object::rdDataCapDelay |
Read data capture delays needed
| uint32_t OSPI_Object::phyRdDataCapDelay |
Read data capture delays needed when phy is enabled
| uint32_t OSPI_Object::phyCfgVal |
Read phy tuning dll values needed when phy is enabled at the previous stage
| uint32_t OSPI_Object::phyDummyCycles |
Read dummy cycle values needed when phy is enabled at the previous stage
| uint32_t OSPI_Object::numAddrBytes |
Number of bytes used to represent address to be sent to flash. This is the actual number of bytes used. The code to be programmed to registers is this value-1. That is, for 4-byte addressing mode, register should be programmed as 3
| uint32_t OSPI_Object::cmdExtType |
In dual byte opcode mode, the extended opcode can vary depending on flash This variable should be populated from the flash driver using the OSPI_setCmdExtType API
| uint32_t OSPI_Object::isOpen |
Flag to indicate if the instance is already open
| SemaphoreP_Object OSPI_Object::lockObj |
Driver lock object
| SemaphoreP_Object OSPI_Object::transferSemObj |
Transfer Sync Semaphore object
| HwiP_Object OSPI_Object::hwiObj |
Interrupt object
| uint32_t OSPI_Object::phyEnableSuccess |
This has to be set from the flash driver if the PHY tuning completed successfully
| uint32_t OSPI_Object::rdDummyValPhyMode |
Read dummy cycle update value for OSPI read in Phy mode
| OSPI_Transaction* OSPI_Object::currTrans |
Pointer to current transaction struct
| void* OSPI_Object::ospiDmaHandle |
Size of the device connected to the OSPI controller
| uint32_t OSPI_Object::deviceSize |
Size of a page in bytes for the OSPI flash memory device
| uint32_t OSPI_Object::pageSize |
Temporary buffer for odd-byte alignment in 8D-8D-8D protocol mode. Max typical flash page size is 512 bytes. Caller must hold lockObj when using readIndirect/writeIndirect to ensure thread-safe access to this buffer