AM62D FreeRTOS SDK  12.00.00
MCASP_DmaIcnt Struct Reference

Data Fields

uint8_t initDone
 
uint32_t txnByteCnt
 
uint16_t icnt0
 
uint16_t icnt1
 
uint16_t icnt2
 
uint16_t icnt3
 
int32_t dim1
 
int32_t dim2
 
int32_t dim3
 

Field Documentation

◆ initDone

uint8_t MCASP_DmaIcnt::initDone

Flag to indicate if the ICNT is initialized

◆ txnByteCnt

uint32_t MCASP_DmaIcnt::txnByteCnt

Byte count for the TR

◆ icnt0

uint16_t MCASP_DmaIcnt::icnt0

ICNT0 value for the TR

◆ icnt1

uint16_t MCASP_DmaIcnt::icnt1

ICNT1 value for the TR

◆ icnt2

uint16_t MCASP_DmaIcnt::icnt2

ICNT2 value for the TR

◆ icnt3

uint16_t MCASP_DmaIcnt::icnt3

ICNT3 value for the TR

◆ dim1

int32_t MCASP_DmaIcnt::dim1

Signed dimension for loop level 1

◆ dim2

int32_t MCASP_DmaIcnt::dim2

Signed dimension for loop level 2

◆ dim3

int32_t MCASP_DmaIcnt::dim3

Signed dimension for loop level 3