AM62D FreeRTOS SDK  12.00.00

Detailed Description

Output args for CPSW_ALE_IOCTL_GET_BCAST_MCAST_LIMIT IOCTL command.

Data Fields

bool rateLimitEn
 
bool rateLimitAtTxPort
 
uint32_t numPorts
 
CpswAle_PortBcastMcastRateLimitParams portPrms [CPSW_ALE_NUM_PORTS]
 

Field Documentation

◆ rateLimitEn

bool CpswAle_GetBcastMcastRateLimitOutArgs::rateLimitEn

Indicates if broadcast/multicast rate limit is enabled

◆ rateLimitAtTxPort

bool CpswAle_GetBcastMcastRateLimitOutArgs::rateLimitAtTxPort

Rate limit to be done at transmit or receive port

◆ numPorts

uint32_t CpswAle_GetBcastMcastRateLimitOutArgs::numPorts

Number of port for which broadcast/multicast rate limiting config to be applied

◆ portPrms

CpswAle_PortBcastMcastRateLimitParams CpswAle_GetBcastMcastRateLimitOutArgs::portPrms[CPSW_ALE_NUM_PORTS]

Per port broadcast/multicast rate limit params