This file contains the SDL PBIST API's.
Go to the source code of this file.
Enumerations | |
| enum | SDL_PBIST_testType { SDL_PBIST_TEST, SDL_PBIST_NEG_TEST } |
| PBIST self test type. More... | |
Functions | |
| int32_t | SDL_PBIST_selfTest (SDL_PBIST_inst instance, SDL_PBIST_testType testType, uint32_t timeout, bool *pResult) |
| PBIST self test. More... | |
| int32_t | SDL_SBL_PBIST_selfTest (SDL_PBIST_inst instance, SDL_PBIST_testType testType) |
| PBIST self test for MCU only. More... | |
| uint32_t | SDL_SBL_PBIST_checkDone (SDL_PBIST_inst instance) |
| PBIST API to check if the test is complete. More... | |
| int32_t | SDL_SBL_PBIST_checkResult (SDL_PBIST_inst instance) |
| PBIST API to check if PBIST test is executed successfully. More... | |