AM62D FreeRTOS SDK  12.00.00
sa3ul.h File Reference

Introduction

This file contains the prototype of SA3UL driver APIs.

Go to the source code of this file.

Data Structures

struct  SA3UL_ContextParams
 Parameters passed to SA3UL_contextAlloc() More...
 
struct  SA3UL_Params
 Parameters passed to SA3UL_open() More...
 
struct  SA3UL_Object
 Object for a SA3UL crypto operation. More...
 
struct  SA3UL_Attrs
 SA3UL instance attributes - used during init time. More...
 
struct  SA3UL_Config
 SA3UL driver context. More...
 
struct  SA3UL_MCEData
 MEDdata for Encryption engine. More...
 
struct  SA3UL_SecCtxAuth
 SA3UL context RAM structure for authentication engine. More...
 
struct  SA3UL_Scctl
 SA3UL SC control structure. More...
 
struct  SA3UL_SecCtxEnc
 SA3UL context RAM structure for Encryption engine. More...
 
struct  SA3UL_SecCtx
 SA3UL context RAM structure. More...
 
struct  SA3UL_ContextObject
 SA3UL context object structure. More...
 

Macros

#define SA3UL_ENC_KEYSIZE_BITS(k)   (128u + (64u * (k)))
 
SA3UL macros

#define SA3UL_MAX_HASH_SIZE_BYTES   (64U)
 Max hash size in bytes. More...
 
#define SA3UL_MAX_KEY_SIZE_BYTES   (32U)
 Max key size in bytes. More...
 
#define SA3UL_MAX_IV_SIZE_BYTES   (16U)
 Max Initialization vector (IV) size in bytes. More...
 
#define SA3UL_NUMBER_OF_RINGS   (3U)
 Max number of rings. More...
 
#define SA3UL_CACHELINE_ALIGNMENT   (128U)
 Cache line size for alignment of descriptor and buffers. More...
 
#define SA3UL_SECCTX_SIZE   (256U)
 Secure context memsize. More...
 
#define SA3UL_INSTANCES_MAX   (4U)
 Max SA3UL instances. More...
 
#define SA3UL_RING_N_ELEMS   (8U)
 Max SA3UL ring n elements. More...
 
#define SA3UL_SW_RING_NUM   (304U)
 Max SA3UL sw ring number. More...
 
#define SA3UL_MAX_INPUT_LENGTH_ENC   (0xFFFFU)
 Max Aes input length for encryption and decryption (64KB-1) More...
 
#define SA3UL_MAX_INPUT_LENGTH_AUTH   (0x3FFFFFU)
 Max input length for authentication (4MB-1) More...
 
SA3UL Algo Types

#define SA3UL_HASH_ALG_NULL   (0x10U)
 Hash Algo NULL. More...
 
#define SA3UL_HASH_ALG_SHA1   (0x12U)
 Hash Algo SHA-1. More...
 
#define SA3UL_HASH_ALG_SHA2_256   (0x14U)
 Hash Algo SHA-256. More...
 
#define SA3UL_HASH_ALG_SHA2_512   (0x16U)
 Hash Algo SHA-512. More...
 
SA3UL Operations Sequence

#define SA3UL_OP_ENC   (0x01U)
 SA3UL operations encryption. More...
 
#define SA3UL_OP_AUTH   (0x02U)
 SA3UL operations authentication. More...
 
#define SA3UL_OP_ENC_THEN_AUTH   (0x03U)
 SA3UL operation encryption then authentication. More...
 
#define SA3UL_OP_AUTH_THEN_ENC   (0x04U)
 SA3UL operations authentication then encryption. More...
 
SA3UL engine operation type

#define SA3UL_ENGINE_CODE_DEFAULT_ENGINE_ID   (0U)
 SA3UL default engine Id. More...
 
#define SA3UL_ENGINE_CODE_ENCRYPTION_MODULE_P1   (2U)
 SA3UL Encryption engine module p1. More...
 
#define SA3UL_ENGINE_CODE_ENCRYPTION_MODULE_P2   (3U)
 SA3UL Encryption engine module p2. More...
 
#define SA3UL_ENGINE_CODE_AUTHENTICATION_MODULE_P1   (4U)
 SA3UL Authentication engine module p1. More...
 
#define SA3UL_ENGINE_CODE_AUTHENTICATION_MODULE_P2   (5U)
 SA3UL Authentication engine module p2. More...
 
#define SA3UL_ENGINE_CODE_DEFAULT_EGRESS_PORT   (20U)
 SA3UL Default Engress Port. More...
 
SA3UL Encryption Algos

#define SA3UL_ENC_ALG_AES   (0x0U)
 SA3UL AES Encryption Algorithm. More...
 
#define SA3UL_ENC_ALG_TDES   (0x1U)
 SA3UL TDES Encryption Algorithm. More...
 
#define SA3UL_ENC_ALG_MAX   (0x2U)
 SA3UL Encryption Maximun number of Algorithms. More...
 
SA3UL Encryption direction

#define SA3UL_ENC_DIR_ENCRYPT   (0x0U)
 Encryption direction. More...
 
#define SA3UL_ENC_DIR_DECRYPT   (0x1U)
 Decryption direction. More...
 
SA3UL Encryption modes

#define SA3UL_ENC_MODE_ECB   (0x0U)
 ECB mode. More...
 
#define SA3UL_ENC_MODE_CBC   (0x1U)
 CBC mode. More...
 
#define SA3UL_ENC_MODE_MAX   (0x2U)
 Maximun Encryption modes. More...
 
SA3UL Encryption key sizes

#define SA3UL_ENC_KEYSIZE_128   (0x0U)
 Encryption 128 bit key size. More...
 
#define SA3UL_ENC_KEYSIZE_192   (0x1U)
 Encryption 192 bit key size. More...
 
#define SA3UL_ENC_KEYSIZE_256   (0x2U)
 Encryption 256 bit key size. More...
 
#define SA3UL_ENC_KEYSIZE_MAX   (0x3U)
 Max key size. More...
 

Typedefs

typedef void * SA3UL_Handle
 Handle to the SA3UL driver returned by SA3UL_open() More...
 

Functions

void SA3UL_init (void)
 This function initializes the SA3UL module. More...
 
void SA3UL_deinit (void)
 This function de-initializes the SA3UL module. More...
 
SA3UL_Handle SA3UL_open (uint32_t index, const SA3UL_Params *params)
 This function opens a given SA3UL module. More...
 
void SA3UL_close (SA3UL_Handle handle)
 Function to close a SA3UL module specified by the SA3UL handle. More...
 
int32_t SA3UL_contextAlloc (SA3UL_Handle handle, SA3UL_ContextObject *ctxObj, const SA3UL_ContextParams *ctxPrms)
 Function to configure secure context. More...
 
int32_t SA3UL_contextFree (SA3UL_ContextObject *pCtxObj)
 Function to free secure context configuration. More...
 
int32_t SA3UL_contextProcess (SA3UL_ContextObject *ctxObj, const uint8_t *input, uint32_t ilen, uint8_t *output)
 Function to transfer and recieve data buffer. More...
 
static void SA3UL_Params_init (SA3UL_Params *prms)
 Function to initialize default SA3UL parameters. More...
 
int32_t SA3UL_rngSetup (SA3UL_Handle handle)
 setup the SA3UL RNG module. More...
 
int32_t SA3UL_rngRead (SA3UL_Handle handle, uint32_t *out)
 Read random numbers into the output buffer. More...
 
static void SA3UL_ContextParams_init (SA3UL_ContextParams *ctxPrms)
 

Variables

SA3UL_Config gSa3ulConfig []
 Externally defined driver configuration array. More...
 
uint32_t gSa3ulConfigNum
 Externally defined driver configuration Num. More...