AM62D FreeRTOS SDK  12.00.00

Introduction

RTC Driver API/interface file.

Go to the source code of this file.

Data Structures

struct  RTC_HwAttrs
 RTC Hardware attributes. More...
 
struct  RTC_Params
 RTC Parameters. More...
 
struct  RTC_Object
 RTC driver object. More...
 
struct  RTC_Config
 RTC Global Configuration. More...
 
struct  RTC_Time
 RTC Time Structure. More...
 

Macros

#define OSCILLATOR_FREQ_HZ   ((uint32_t) 32768U)
 32.768 kHz Crystal Oscillator Frequency More...
 
#define RTC_FREEZE_MODE   ((uint32_t) 0x02000000U)
 Enable Freeze Mode. More...
 
#define O32K_OSC_DEP_EN_MASK   (CSL_RTC_GENRAL_CTL_O32K_OSC_DEP_EN_MASK)
 O32K_OSC_DEP_EN_MASK. More...
 
#define RD_PEND_MASK   (CSL_RTC_SYNCPEND_RD_PEND_MASK)
 Read Pend Status. More...
 
#define WR_PEND_MASK   (CSL_RTC_SYNCPEND_WR_PEND_MASK)
 Write Pend Status. More...
 
#define O32K_CLK_OBS_BIT_MASK   (CSL_RTC_SYNCPEND_O32K_CLK_OBS_MASK)
 O32K_CLK_OBS_BIT_MASK. More...
 
#define RTC_SW_OFF_MASK   (CSL_RTC_GENRAL_CTL_SW_OFF_MASK)
 RTC_SW_OFF_MASK. More...
 
#define RTC_UNLOCK_MASK   (CSL_RTC_GENRAL_CTL_UNLOCK_MASK)
 Unlock State Status. More...
 
#define OSC_LOCK_WAIT   (3U)
 Wait time for stabalizing OSC. More...
 
#define KICK0_UNLOCK_VALUE   (uint32_t)0x83E70B13U
 RTC Kick unlock values. More...
 
#define KICK1_UNLOCK_VALUE   (uint32_t)0x95A4F1E0U
 
#define KICK0_LOCK_VALUE   (CSL_RTC_KICK0_RESETVAL)
 RTC Kick lock values. More...
 
#define KICK1_LOCK_VALUE   (CSL_RTC_KICK1_RESETVAL)
 
#define RTC_BASEADDR   (uint32_t)0x2B1F0000U
 RTC Base Address. More...
 
RTC Timer Interrupt Set/Indication Flags

#define RTC_TMR_INT_INT0_STATUS_FLAG   (CSL_RTC_IRQSTATUS_SYS_EVENT_ON_OFF_MASK)
 ON_OFF status interrupt. More...
 
#define RTC_TMR_INT_INT1_STATUS_FLAG   (CSL_RTC_IRQSTATUS_SYS_EVENT_OFF_ON_MASK)
 OFF_ON status interrupt. More...
 
#define RTC_TMR_INT_INT0_CLEAR_FLAG   (CSL_RTC_IRQENABLE_CLR_SYS_EN_EVENT_ON_OFF_MASK)
 ON_OFF clear interrupt. More...
 
#define RTC_TMR_INT_INT1_CLEAR_FLAG   (CSL_RTC_IRQENABLE_CLR_SYS_EN_EVENT_OFF_ON_MASK)
 OFF_ON clear interrupt. More...
 
#define RTC_TMR_INT_INT0_SET_FLAG   (CSL_RTC_IRQENABLE_SET_SYS_EN_EVENT_ON_OFF_MASK)
 ON_OFF set interrupt. More...
 
#define RTC_TMR_INT_INT1_SET_FLAG   (CSL_RTC_IRQENABLE_SET_SYS_EN_EVENT_OFF_ON_MASK)
 OFF_ON set interrupt. More...
 
#define RTC_TMR_INT_INT0_RAW_STATUS_FLAG   (CSL_RTC_IRQSTATUS_RAW_SYS_EVENT_ON_OFF_MASK)
 ON_OFF raw status interrupt. More...
 
#define RTC_TMR_INT_INT1_RAW_STATUS_FLAG   (CSL_RTC_IRQSTATUS_RAW_SYS_EVENT_OFF_ON_MASK)
 OFF_ON raw status interrupt. More...
 
#define RTC_TMR_INT_STATUS_ALL
 All interrupt status mask. More...
 
#define RTC_TMR_INT_CLEAR_ALL
 All interrupt clear mask. More...
 
#define RTC_TMR_INT_REQ_ALL
 All interrupt set mask. More...
 
#define RTC_TMR_INT_RAW_STATUS_ALL
 All interrupt raw status mask. More...
 

Typedefs

typedef struct RTC_Config_s * RTC_Handle
 A handle that is returned from a RTC_open() call. More...
 
typedef void(* RTC_OnOffCallbackFxn) (RTC_Handle handle)
 The definition of a ON_OFF callback function used by the RTC driver. More...
 
typedef void(* RTC_OffOnCallbackFxn) (RTC_Handle handle)
 The definition of a OFF_ON callback function used by the RTC driver. More...
 

Functions

void RTC_init (void)
 Initialize the RTC module. More...
 
void RTC_deinit (void)
 De-initialize the RTC module. More...
 
void RTC_paramsInit (RTC_Params *params)
 Function to set default values of RTC_Params in params. More...
 
RTC_Handle RTC_open (uint32_t idx, const RTC_Params *params)
 Open the RTC at index idx with parameters params. More...
 
void RTC_close (RTC_Handle handle)
 Function to close the RTC Peripheral specified by the handle. More...
 
int32_t RTC_setTime (RTC_Handle handle, const RTC_Time *rtc_time)
 Set the RTC time. More...
 
int32_t RTC_getTime (RTC_Handle handle, RTC_Time *rtc_time)
 Get the current RTC time. More...
 
int32_t RTC_setOff_OnTimerEvent (RTC_Handle handle, const RTC_Time *rtc_time)
 Set the off-on timer event / Use as timer 1 for RTC. More...
 
int32_t RTC_setOn_OffTimerEvent (RTC_Handle handle, const RTC_Time *rtc_time)
 Set the on-off timer event / Use as timer 2 for RTC. More...
 
uint32_t RTC_readScratchRegister (RTC_Handle handle, uint32_t scratchIndex)
 Read a value from a specific RTC scratch register. More...
 
int32_t RTC_writeScratchRegister (RTC_Handle handle, uint32_t scratchIndex, uint32_t value)
 Write a value to a specific RTC scratch register. More...
 
RTC_Time RTC_calculateElapsedTime (const RTC_Time *startTime, const RTC_Time *endTime)
 Calculate Elapsed Time. More...
 
int32_t RTC_adjustForDrift (RTC_Handle handle, Float32 measuredDriftInSeconds)
 Calculate Elapsed Time. More...
 
int32_t RTC_stop (RTC_Handle handle)
 Stop the RTC. More...
 
int32_t RTC_start (RTC_Handle handle)
 Start the RTC after it's stopped. More...
 
void RTC_erratumi2327Init (void)
 RTC Erratum i2327 Workaround. More...