AM62D FreeRTOS SDK  12.00.00

Introduction

This module contains APIs to program and use the Flash module on the board like XSPI NOR Flash. See Flash for more details.

Data Structures

struct  Flash_DevConfig
 Flash device config. This will be part of the flash config, so has to be filled by sysconfig or otherwise before invoking Flash_open. More...
 
struct  Flash_Params
 Parameters passed during Flash_open() More...
 
struct  Flash_Fxns
 Driver implementation callbacks. More...
 
struct  Flash_Attrs
 Flash device attributes, these are filled by SysCfg based on the flash device that is selected. More...
 
struct  Flash_Config
 Flash driver configuration, these are filled by SysCfg based on the flash device that is selected. More...
 

Functions

void Flash_Params_init (Flash_Params *params)
 Set default parameters in the Flash_Params_s structure. More...
 
Flash_Handle Flash_open (uint32_t instanceId, Flash_Params *params)
 Open flash driver. More...
 
void Flash_close (Flash_Handle handle)
 Close flash driver. More...
 
Flash_Handle Flash_getHandle (uint32_t instanceId)
 Get handle to flash driver. More...
 
int32_t Flash_read (Flash_Handle handle, uint32_t offset, uint8_t *buf, uint32_t len)
 Read data from flash. More...
 
int32_t Flash_write (Flash_Handle handle, uint32_t offset, uint8_t *buf, uint32_t len)
 Write to flash. More...
 
int32_t Flash_blkPageToOffset (Flash_Handle handle, uint32_t *offset, uint32_t block, uint32_t page)
 Utility API to convert (Block Num, Page Num) to offset in bytes. More...
 
int32_t Flash_offsetToBlkPage (Flash_Handle handle, uint32_t offset, uint32_t *block, uint32_t *page)
 Utility API to convert offset in bytes to (Block Num, Page Num) More...
 
int32_t Flash_SectorPageToOffset (Flash_Handle handle, uint32_t *offset, uint32_t sector, uint32_t page)
 Utility API to convert (Sector Num, Page Num) to offset in bytes. More...
 
int32_t Flash_offsetToSectorPage (Flash_Handle handle, uint32_t offset, uint32_t *sector, uint32_t *page)
 Utility API to convert offset in bytes to (Sector Num, Page Num) More...
 
int32_t Flash_eraseBlk (Flash_Handle handle, uint32_t blockNum)
 Erase a block from flash. More...
 
int32_t Flash_eraseSector (Flash_Handle handle, uint32_t sectorNum)
 Erase a sector from flash. More...
 
int32_t Flash_reset (Flash_Handle handle)
 Do a soft reset of the flash. More...
 
int32_t Flash_enablePhyPipeline (Flash_Handle handle)
 Enables PHY mode in flash. More...
 
int32_t Flash_disablePhyPipeline (Flash_Handle handle)
 Disable PHY mode in flash. More...
 
uint32_t Flash_getPhyTuningOffset (Flash_Handle handle)
 Return flash offset to write PHY tuning data. More...
 
Flash_AttrsFlash_getAttrs (uint32_t instanceId)
 Return flash attributes. More...
 
uint32_t Flash_getFlashInterfaceIndex (uint32_t flashType)
 Return flash index based on type of flash. More...
 
void Flash_init (void)
 This function initializes the Flash module. More...
 
void Flash_deinit (void)
 This function de-initializes the Flash module. More...
 
int32_t Flash_phyTune (Flash_Handle handle)
 This function performs PHY tuning. More...
 

Typedefs

typedef void * Flash_Handle
 Handle to the FLash driver returned by Flash_opem() More...
 

Flash driver implementation callbacks

typedef int32_t(* Flash_OpenFxn) (Flash_Config *config, Flash_Params *params)
 Driver implementation to open a specific flash driver. More...
 
typedef void(* Flash_CloseFxn) (Flash_Config *config)
 Driver implementation to close a specific flash driver. More...
 
typedef int32_t(* Flash_ReadFxn) (Flash_Config *config, uint32_t offset, uint8_t *buf, uint32_t len)
 Driver implementation to read from flash using a specific flash driver. More...
 
typedef int32_t(* Flash_WriteFxn) (Flash_Config *config, uint32_t offset, uint8_t *buf, uint32_t len)
 Driver implementation to write to flash using specific flash driver. More...
 
typedef int32_t(* Flash_EraseFxn) (Flash_Config *config, uint32_t blockNum)
 Driver implementation to erase a block using a specific flash driver. More...
 
typedef int32_t(* Flash_EraseSectorFxn) (Flash_Config *config, uint32_t sectorNum)
 Driver implementation to erase a sector using a specific flash driver. More...
 
typedef int32_t(* Flash_ResetFxn) (Flash_Config *config)
 Driver implementation to soft reset the flash. More...
 
typedef int32_t(* Flash_EnablePhyPipelineFxn) (Flash_Config *config)
 Driver implementation to enable PHY pipeline mode in Flash. More...
 
typedef int32_t(* Flash_DisablePhyPipelineFxn) (Flash_Config *config)
 Driver implementation to disable PHY pipeline mode in Flash. More...
 
typedef int32_t(* Flash_quirksFxn) (Flash_Config *config)
 User implementation of a custom function to handle vendor specific quirks. More...
 
typedef int32_t(* Flash_custProtocolFxn) (Flash_Config *config)
 User implementation of a custom function to configure flash to operate in a specific protocol. More...
 
typedef int32_t(* Flash_PhyTuneFxn) (Flash_Config *config)
 Driver implementation to perform phy tuning using a specific flash driver. More...
 

Typedef Documentation

◆ Flash_Handle

typedef void* Flash_Handle

Handle to the FLash driver returned by Flash_opem()

◆ Flash_OpenFxn

typedef int32_t(* Flash_OpenFxn) (Flash_Config *config, Flash_Params *params)

Driver implementation to open a specific flash driver.

Typically this callback is hidden from the end application and is implemented when a new type of flash device needs to be implemented.

Parameters
config[in] Flash configuration for the specific flash device
params[in] User controllable parameters when opening the flash device
Returns
SystemP_SUCCESS on success, else failure

◆ Flash_CloseFxn

typedef void(* Flash_CloseFxn) (Flash_Config *config)

Driver implementation to close a specific flash driver.

Typically this callback is hidden from the end application and is implemented when a new type of flash device needs to be implemented.

Parameters
config[in] Flash configuration for the specific flash device
Returns
SystemP_SUCCESS on success, else failure

◆ Flash_ReadFxn

typedef int32_t(* Flash_ReadFxn) (Flash_Config *config, uint32_t offset, uint8_t *buf, uint32_t len)

Driver implementation to read from flash using a specific flash driver.

Typically this callback is hidden from the end application and is implemented when a new type of flash device needs to be implemented.

Parameters
config[in] Flash configuration for the specific flash device
offset[in] Offset in the flash from where to start the read
buf[in] Buffer into which to read the data into
len[in] Length of the data to read, in bytes
Returns
SystemP_SUCCESS on success, else failure

◆ Flash_WriteFxn

typedef int32_t(* Flash_WriteFxn) (Flash_Config *config, uint32_t offset, uint8_t *buf, uint32_t len)

Driver implementation to write to flash using specific flash driver.

Typically this callback is hidden from the end application and is implemented when a new type of flash device needs to be implemented.

Parameters
config[in] Flash configuration for the specific flash device
offset[in] Offset in the flash from where to start the write.
buf[in] Buffer which has the data to write.
len[in] Length of the data to write, in bytes
Returns
SystemP_SUCCESS on success, else failure

◆ Flash_EraseFxn

typedef int32_t(* Flash_EraseFxn) (Flash_Config *config, uint32_t blockNum)

Driver implementation to erase a block using a specific flash driver.

Typically this callback is hidden from the end application and is implemented when a new type of flash device needs to be implemented.

Parameters
config[in] Flash configuration for the specific flash device
blockNum[in] Block number to erase.
Returns
SystemP_SUCCESS on success, else failure

◆ Flash_EraseSectorFxn

typedef int32_t(* Flash_EraseSectorFxn) (Flash_Config *config, uint32_t sectorNum)

Driver implementation to erase a sector using a specific flash driver.

Typically this callback is hidden from the end application and is implemented when a new type of flash device needs to be implemented.

Parameters
config[in] Flash configuration for the specific flash device
sectorNum[in] Sector number to erase.
Returns
SystemP_SUCCESS on success, else failure

◆ Flash_ResetFxn

typedef int32_t(* Flash_ResetFxn) (Flash_Config *config)

Driver implementation to soft reset the flash.

Typically this callback is hidden from the end application and is implemented when a new type of flash device needs to be implemented.

Parameters
config[in] Flash configuration for the specific flash device
Returns
SystemP_SUCCESS on success, else failure

◆ Flash_EnablePhyPipelineFxn

typedef int32_t(* Flash_EnablePhyPipelineFxn) (Flash_Config *config)

Driver implementation to enable PHY pipeline mode in Flash.

Typically this callback is hidden from the end application and is implemented when a new type of flash device needs to be implemented.

Parameters
config[in] Flash configuration for the specific flash device
Returns
SystemP_SUCCESS on success, else failure

◆ Flash_DisablePhyPipelineFxn

typedef int32_t(* Flash_DisablePhyPipelineFxn) (Flash_Config *config)

Driver implementation to disable PHY pipeline mode in Flash.

Typically this callback is hidden from the end application and is implemented when a new type of flash device needs to be implemented.

Parameters
config[in] Flash configuration for the specific flash device
Returns
SystemP_SUCCESS on success, else failure

◆ Flash_quirksFxn

typedef int32_t(* Flash_quirksFxn) (Flash_Config *config)

User implementation of a custom function to handle vendor specific quirks.

Typically this callback is hidden from the end application and is implemented when a new type of flash device needs to be implemented.

Parameters
config[in] Flash configuration for the specific flash device
Returns
SystemP_SUCCESS on success, else failure

◆ Flash_custProtocolFxn

typedef int32_t(* Flash_custProtocolFxn) (Flash_Config *config)

User implementation of a custom function to configure flash to operate in a specific protocol.

Parameters
config[in] Flash configuration for the specific flash device
Returns
SystemP_SUCCESS on success, else failure

◆ Flash_PhyTuneFxn

typedef int32_t(* Flash_PhyTuneFxn) (Flash_Config *config)

Driver implementation to perform phy tuning using a specific flash driver.

Parameters
config[in] Flash configuration for the specific flash device
Returns
SystemP_SUCCESS on success, else failure

Function Documentation

◆ Flash_Params_init()

void Flash_Params_init ( Flash_Params *  params)

Set default parameters in the Flash_Params_s structure.

Call this API to set defaults and then override the fields as needed before calling Flash_open.

Parameters
params[out] Initialized parameters

◆ Flash_open()

Flash_Handle Flash_open ( uint32_t  instanceId,
Flash_Params *  params 
)

Open flash driver.

Make sure the SOC peripheral driver is opened before calling this API. Drivers_open function generated by SysCfg opens the underlying SOC peripheral driver, e.g OSPI.

Internally this API also reads the device and manufacture ID and checks if it matches the expected value for the flash device, if there is mismatch then NULL is returned.

Global variables Flash_Config gFlashConfig[] and uint32_t gFlashConfigNum is instantiated by SysCfg to describe the flash configuration based on user selection in SysCfg.

Parameters
instanceId[in] Index within Flash_Config gFlashConfig[] denoting the flash driver to open
params[in] Open parameters
Returns
Handle to flash driver which should be used in subsequent API call
NULL in case of failure

◆ Flash_close()

void Flash_close ( Flash_Handle  handle)

Close flash driver.

Parameters
handle[in] Flash driver handle from Flash_open

◆ Flash_getHandle()

Flash_Handle Flash_getHandle ( uint32_t  instanceId)

Get handle to flash driver.

Parameters
instanceId[in] Index within Flash_Config gFlashConfig[]
Returns
Handle to flash driver
NULL in case of failure

◆ Flash_read()

int32_t Flash_read ( Flash_Handle  handle,
uint32_t  offset,
uint8_t *  buf,
uint32_t  len 
)

Read data from flash.

Internally it will use DMA and do the needed cache sync operations as needed.

Parameters
handle[in] Flash driver handle from Flash_open
offset[in] Offset in the flash from where to start the read
buf[in] Buffer into which to read the data into
len[in] Length of the data to read, in bytes
Returns
SystemP_SUCCESS on success, else failure

◆ Flash_write()

int32_t Flash_write ( Flash_Handle  handle,
uint32_t  offset,
uint8_t *  buf,
uint32_t  len 
)

Write to flash.

Make sure the block is erased before writing

Parameters
handle[in] Flash driver handle from Flash_open
offset[in] Offset in the flash from where to start the write.
buf[in] Buffer which has the data to write.
len[in] Length of the data to write, in bytes
Returns
SystemP_SUCCESS on success, else failure

◆ Flash_blkPageToOffset()

int32_t Flash_blkPageToOffset ( Flash_Handle  handle,
uint32_t *  offset,
uint32_t  block,
uint32_t  page 
)

Utility API to convert (Block Num, Page Num) to offset in bytes.

Parameters
handle[in] Flash driver handle from Flash_open
offset[out] Offset in the flash, in bytes.
block[in] Block number to convert
page[in] Page number within the block
Returns
SystemP_SUCCESS on success, else failure

◆ Flash_offsetToBlkPage()

int32_t Flash_offsetToBlkPage ( Flash_Handle  handle,
uint32_t  offset,
uint32_t *  block,
uint32_t *  page 
)

Utility API to convert offset in bytes to (Block Num, Page Num)

Parameters
handle[in] Flash driver handle from Flash_open
offset[in] Offset in the flash, in bytes. MUST be page size aligned.
block[out] Converted Block number
page[out] Converted Page number within the block
Returns
SystemP_SUCCESS on success, else failure

◆ Flash_SectorPageToOffset()

int32_t Flash_SectorPageToOffset ( Flash_Handle  handle,
uint32_t *  offset,
uint32_t  sector,
uint32_t  page 
)

Utility API to convert (Sector Num, Page Num) to offset in bytes.

Parameters
handle[in] Flash driver handle from Flash_open
offset[out] Offset in the flash, in bytes.
sector[in] Sector number to convert
page[in] Page number within the block
Returns
SystemP_SUCCESS on success, else failure

◆ Flash_offsetToSectorPage()

int32_t Flash_offsetToSectorPage ( Flash_Handle  handle,
uint32_t  offset,
uint32_t *  sector,
uint32_t *  page 
)

Utility API to convert offset in bytes to (Sector Num, Page Num)

Parameters
handle[in] Flash driver handle from Flash_open
offset[in] Offset in the flash, in bytes. MUST be page size aligned.
sector[out] Converted sector number
page[out] Converted Page number within the block
Returns
SystemP_SUCCESS on success, else failure

◆ Flash_eraseBlk()

int32_t Flash_eraseBlk ( Flash_Handle  handle,
uint32_t  blockNum 
)

Erase a block from flash.

Use the utility API Flash_offsetToBlkPage to convert a offset to block number

Parameters
handle[in] Flash driver handle from Flash_open
blockNum[in] Block number to erase.
Returns
SystemP_SUCCESS on success, else failure

◆ Flash_eraseSector()

int32_t Flash_eraseSector ( Flash_Handle  handle,
uint32_t  sectorNum 
)

Erase a sector from flash.

Use the utility API Flash_offsetToSectorPage to convert a offset to block number

Parameters
handle[in] Flash driver handle from Flash_open
sectorNum[in] Sector number to erase.
Returns
SystemP_SUCCESS on success, else failure

◆ Flash_reset()

int32_t Flash_reset ( Flash_Handle  handle)

Do a soft reset of the flash.

Parameters
handle[in] Flash driver handle from Flash_open
Returns
SystemP_SUCCESS on success, else failure

◆ Flash_enablePhyPipeline()

int32_t Flash_enablePhyPipeline ( Flash_Handle  handle)

Enables PHY mode in flash.

Parameters
handle[in] Flash driver handle from Flash_open
Returns
SystemP_SUCCESS on success, else failure

◆ Flash_disablePhyPipeline()

int32_t Flash_disablePhyPipeline ( Flash_Handle  handle)

Disable PHY mode in flash.

Parameters
handle[in] Flash driver handle from Flash_open
Returns
SystemP_SUCCESS on success, else failure

◆ Flash_getPhyTuningOffset()

uint32_t Flash_getPhyTuningOffset ( Flash_Handle  handle)

Return flash offset to write PHY tuning data.

Parameters
handle[in] Flash driver handle from Flash_open
Returns
Tuning offset on SUCCESS, else 0xFFFFFFFF if handle is invalid

◆ Flash_getAttrs()

Flash_Attrs* Flash_getAttrs ( uint32_t  instanceId)

Return flash attributes.

Parameters
instanceId[in] Flash instance ID
Returns
Flash_Attrs, else NULL if instanceId is invalid

◆ Flash_getFlashInterfaceIndex()

uint32_t Flash_getFlashInterfaceIndex ( uint32_t  flashType)

Return flash index based on type of flash.

Parameters
flashType[in] Flash Type (Serial/Parallel)
Returns
Flash_Attrs driver instance index corresponding to the flash type

◆ Flash_init()

void Flash_init ( void  )

This function initializes the Flash module.

◆ Flash_deinit()

void Flash_deinit ( void  )

This function de-initializes the Flash module.

◆ Flash_phyTune()

int32_t Flash_phyTune ( Flash_Handle  handle)

This function performs PHY tuning.

Make sure phy is enabled before calling this

Parameters
handle[in] Flash driver handle from Flash_open
Returns
SystemP_SUCCESS on success, else failure