AM62D FreeRTOS SDK  12.00.00
calcratio.h File Reference

Introduction

CALCRATIO API/interface file.

Go to the source code of this file.

Data Structures

struct  CalcRatio_t
 CALCRATIO Parameters. More...
 

Macros

#define CALCRATIO_MA1_LENGTH   (1024U)
 Length of the first-stage moving average filter used in ratio smoothing. More...
 
#define CALCRATIO_MA2_LENGTH   (128U)
 Length of the second-stage moving average filter for refined smoothing. More...
 

Functions

int32_t calcRatio_init (CalcRatio_t *calcRatioInstance, float sampleRateIn, float sampleRateOut)
 Initializes the ratio calculation module for ASRC (Asynchronous Sample Rate Converter) with input and output sample rates. More...
 
int32_t calcRatio_exec (CalcRatio_t *calcRatioInstance, double *Tx_Counter, double *Rx_Counter)
 Executes the CALCRATIO algorithm to derive and update the smoothed actual sample rate ratio. More...
 
double calcRatio_getActualratio (CalcRatio_t *calcRatioInstance)
 Safely retrieve the derived actual sample rate ratio. More...