OSPI PHY Tuning Window Parameters.
These are input window parameters for OSPI PHY tuning algorithm. This data is usually SOC specific and is filled by SysConfig.
Data Fields | |
| int32_t | txDllLowWindowStart |
| int32_t | txDllLowWindowEnd |
| int32_t | txDllHighWindowStart |
| int32_t | txDllHighWindowEnd |
| int32_t | rxLowSearchStart |
| int32_t | rxLowSearchEnd |
| int32_t | rxHighSearchStart |
| int32_t | rxHighSearchEnd |
| int32_t | txLowSearchStart |
| int32_t | txLowSearchEnd |
| int32_t | txHighSearchStart |
| int32_t | txHighSearchEnd |
| int32_t | txDLLSearchOffset |
| uint32_t | rxTxDLLSearchStep |
| uint32_t | rdDelayMin |
| uint32_t | rdDelayMax |
| int32_t OSPI_PhyTuneWindowParams::txDllLowWindowStart |
Tx Dll window lower value to search RxDLL low and high. This corresponds to the bottom left point serach.
| int32_t OSPI_PhyTuneWindowParams::txDllLowWindowEnd |
Tx Dll window higher value to search RxDLL low and high. This corresponds to the bottom left point search.
| int32_t OSPI_PhyTuneWindowParams::txDllHighWindowStart |
Tx Dll window lower value to search RxDLL low and high. This corresponds to the top right point search.
| int32_t OSPI_PhyTuneWindowParams::txDllHighWindowEnd |
Tx Dll window higher value to search RxDLL low and high. This corresponds to the top right point search.
| int32_t OSPI_PhyTuneWindowParams::rxLowSearchStart |
Rx Dll lower value for Rx Dll low search. The value of Rx dll will lie in this window bottom left point search.
| int32_t OSPI_PhyTuneWindowParams::rxLowSearchEnd |
Rx Dll higher value for Rx Dll low search. The value of Rx dll will lie in this window bottom left point search.
| int32_t OSPI_PhyTuneWindowParams::rxHighSearchStart |
Rx Dll lower value for Rx Dll high search. The value of Rx dll will lie in this window top right point search.
| int32_t OSPI_PhyTuneWindowParams::rxHighSearchEnd |
Rx Dll higher value for Rx Dll high search. The value of Rx dll will lie in this window for top right point search.
| int32_t OSPI_PhyTuneWindowParams::txLowSearchStart |
Tx Dll lower value for Tx Dll low search. The value of Tx dll will lie in this window.
| int32_t OSPI_PhyTuneWindowParams::txLowSearchEnd |
Tx Dll higher value for Tx Dll low search. The value of Tx dll will lie in this window.
| int32_t OSPI_PhyTuneWindowParams::txHighSearchStart |
Tx Dll lower value for Tx Dll high search. The value of Tx dll will lie in this window.
| int32_t OSPI_PhyTuneWindowParams::txHighSearchEnd |
Tx Dll higher value for Tx Dll high search. The value of Tx dll will lie in this window.
| int32_t OSPI_PhyTuneWindowParams::txDLLSearchOffset |
Tx Dll step increase for backup Rx Dll low and high search.
| uint32_t OSPI_PhyTuneWindowParams::rxTxDLLSearchStep |
Rx Dll and Tx DLL step increase for Rx Dll and Tx Dll low and high search.
| uint32_t OSPI_PhyTuneWindowParams::rdDelayMin |
Minimum value of Read delay for Read Delay Capture Register for tuning search.
| uint32_t OSPI_PhyTuneWindowParams::rdDelayMax |
Maximum value of Read delay for Read Delay Capture Register for tuning search.