Structure for MCAN High Priority Message.
Data Fields | |
| uint32_t | bufIdx |
| uint32_t | msi |
| uint32_t | filterIdx |
| uint32_t | filterList |
| uint32_t MCAN_HighPriorityMsgInfo::bufIdx |
Buffer Index Only valid when MSI[1] = 1.
| uint32_t MCAN_HighPriorityMsgInfo::msi |
Message Storage Indicator MSI[1:0] 00 = No FIFO selected 01 = FIFO message lost 10 = Message stored in FIFO 0 11 = Message stored in FIFO 1
| uint32_t MCAN_HighPriorityMsgInfo::filterIdx |
Filter Index
| uint32_t MCAN_HighPriorityMsgInfo::filterList |
Indicates the filter list of the matching filter element 0 = Standard Filter List 1 = Extended Filter List