AM62Ax MCU+ SDK  09.02.00
safety_checkers_pm_soc.h File Reference

Introduction

This file contains data structures for PM safety checker module.

Go to the source code of this file.

Macros

#define SAFETY_CHECKERS_PM_WKUP_PSC_BASE_ADDRESS   (CSL_WKUP_PSC0_BASE)
 WKUP PSC base address. More...
 
#define SAFETY_CHECKERS_PM_PSC_PD_STAT_OFFSET   (0x200U)
 PSC Power Domain(PD) STAT register offset. More...
 
#define SAFETY_CHECKERS_PM_PSC_MD_STAT_OFFSET   (0x800U)
 PSC Module Domain(MD) STAT register offset. More...
 
#define SAFETY_CHECKERS_PM_PLL_BASE_ADDRESS(i)   (SAFETY_CHECKERS_PM_PLL_CFG_BASE_ADDRESS + (0x1000U * (uint32_t)i))
 Each PLL base addresses. More...
 
#define SAFETY_CHECKERS_PM_MCU_PLL_BASE_ADDRESS(i)   (SAFETY_CHECKERS_PM_MCU_PLL_CFG_BASE_ADDRESS + (0x1000U * (uint32_t)i))
 
#define SAFETY_CHECKERS_PM_KICK_LOCK   (0x00000000U)
 KICK lock values. More...
 
#define SAFETY_CHECKERS_PM_LOCK_KEY0_OFFSET   (0x10U)
 
#define SAFETY_CHECKERS_PM_LOCK_KEY1_OFFSET   (0x14U)
 

Variables

static uint32_t gSafetyCheckers_PmPllRegOffset0 []
 This defines the array holding register offset values for the each PLL's. More...
 
static uint32_t gSafetyCheckers_PmPllRegOffset1 []
 
static uint32_t gSafetyCheckers_PmPllRegOffset2 []
 
static uint32_t gSafetyCheckers_PmPllRegOffset3 []
 
static uint32_t gSafetyCheckers_PmPllRegOffset4 []
 
static uint32_t gSafetyCheckers_PmPllRegOffset5 []